AM275 FreeRTOS SDK  12.00.00
Data Abort Test

Introduction

This example shows the how custom data abort handler be implemented in the user application. Provides information about the prefetch abort exception

  1. Contents of DFSR (Data Fault Status Register) register
    1. status: indicates the type of fault generated
    2. sd: distinguishes between an AXI Decode or Slave error on an external abort. This bit is only valid for external aborts. For all other aborts types of abort, this bit is set to zero.
    3. rw: Indicates whether a read or write access caused an abort (0=read abort; 1=write abort)
  2. Contents of ADFSR (Auxillary Data Fault Status Register) register
    1. index: returns the index value for the access giving the error
    2. side_ext: value returned in this field indicates the source of the error
    3. recoverable_error: value returned in this field indicates if the error is recoverable (0=Unrecoverable error, 1=Recoverable Error)
    4. cacheway: value returned in this field indicates the cache way or ways in which the error occurred
  3. dfar (Data Fault Address Register): Address of the data trying to be written or read.
  4. lr: Link Register when the exception occurred.
  5. spsr: Saved Program status registers to get the program status when the exception occurred.
Note
Please refer to R5F TRM for more information

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
r5fss0-0 freertos
Toolchain ti-arm-clang
Board am275x-evm
Example folder examples/kernel/dpl/test_data_abort/

Steps to Run the Example

Sample Output

Note
this application do not gives any output. This goes inside the HwiP_user_data_abort_handler_c function and loops forever there. User needs to pause the applcaition and see the values.