AM275 FreeRTOS SDK  12.00.00
RL2 Example

Introduction

Rl2 example provides how to use RL2 in applications and also shows how RL2 brings in benefits.

Supported Combinations

Parameter       Value
CPU + OS       r5fss0-0 nortos
Toolchain       ti-arm-clang
Boards         am275x-evm
Example folder examples/drivers/rl2

Steps to Run the Example

Sample Output

Starting OSPI Bootloader ...
SYSFW Firmware Version 11.0.7--v11.00.07 (Fancy Rat)
SYSFW Firmware revision 0xb
SYSFW ABI revision 4.0
[BOOTLOADER_PROFILE] Boot Media : FLASH
[BOOTLOADER_PROFILE] Boot Media Clock : 166.667 MHz
[BOOTLOADER_PROFILE] Boot Image Size : 441 KB
[BOOTLOADER_PROFILE] Cores present :
[BOOTLOADER PROFILE] TIFS init : 750us
[BOOTLOADER PROFILE] System_init : 1895us
[BOOTLOADER PROFILE] Board_init : 2us
[BOOTLOADER PROFILE] FreeRtosTask Create : 255us
[BOOTLOADER PROFILE] Drivers_open : 98us
[BOOTLOADER PROFILE] Board_driversOpen : 0us
[BOOTLOADER PROFILE] sciServer_init : 15068us
[BOOTLOADER PROFILE] SBL Drivers_open : 3168us
[BOOTLOADER PROFILE] SBL Board_driversOpen : 2917us
[BOOTLOADER PROFILE] Sciclient Get Version : 10023us
[BOOTLOADER PROFILE] R5FSS0_0 Image Load : 1674us
[BOOTLOADER PROFILE] R5FSS0_1 Image Load : 1564us
[BOOTLOADER PROFILE] R5FSS1_0 Image Load : 1568us
[BOOTLOADER PROFILE] R5FSS1_1 Image Load : 1552us
[BOOTLOADER PROFILE] DSP 0 Image Load : 6963us
[BOOTLOADER PROFILE] DSP 1 Image Load : 6821us
[BOOTLOADER_PROFILE] SBL Total Time Taken : 54325us
Image loading done...
Starting RTOS/Baremetal applications
L2 Cache: i = 0 Miss = 129 Hits = 0
L2 Cache: i = 1 Miss = 0 Hits = 129
L2 Cache: i = 2 Miss = 0 Hits = 129
L2 Cache: i = 3 Miss = 0 Hits = 129
L2 Cache: i = 4 Miss = 0 Hits = 129
L2 Cache: i = 5 Miss = 0 Hits = 129
L2 Cache: i = 6 Miss = 0 Hits = 129
L2 Cache: i = 7 Miss = 0 Hits = 129
L2 Cache: i = 8 Miss = 0 Hits = 129
L2 Cache: i = 9 Miss = 0 Hits = 129
Profile Point: With RL2
Cycle Count: 97006
No. Of CPU instructions executed Count: 21184
ICache Miss Count: 8
ICache Access Count: 450
Profile Point: Without RL2
Cycle Count: 340983
No. Of CPU instructions executed Count: 20699
ICache Miss Count: 0
ICache Access Count: 165
All tests have passed!!

Description

On how to configure RL2, please go through Configuring OptiFlash various IP.

This example shows how RL2 is used and how its different functions are used. With RL2 enabled, the function that was being executed is getting cached in the RL2 cache bank. First time, it caused 129 L2 cache misses, and because each L2 cache line (at a size of 128KB) is 32 bytes, it implies that a total of ~4KB of code is being cached. This is in alignment with the size of the function that is being executed from the flash. Later on, every time there were L2 cache hits,

Another point to highlight is performance improvement. This is clear from the cycle count with RL2 and without RL2.