AM275 FreeRTOS SDK  12.00.00
MCSPI Loopback

Introduction

This example demonstrates the McSPI RX and TX operation configured in blocking, interrupt mode of operation.

This example sends a known data in the TX mode of length APP_MCSPI_MSGSIZE and then receives the same in RX mode. Internal pad level loopback mode is enabled to receive data. To enable internal pad level loopback mode, D0 pin is configured to both TX Enable as well as RX input pin in the SYSCFG.

When transfer is completed, TX and RX buffer data are compared. If data is matched, test result is passed otherwise failed.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 freertos
r5fss0-0 nortos
c75ss0-0 freertos
Toolchain ti-arm-clang
ti-c7000
Board am275x-evm
Example folder examples/drivers/mcspi/mcspi_loopback

Steps to Run the Example

See Also

MCSPI

Sample Output

Shown below is a sample output when the application is run,

[MCSPI] Loopback example started ...
All tests have passed!!