AM275 FreeRTOS SDK  12.00.00
AASRC Stereo Playback

Introduction

This example demonstrates the AASRC configured for STEREO operating mode. AASRC takes the digital audio data streams received using McASP at 48 kHz FSYNC rate and converts the same to 96 kHz and send out the converted data as audio out using McASP. McASP FSYNC clocks is being used as the reference clock for AASRC receive and transmit. Audio can be inputed from the 3.5mm audio line in jack (J2 Top) and audio out can be heard from audio line out jack (J3 Top).

  • AASRC & McASP is configured in 24 bit data format

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 freertos
c75ss0-0 freertos
Toolchain ti-arm-clang
ti-c7000
Board am275x-evm
Example folder examples/drivers/aasrc/aasrc_stereo_playback

Steps to Run the Example

  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
  • Connect audio devices as mentioned in the introduction
  • Launch a CCS debug session and run the executable, see CCS Launch, Load and Run

See Also

AASRC

Sample Output

Shown below is a sample output when the application is run,

[AASRC] Audio playback example started.
Enter your response on UART terminal
Stop the demo? (y/n) : y
Exiting demo