AM275 FreeRTOS SDK  12.00.00
DMA Utils autoincrement circular example

Introduction

Demostrates a simple application demonstrating 2D auto increment feature with circularity enabled of dmautils

The application runs on C7x core. UDMA is configured for UTC/DRU mode.

Supported Combinations

Parameter Value
CPU + OS c75ss0-0 freertos
c75ss1-0 freertos
Toolchain ti-c7000
Board am275x-evm
Example folder examples/dmautils/dmautils_autoinc_circular/

Steps to Run the Example

Sample Output

Shown below is a sample output when the application is run,

DMAUtils TestCase 0, PASSED
All tests have passed!!