AM275 FreeRTOS SDK  12.00.00
HYPERBUS

HYPERBUS peripheral is a driver which provides an interface with storage devices which follows HYPERRAM/HYPERFLASH protocol. The driver supports single bit, four bit and eight bit data lines to communicate with the connected media.

Features Supported

  • Support for Cypress® HyperRAM
  • Up to 166 MHz maximum memory bus operation for reads
  • Low pin count interface with LVCMOS I/O pins (can be muxed with other FSS interfaces (OSPIs)) Two memory chip selects
  • Linear incrementing mode for reads and writes
  • Asynchronous bus clock

SysConfig Features

Note
It is strongly recommend to use SysConfig where it is available instead of using direct SW API calls. This will help simplify the SW application and also catch common mistakes early in the development cycle.

Features not Supported

  • Cache-line wrap and fixed address modes for reads or writes
  • General Purpose Output register (FSS0_HPB0_MC_GPOR) of the HBMC is not used
  • HyperFlash
  • ECC
  • OTFA

Example Usage

Include the below file to access the APIs

#include <stdio.h>

Instance Open Example

gHyperBusHandle = HYPERBUS_open(0);
DebugP_assert(gHyperBusHandle != NULL);

Instance Close Example

HYPERBUS_close(gHyperBusHandle);

API

APIs for HYPERBUS

HYPERBUS_close
void HYPERBUS_close(HYPERBUS_Handle handle)
Function to close a HYPERBUS peripheral specified by the HYPERBUS handle.
hyperbus.h
HYPERBUS_open
HYPERBUS_Handle HYPERBUS_open(uint32_t index)
This function opens a given HYPERBUS peripheral.
DebugP_assert
#define DebugP_assert(expression)
Function to call for assert check.
Definition: DebugP.h:183