AM275 FreeRTOS SDK  12.00.00
Flash

The driver takes care of all sequencing necessary to perform writes across pages and the application need not take care of the programming intricacies.

Features Supported

  • APIs to read and write to a flash offset
  • Provides API to return flash attributes like block size, page size etc
  • API for block erases

Flash Layout

The NOR flash S28HS512T present in AM62 SoCs allows users to configure flash in different layouts by writing to the configuration registers, a feature not supported by other NOR flash devices. Other NOR flash parts from vendors like Micron, Macronix, ISSI, and Winbond only support uniform flash layouts, where the entire flash is divided into blocks of uniform size, with blocks further divided into sectors. In these standard flash devices, block erase and sector erase operations can be performed at any offset, erasing either an entire block or a sector based on the operation chosen.

In contrast, the S28HS512T supports sector erase operations only in non-uniform mode specifically on the 4KB sectors. In uniform mode, only block erase operations are allowed, and attempting sector erase operations has no effect.

The S28HS512T supports four different flash layouts:

  • Uniform: The entire flash is divided into uniform 256KB blocks.
  • Bottom Hybrid: The first 256KB of flash is divided into 32 sectors of 4KB each and 1 block of 128KB, while the remaining flash is divided into 256KB blocks.
  • Top Hybrid: The last 256KB of flash is divided into 32 sectors of 4KB each and 1 block of 128KB, while the remaining flash is divided into 256KB blocks.
  • Split Hybrid: The first and last blocks are each divided into 16 sectors of 4KB and 1 block of 192KB, with the middle portion of flash divided into 256KB blocks.

How To Configure Hybrid Layout

Flash Layout Configuration

The S28HS512T NOR flash supports multiple memory layout configurations that affect sector organization and erase operations. The driver automatically configures the flash layout during initialization through the Flash_quirkSpansionConfigureLayout function in flash_nor_ospi.c.

Configuring Flash Layout

To customize the flash layout, modify the layout configuration using Flash_NorOspiHybridLayoutCfg structure before calling flash open.

typedef struct {
uint32_t isHybridLayout; /* 0: Uniform layout, 1: Hybrid layout */
uint32_t hybridLayoutType; /* Hybrid layout type (see table below) */
} Flash_NorOspiHybridLayoutCfg;

Available Layout Options

Main Layout Types

Layout Type Value Description
Uniform Layout 0U Standard uniform sector sizes throughout the entire flash memory
Hybrid Layout 1U Mixed sector sizes for more flexible memory management

Hybrid Layout Configurations

When isHybridLayout is set to 1, you must specify the hybrid layout type using hybridLayoutType:

Hybrid Layout Type Value Description
Bottom Hybrid 0U Smaller sectors at the bottom (low addresses) of flash memory
Top Hybrid 1U Smaller sectors at the top (high addresses) of flash memory
Split Hybrid 2U Smaller sectors at both bottom and top of flash memory

Example Configuration

For a hybrid layout with smaller sectors at both the bottom and top of memory (Split Hybrid):

/* Get the layout configuration from flash config */
Flash_NorOspiHybridLayoutCfg *layoutCfg = (Flash_NorOspiHybridLayoutCfg*)(gFlashConfig[CONFIG_FLASH0].layoutCfg);
/* Configure for split hybrid layout */
layoutCfg->isHybridLayout = 1U; /* Hybrid layout */
layoutCfg->hybridLayoutType = 2U; /* Split hybrid type */

Custom Flash Layout Implementation

Developers can implement their own custom configuration function to accommodate specific flash layouts according to flash datasheet specifications. This is particularly useful when:

  • Working with flash devices that have non-standard sector arrangements
  • Implementing custom command sequences
  • Supporting specialized flash memory with unique organization requirements

To add a custom flash configuration function:

  1. Define a layout configuration struct as described in Configuring Flash Layout. This struct can be accessed within your quirk function via the Flash_Config *cfg parameter. The config struct includes a void* layoutCfg pointer that references your layout configuration.
  2. Implement your quirk function in flash_nor_ospi.c following the required signature:
    int32_t YourQuirkFunction(Flash_Config *cfg);
  3. Register your quirk function by updating the quirk_function field in the flash section of your board configuration.

Example implementation:

/* In flash_nor_ospi.c */
int32_t myQuirksFxn(Flash_Config *cfg)
{
/* Access layout configuration if needed */
MyFlashLayoutCfg *layoutCfg = (MyFlashLayoutCfg *)cfg->layoutCfg;
/* Your code for handling quirks goes here */
/* For example: modify flash timing parameters, handle special initialization, etc. */
return status;
}
Flash Quirks Fxn Configuration

SysConfig Features

Note
It is strongly recommend to use SysConfig where it is available instead of using direct SW API calls. This will help simplify the SW application and also catch common mistakes early in the development cycle.
  • Option to select flash type based on board
  • Supported flash devices
    • S28HS512T

Features NOT Supported

NA

Important Usage Guidelines

  • Typically before writing to an offset, erase the block which corresponds to the offset
  • Flash writes can only be done to a page size aligned offset, otherwise the write API returns an error

Example Usage

Include the below file to access the APIs

#include <board/flash.h>

Flash Read API

uint32_t offset;
/* Set offset to read from */
offset = 0;
/* Do the read */
status = Flash_read(handle, offset, buffer, 100);

Flash Write API

uint32_t offset;
/* Set offset to write to */
offset = 0;
/* Do the write */
status = Flash_write(handle, offset, buffer, 100);

Flash Erase API

uint32_t offset, blk, page;
/* Set offset to erase */
offset = 0;
/* Find the block number corresponding to the offset */
status = Flash_offsetToBlkPage(handle, offset, &blk, &page);
/* Erase the block */
status = Flash_eraseBlk(handle,blk);

API

APIs for FLASH

status
uint32_t status
Definition: tisci_lpm.h:1
Flash_offsetToBlkPage
int32_t Flash_offsetToBlkPage(Flash_Handle handle, uint32_t offset, uint32_t *block, uint32_t *page)
Utility API to convert offset in bytes to (Block Num, Page Num)
SystemP_SUCCESS
#define SystemP_SUCCESS
Return status when the API execution was successful.
Definition: SystemP.h:56
DebugP_assert
#define DebugP_assert(expression)
Function to call for assert check.
Definition: DebugP.h:183
Flash_eraseBlk
int32_t Flash_eraseBlk(Flash_Handle handle, uint32_t blockNum)
Erase a block from flash.
Flash_write
int32_t Flash_write(Flash_Handle handle, uint32_t offset, uint8_t *buf, uint32_t len)
Write to flash.
flash.h
Flash_read
int32_t Flash_read(Flash_Handle handle, uint32_t offset, uint8_t *buf, uint32_t len)
Read data from flash.