![Logo](ti_logo.svg) |
AM273x MCU+ SDK
09.02.00
|
|
Go to the documentation of this file.
94 typedef struct Sdl_HWA_Status_t
156 #define SDL_HWA_ENABLE_STS (1U)
158 #define SDL_HWA_DISABLE_STS (0U)
160 #define SDL_HWA_DMEM_PARITY (1U)
162 #define SDL_HWA_DMEM_WINDOW_RAM_PARITY (2U)
164 #define SDL_HWA_DMEM_FSM_LOCKSTEP_INV_EN (3U)
166 #define SDL_HWA_DMEM_FSM_LOCKSTEP_EN (4U)
@ SDL_HWA_WINDOW_RAM_MEM_ID
Definition: sdl_ip_hwa.h:138
int32_t SDL_HWA_getMemblockBaseaddr(SDL_HWA_MemID memID, SDL_HWA_MemBlock memBlock, uint32_t *baseAddr)
This API is used to get the memory block base address.
uint8_t SDL_HWA_memoryInitStatus(SDL_HWA_MemBlock memBlock)
This API is used to check the initialize status.
void SDL_HWA_setParityEnableDisable(uint8_t memBlockParity, uint8_t enableSts)
This API is used to enable or disable the parity for memory block and lockstep logic.
void SDL_HWA_clearErrStatus(SDL_HWA_MemBlock memBlock)
This API is used to clear error status.
@ SDL_HWA_INVALID
Definition: sdl_ip_hwa.h:129
@ SDL_HWA_INVALID_ID
Definition: sdl_ip_hwa.h:140
@ SDL_HWA_DMA0_MEM_ID
Definition: sdl_ip_hwa.h:134
@ SDL_HWA_DMEM6
Definition: sdl_ip_hwa.h:121
@ SDL_HWA_WINDOW_RAM
Definition: sdl_ip_hwa.h:125
@ SDL_HWA_DMEM0
Definition: sdl_ip_hwa.h:109
int32_t SDL_HWA_getHwaEnableDisable(SDL_HWA_Status_s *pHWAStats)
This API is used to get enable/disable Radar Hardware Accelerator and respective clock.
uint8_t SDL_HWA_getErrStatus(SDL_HWA_MemBlock memBlock)
This API is used to get error status.
SDL_HWA_MemBlock
Definition: sdl_ip_hwa.h:108
@ SDL_HWA_DMEM7
Definition: sdl_ip_hwa.h:123
SDL_HWA_MemID
Definition: sdl_ip_hwa.h:133
uint8_t SDL_HWA_memoryInitDone(SDL_HWA_MemBlock memBlock)
This API is used to check the initialize done status.
@ SDL_HWA_DMEM1
Definition: sdl_ip_hwa.h:111
uint8_t SDL_HWA_enableHwaClkSTS
Definition: sdl_ip_hwa.h:97
uint8_t SDL_HWA_enableHwaSTS
Definition: sdl_ip_hwa.h:99
@ SDL_HWA_DMEM5
Definition: sdl_ip_hwa.h:119
uint8_t SDL_HWA_getParityErrMaskUnmask(SDL_HWA_MemBlock memBlock)
This API is used get mask/unmask parity error status.
@ SDL_HWA_FSM_LOCKSTEP
Definition: sdl_ip_hwa.h:127
@ SDL_HWA_DMEM3
Definition: sdl_ip_hwa.h:115
@ SDL_HWA_DMEM4
Definition: sdl_ip_hwa.h:117
Definition: sdl_ip_hwa.h:95
void SDL_HWA_setHwaEnableDisable(uint8_t enableSts)
This API is used to enable/disable Radar Hardware Accelerator and respective clock.
@ SDL_HWA_DMA1_MEM_ID
Definition: sdl_ip_hwa.h:136
uint8_t SDL_HWA_getParityStatus(uint8_t memBlockParity)
This API is used to get status for parity for memory block.
void SDL_HWA_setParityErrMaskUnmask(SDL_HWA_MemBlock memBlock, uint8_t enableSts)
This API is used to mask/unmask parity error status.
@ SDL_HWA_DMEM2
Definition: sdl_ip_hwa.h:113
void SDL_HWA_memoryInitStart(SDL_HWA_MemBlock memBlock)
This API is used to initialize the memory.