|
AM273x MCU+ SDK
09.02.00
|
|
Go to the documentation of this file.
50 #ifndef INCLUDE_SDL_COMMON_H_
51 #define INCLUDE_SDL_COMMON_H_
@ SDL_CCM_READ_REG_FAILURE
Definition: sdl_common.h:84
SDL_assertErrorNumber
Defines the different Assert error codes.
Definition: sdl_common.h:77
uint32_t SDL_getTime(void)
Application provided timestamp function This function will be called inside the reference function to...
@ SDL_ESM_INT_SRC_OUT_OF_BOUNDS
Definition: sdl_common.h:78
@ SDL_CCM_INTERRUPT_WITHOUT_ANY_ERROR
Definition: sdl_common.h:86
void SDL_assertExternalFunction(SDL_assertErrorNumber errorNumber)
Application provided external assert function Called inside the reference functions when unexpected c...
@ SDL_CCM_INVALID_INTERRUPT_SOURCE
Definition: sdl_common.h:90
@ SDL_CCM_CONFIG_REG_FAILURE
Definition: sdl_common.h:88
@ SDL_ECC_RAM_ID_NOT_FOUND
Definition: sdl_common.h:82
@ SDL_ECC_INTERRUPT_WITH_NOEVENT
Definition: sdl_common.h:80