C:/ti in Windows, and ${HOME}/ti in Linux. To install to other locations, refer Installing SDK at non-default location{some text} refers to a variable string that should be replaced by user and {some text} should not be typed verbatim on the command prompt.cmd.exe as command prompt and in Linux, use the bash shell as the command prompt.On successful completion of below steps, you would have achieved the following
| Term | Description |
|---|---|
| MibSPI Controller | MibSPI in communication which generates the clock and initiates the transfer |
| MibSPI Peripheral | MibSPI in communication which read and write data based on Controller clock |
| I2C Controller | I2C device generates the SCL clock and initiates communication |
| I2C Target | I2C device which responds to I2C Controller |
| LIN Commander | LIN device which intiates the transfer |
| LIN Responder | LIN device which responds to the transfer |
| PTP Sync Time Source | Ethernet device that periodically broadcasts the current time as a message to the other clocks |
| PTP Sync Receiver | Ethernet device that is waiting for the master to poll for data to actually send it |
Now you can explore the SDK by running more examples (see Examples and Demos) and browsing through various developer notes (see Developer Guides), to understand the SDK better and develop your own applications with the SDK.