Introduction
This example demonstrates how to perform STC for a given core.
This example displays:
* How to check if STC is Done for a Instance(CPU core).
* How to Run STC for the Instance (CPU core).
Use Cases
- STC run for DSP core after that it will run for R5F(Self Core).
Supported Combinations
| Parameter | Value |
| CPU + OS | r5fss0-0 nortos |
| Toolchain | ti-arm-clang |
| Board | am273x-evm |
| Example folder | examples/sdl/stc/stc_mcu/ |
Steps to Run the Example
See Also
STC
Sample Output
Shown below is a sample output when the application is run for R5F,
DSP STC Test Application started.
DSP STC Test should Pass & Completed.
If DSP STC test is successfull, DSP Core will be reset.
Wait for interrupt registration in DSP Core .
Interrupt registration in Done on DSP Core .
DSP Core is Reset.
DSP STC is done Successfully & Passed.
R5F STC Test Application started.
R5F STC Test should Pass & Completed.
If R5F STC test is successfull, Core will go in to Reset.
R5F Core is Reset.
R5F STC is done Successfully & Passed.
R5F STC Test Application started.
R5F STC Test should Fail & Completed.
If R5F STC test is successfull, Core will go in to Reset.
R5F Core is Reset.
R5F STC Test is Completed & failing.
Waiting in loop in STC_func_test_Main().