This example demonstrates the usage of the R5 PMU Driver. The PMU supports three event counters in additional to the cycle counter. So in total we could profile a block of code / or a function for four metrics. The cycle counter is a dedicated counter, but the other three are configurable for various PMU events. In this example, we configure the counters to count these events:
| Parameter | Value |
|---|---|
| CPU + OS | r5fss0-0 nortos |
| r5fss0-1 nortos | |
| Toolchain | ti-arm-clang |
| Boards | am273x-evm |
| Example folder | examples/drivers/pmu/pmu_multievent |
Shown below is a sample output when the application is run, Please note that application prints in both CCS and UART console.
UART Console: