AM273x MCU+ SDK  09.01.00
CBUFF

The CBUFF (Common Buffer Controller) driver provides API to configure the CBUFF Module. Below are the high level features supported by the CBUFF driver.

Features Supported

  • 128-bit device write-only interface over the EDMA writes user data to be sent over the LVDS interface
  • Packing of user data into RAW12/RAW14/RAW8 to send data formats DATA12/DATA14/DATA16, respectively.
  • SDR and DDR clocking modes.
  • Detection of erroneous incomplete transfer when the trigger for the next transfer is received.

Features NOT Supported

NA

Important Usage Guidelines

  • It is the responsiblity of the application to guarantee that the transfers in the CBUFF sessions do not overlap.

Example Usage

Include the below file to access the APIs

API

APIs for CBUFF