![Logo](ti_logo.svg) |
AM273x MCU+ SDK
08.06.00
|
|
Go to the documentation of this file.
60 #define SOC_DOMAIN_ID_MSS_TOP_RCM (0U)
61 #define SOC_DOMAIN_ID_MSS_RCM (1U)
62 #define SOC_DOMAIN_ID_DSS_RCM (2U)
63 #define SOC_DOMAIN_ID_RCSS_RCM (3U)
64 #define SOC_DOMAIN_ID_MSS_CTRL (4U)
65 #define SOC_DOMAIN_ID_DSS_CTRL (5U)
66 #define SOC_DOMAIN_ID_RCSS_CTRL (6U)
67 #define SOC_DOMAIN_ID_MSS_IOMUX (7U)
int32_t SOC_moduleSetClockFrequency(uint32_t moduleId, uint32_t clkId, uint64_t clkRate)
Set module clock to specified frequency.
void SOC_controlModuleUnlockMMR(uint32_t domainId, uint32_t partition)
Unlock control module partition to allow writes into control MMRs.
uint64_t SOC_virtToPhy(void *virtAddr)
SOC Virtual (CPU) to Physical address translation function.
void SOC_logAllClockHz(void)
Print's module clock info to the console.
void * SOC_phyToVirt(uint64_t phyAddr)
Physical to Virtual (CPU) address translation function.
uint64_t SOC_getSelfCpuClk(void)
Get the clock frequency in Hz of the CPU on which the driver is running.
void SOC_controlModuleLockMMR(uint32_t domainId, uint32_t partition)
Lock control module partition to prevent writes into control MMRs.
int32_t SOC_moduleClockEnable(uint32_t moduleId, uint32_t enable)
Enable clock to specified module.
const char * SOC_getCoreName(uint16_t coreId)
Convert a core ID to a user readable name.
void SOC_setEpwmTbClk(uint32_t epwmInstance, uint32_t enable)
Enable or disable ePWM time base clock from Control MMR.