AM273x MCU+ SDK  08.06.00
SDL ECC TCM

Introduction

This example demonstrates the usage of the SDL ECC TCM parity. The example shows how to setup and use the Parity Safety Diagnostic operation. This shows the TCM parity error injection.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
Toolchain ti-arm-clang
Board am273x-evm
Example folder examples/sdl/ecc/sdl_ecc_tcm_parity/

Steps to Run the Example

See Also

ECC : Error Correcting Code

Sample Output

Shown below is a sample output when the application is run,

Parity Example Application
TCM PARITY Example : Started
ESM_Test_init: Init MSS ESM complete
MSS TCM PARITY: ATCM0 Started
ESM Call back function called : instType 0x1, grpChannel 0x2, intSrc 0x3
Take action
MSS ATCM0 Parity : Completed
ESM_Test_init: Init MSS ESM complete
MSS TCM PARITY: ATCM1 Started
ESM Call back function called : instType 0x1, grpChannel 0x2, intSrc 0x6
Take action
MSS ATCM1 Parity : Completed
ESM_Test_init: Init MSS ESM complete
MSS TCM PARITY: B0TCM0 Started
ESM Call back function called : instType 0x1, grpChannel 0x2, intSrc 0x4
Take action
MSS B0TCM0 Parity : Completed
ESM_Test_init: Init MSS ESM complete
MSS TCM PARITY: B0TCM1 Started
ESM Call back function called : instType 0x1, grpChannel 0x2, intSrc 0x7
Take action
MSS B0TCM1 Parity : Completed
ESM_Test_init: Init MSS ESM complete
MSS TCM PARITY: B1TCM0 Started
ESM Call back function called : instType 0x1, grpChannel 0x2, intSrc 0x5
Take action
MSS B1TCM0 Parity : Completed
ESM_Test_init: Init MSS ESM complete
MSS TCM PARITY: B1TCM1 Started
ESM Call back function called : instType 0x1, grpChannel 0x2, intSrc 0x8
Take action
MSS B1TCM1 Parity : Completed
All tests have passed.