AM273x MCU+ SDK  08.06.00
SDL DSS ECC MAILBOX

Introduction

This example demonstrates the usage of the SDL DSS MAILBOX module. The example shows how to setup and use the ECC BUS Safety Diagnostic operation. Shows the generation of SEC and DED error on DSS MAILBOX ECC Aggregator.

Use Cases

Use Case Description
UC-1 Single bit error injection on DSS_MAILBOX.
UC-2 Double bit error injection on DSS_MAILBOX.

Supported Combinations

Parameter Value
CPU + OS c66ss0 nortos
Toolchain ti-c6000
Board am273x-evm
Example folder examples/sdl/ecc/sdl_dss_mailbox/

Steps to Run the Example

See Also

ECC : Error Correcting Code

Sample Output

Shown below is a sample output when the application is run,

ECC Example Application
ECC UC-1 and UC-2 Test
ECC_Test_init: Initialize of DSS ECC AGGR Memory is complete
ESM_Test_init: Init DSS ESM complete
ECC_Test_init: DSS ECC AGGR initialization is completed
ECC Safety Example tests: starting
DSS MAILBOX Single bit error inject: test starting
DSS MAILBOX Single bit error inject at pErrMem 0x83100000
Waiting for ESM Interrupt
UC-1: Injected 1-bit error and got ESM Interrupt
DSS MAILBOX Double bit error inject: starting
DSS MAILBOX Double bit error inject at pErrMem 0x83100000
Waiting for ESM Interrupt
UC-2: Injected 2-bit error and got ESM Interrupt
All Use_Cases have passed.