AM273x MCU+ SDK  08.06.00
DSP LIB Add32

Introduction

This example demonstrates the the usage of dsplib functions from MCU SDK. This is a ADD32 example taken from DSP LIB package itself to demonstrate building with the MCU SDK build system.

Supported Combinations

Parameter Value
CPU + OS c66ss0 nortos
Toolchain ti-c6000
Boards am273x-evm
Example folder examples/drivers/dsplib/add32

Steps to Run the Example

Sample Output

Shown below is a sample output when the application is run,

[DSPLIB] ADD32 Sample Application Started...
DSP_add32 Iter#: 1 Result Successful (r_i) NX = 8 natC: 112 optC: 39
DSP_add32 Iter#: 2 Result Successful (r_i) NX = 16 natC: 150 optC: 42
DSP_add32 Iter#: 3 Result Successful (r_i) NX = 32 natC: 292 optC: 62
DSP_add32 Iter#: 4 Result Successful (r_i) NX = 64 natC: 562 optC: 102
DSP_add32 Iter#: 5 Result Successful (r_i) NX = 128 natC: 1102 optC: 182
DSP_add32 Iter#: 6 Result Successful (r_i) NX = 256 natC: 2168 optC: 342
Memory: 8498912 bytes
Cycles: 5/4*Nx + 22
[DSPLIB] ADD32 Sample Application Completed!!
All tests have passed!!