AM273x MCU+ SDK  08.06.00
I2C

I2C module provides an interface to any I2C bus compatible device accessible via I2C serial bus. External components attached to I2C bus can serially transmit/receive data to/from the CPU through two wire interface. I2C driver provides API to perform transmit/receive to any of the I2C peripherals on the board, with the multiple modes of operation.

Features Supported

  • Controller and Target mode of operation
  • Interrupt, Polled Mode
  • Blocking and Non-blocking (callback) transfers
  • Queueing of I2C transactions
  • I2C Bus Recovery

SysConfig Features

Note
It is strongly recommend to use SysConfig where it is available instead of using direct SW API calls. This will help simplify the SW application and also catch common mistakes early in the development cycle.

SysConfig can be used to configure below parameters apart from common configuration like Clock,MPU,RAT and others.

  • I2C module configuration parmaters like bitrate, target addresses to probe.
  • I2C instances and pin configurations.
  • Interrupt mode enable option.If you disable it, configures to polling mode.
  • Based on above parameters, the SysConfig generated code does below as part of Drivers_open and Drivers_close functions
    • Set I2C instance parameter configuration.
    • Driver ISR registration if Interrupt Mode is enabled.

Features NOT Supported

  • Target mode is not supported in polling mode.

Important Usage Guidelines

NA

Example Usage

Include the below file to access the APIs

#include <drivers/i2c.h>

Instance Open Example

I2C_Params params;
I2C_Params_init(&params);
gI2cHandle = I2C_open(CONFIG_I2C0, &params);
if (!gI2cHandle) {
DebugP_assert(FALSE);
}

Instance Close Example

I2C_close(gI2cHandle);

I2c Transfer Example

int32_t status;
I2C_Transaction i2cTransaction;
I2C_Transaction_init(&i2cTransaction);
i2cTransaction.writeBuf = txBuffer;
i2cTransaction.writeCount = 1U;
i2cTransaction.readBuf = rxBuffer;
i2cTransaction.readCount = 2U;
status = I2C_transfer(gI2cHandle, &i2cTransaction);
if (SystemP_SUCCESS != status) {
DebugP_assert(FALSE);
}

API

APIs for I2C

I2C_transfer
int32_t I2C_transfer(I2C_Handle handle, I2C_Transaction *transaction)
Function to initiate a transfer from I2C.
I2C_close
void I2C_close(I2C_Handle handle)
Function to close the I2C.
I2C_Transaction::writeBuf
const void * writeBuf
Definition: i2c/v1/i2c.h:220
I2C_Transaction_init
void I2C_Transaction_init(I2C_Transaction *transaction)
Function to set default values of I2C_Transaction in transaction.
I2C_Transaction
I2C transaction.
Definition: i2c/v1/i2c.h:215
I2C_Params
I2C Parameters.
Definition: i2c/v1/i2c.h:279
I2C_open
I2C_Handle I2C_open(uint32_t idx, const I2C_Params *params)
Open the I2C at index idx with parameters params.
SystemP_SUCCESS
#define SystemP_SUCCESS
Return status when the API execution was successful.
Definition: SystemP.h:56
I2C_Transaction::readBuf
void * readBuf
Definition: i2c/v1/i2c.h:230
I2C_Transaction::writeCount
size_t writeCount
Definition: i2c/v1/i2c.h:225
I2C_Params_init
void I2C_Params_init(I2C_Params *params)
Function to set default values of I2C_Params in params.
I2C_Transaction::readCount
size_t readCount
Definition: i2c/v1/i2c.h:235
DebugP_assert
#define DebugP_assert(expression)
Function to call for assert check.
Definition: DebugP.h:177
i2c.h
I2C_init
void I2C_init(void)
Initialize the I2C module.
I2C_Params::transferMode
uint8_t transferMode
Definition: i2c/v1/i2c.h:281
I2C_MODE_BLOCKING
#define I2C_MODE_BLOCKING
Definition: i2c/v1/i2c.h:133