![Logo](ti_logo.svg) |
AM273x MCU+ SDK
08.05.00
|
|
Go to the documentation of this file.
62 #include "sdl_hwa_hw.h"
63 #include <sdl/hwa/v0/soc/sdl_hwa_soc.h>
SDL_HWA_MemBlock
This enumerator defines the HWA memories.
Definition: sdl_hwa_soc.h:64
void SDL_HWA_DMA0_secErrorClear(void)
This API is used to clear SEC error from DMA0.
@ SDL_HWA_FI_TYPE_INVALID
Definition: hwa/v0/sdl_hwa.h:91
@ SDL_HWA_FI_MAIN
Definition: hwa/v0/sdl_hwa.h:78
@ SDL_HWA_MAIN_CMD_INTERFACE
Definition: hwa/v0/sdl_hwa.h:87
int32_t SDL_HWA_fsmLockStepExecute(void)
This API is used to induce the error in the fsm lockstep for HWA.
SDL_HWA_busSftyFiRedType
Definition: hwa/v0/sdl_hwa.h:86
uint32_t SDL_HWA_DMA1_dedErrorStatus(void)
This API is used to get DED error status from DMA1.
int32_t SDL_HWA_DMA0_redExecute(SDL_HWA_busSftyFiType fiType, SDL_HWA_busSftyFiRedType redType)
This API is used for RED test on DMA0.
@ SDL_HWA_FI_SAFE
Definition: hwa/v0/sdl_hwa.h:79
void SDL_HWA_DMA0_dedErrorClear(void)
This API is used to clear DED error from DMA0.
void SDL_HWA_DMA1_dedExecute(void)
This API is used for DED test on DMA1.
void SDL_HWA_DMA1_redErrorClear(void)
This API is used to clear red error from DMA1.
void SDL_HWA_DMA0_dedExecute(void)
This API is used for DED test on DMA0.
int32_t SDL_HWA_DMA1_redExecute(SDL_HWA_busSftyFiType fiType, SDL_HWA_busSftyFiRedType redType)
This API is used for RED test on DMA1.
@ SDL_HWA_FI_INVALID
Definition: hwa/v0/sdl_hwa.h:82
uint32_t SDL_HWA_DMA0_dedErrorStatus(void)
This API is used to get DED error status from DMA0.
uint32_t SDL_HWA_DMA1_secErrorStatus(void)
This API is used to get SEC error status from DMA1.
void SDL_HWA_DMA0_redErrorClear(void)
This API is used to clear RED error from DMA0.
SDL_HWA_busSftyFiType
Definition: hwa/v0/sdl_hwa.h:77
uint32_t SDL_HWA_DMA1_redErrorStatus(void)
This API is used to get RED error status from DMA1.
@ SDL_HWA_FI_GLOBAL_MAIN
Definition: hwa/v0/sdl_hwa.h:80
SDL_HWA_MemID
This enumerator defines the HWA IDs.
Definition: sdl_hwa_soc.h:93
@ SDL_HWA_FI_GLOBAL_SAFE
Definition: hwa/v0/sdl_hwa.h:81
void SDL_HWA_DMA1_secExecute(void)
This API is used for SEC test on DMA1.
@ SDL_HWA_MAIN_WRITE_STATUS_INTERFACE
Definition: hwa/v0/sdl_hwa.h:89
void SDL_HWA_DMA1_dedErrorClear(void)
This API is used to clear DED error from DMA1.
uint32_t SDL_HWA_DMA0_secErrorStatus(void)
This API is used to get SEC error status from DMA0.
void SDL_HWA_DMA1_secErrorClear(void)
This API is used to clear SEC error from DMA1.
uint32_t SDL_HWA_DMA0_redErrorStatus(void)
This API is used to get RED error status from DMA0.
@ SDL_HWA_MAIN_WRITE_INTERFACE
Definition: hwa/v0/sdl_hwa.h:88
@ SDL_HWA_MAIN_READ_INTERFACE
Definition: hwa/v0/sdl_hwa.h:90
void SDL_HWA_DMA0_secExecute(void)
This API is used for SEC test on DMA0.
int32_t SDL_HWA_memParityExecute(SDL_HWA_MemID memID, SDL_HWA_MemBlock memBlock)
This API is used for configuring and testing parity of the HWA memory.