Introduction
This example demonstrates the usage of the MCRC module. The example shows how to setup and use the MCRC controller in the full mode of operation. Shows the generation of matching CRC as well as non-matching signature due to insertion of error in the block of information on which the CRC is being performed or in the signature provided to the PSA Signature Register (or both, depending on the mode).
Use Cases
Use Case | Description |
UC-1 | Full CPU-mode signature compute for Channel 1 and comparison against known value. |
UC-2 | Full CPU-mode signature compute for Channel 2 and comparison against known value. |
Supported Combinations
Parameter | Value |
CPU + OS | r5fss0-0 nortos, c66ss0 nortos |
Toolchain | ti-arm-clang, ti-c6000 |
Board | am273x-evm |
Example folder | examples/sdl/mcrc/mcrc_auto_cpu/ |
Steps to Run the Example
See Also
MCRC
Sample Output
MCRC Application
MCRC FULL CPU mode : starting
Full_CPU mode MCRC signature verification done successfull
MCRC FULL CPU mode : starting
Full_CPU mode MCRC signature verification done successful
Applications Name: MCRC_fullCPU_mode PASSED