This example demonstrates the usage of the SDL MBOX module. The example shows how to setup and use the ECC BUS Safety Diagnostic operation. Shows the generation of SEC, DED and RED error on MSS MBOX, DSS MBOX and RSS MBOX
Note : SEC - Single Error Correction, DED - Double Error Correction, RED - Redundancy Error Correction
AM263x : Supports MSS MBOX AM273X : Supports MSS MBOX and DSS MBOX AWR294x : Supports MSS MBOX, DSS MBOX and RSS MBOX
Use Case | Description |
---|---|
UC-1 | SEC Error insertion on RSS MBOX. |
UC-2 | DED Error insertion on RSS MBOX. |
UC-3 | RED Error insertion on RSS MBOX. |
Use Case | Description |
---|---|
UC-1 | SEC Error insertion on DSS MBOX. |
UC-2 | DED Error insertion on DSS MBOX. |
UC-3 | RED Error insertion on DSS MBOX. |
UC-4 | SEC Error insertion on RSS MBOX. |
UC-5 | DED Error insertion on RSS MBOX. |
UC-6 | RED Error insertion on RSS MBOX. |
Shown below is a sample output when the application is run on On R5F Core,
Shown below is a sample output when the application is run on On C66 Core,