Introduction
This example demonstrates the usage of the SDL ECC BUS SAFETY module. The example shows how to setup and use the ECC BUS Safety Diagnostic operation. Shows the generation of SEC, DED and RED error on all MSS DSS and RSS nodes
Note
Note :
- SEC - Single Error Correction, DED - Double Error Correction, RED - Redundancy Error Correction.
- DSS Nodes are applicable to AWR294X and AM273X.
AM263x : Supports MSS Nodes. (MSS_CR5C_AHB, MSS_CR5D_AHB , MSS_CR5C_AXI & MSS_CR5D_AXI)\ AM273X : Supports MSS Nodes,DSS Nodes and RSS Nodes.\ AWR294x : Supports MSS Nodes,DSS Nodes and RSS Nodes.\
MSS Nodes Supported :
- MSS_TPTC_A0_RD
- MSS_TPTC_A1_RD
- MSS_TPTC_B0_RD
- MSS_TPTC_A0_WR
- MSS_TPTC_A1_WR
- MSS_TPTC_B0_WR
- MSS_CR5A_AHB
- MSS_CR5B_AHB
- MSS_CR5C_AHB
- MSS_CR5D_AHB
- MSS_MBOX
- MSS_CR5A_AXI_WR
- MSS_CR5B_AXI_WR
- MSS_CR5C_AXI_WR
- MSS_CR5D_AXI_WR
- MSS_CR5A_AXI_RD
- MSS_CR5B_AXI_RD
- MSS_CR5C_AXI_RD
- MSS_CR5D_AXI_RD
- MSS_CR5A_AXI_S
- MSS_CR5B_AXI_S
- MSS_CR5C_AXI_S
- MSS_CR5D_AXI_S
DSS Nodes Supported :
- DSS_DSP_MDMA
- DSS_L3_BANKA
- DSS_L3_BANKB
- DSS_L3_BANKC
- DSS_L3_BANKD
- DSS_DSP_SDMA
- DSS_TPTC_A0_RD
- DSS_TPTC_A1_RD
- DSS_TPTC_B0_RD
- DSS_TPTC_B1_RD
- DSS_TPTC_C0_RD
- DSS_TPTC_C1_RD
- DSS_TPTC_C2_RD
- DSS_TPTC_C3_RD
- DSS_TPTC_C4_RD
- DSS_TPTC_C5_RD
- DSS_TPTC_A0_WR
- DSS_TPTC_A1_WR
- DSS_TPTC_B0_WR
- DSS_TPTC_B1_WR
- DSS_TPTC_C0_WR
- DSS_TPTC_C1_WR
- DSS_TPTC_C2_WR
- DSS_TPTC_C3_WR
- DSS_TPTC_C4_WR
- DSS_TPTC_C5_WR
- DSS_CBUFF_FIFO
- DSS_MCRC
- DSS_PCR
- DSS_HWA_DMA0
- DSS_HWA_DMA1
- DSS_MBOX
- RSS_ADCBUF_RD applicable only for AWR294X
- RSS_ADCBUF_WR applicable only for AWR294X
- RSS_MBOX applicable only for AWR294X
Use Cases On AM263X in R5 Core
Use Case | Description |
UC-1 | CR5A_AHB_RED_Test in INTERRUPT Method. |
UC-2 | CR5B_AHB_RED_Test in INTERRUPT Method. |
UC-3 | CR5C_AHB_RED_Test in INTERRUPT Method. |
UC-4 | CR5D_AHB_RED_Test in INTERRUPT Method. |
UC-5 | TPTC_A0_WR_RED_Test in Interrupt Method. |
UC-6 | TPTC_A1_WR_RED_Test in Interrupt Method. |
UC-7 | TPTC_A0_RD_SEC_Test in Interrupt Method. |
UC-8 | TPTC_A0_RD_DED_Test in Interrupt Method. |
UC-9 | TPTC_A0_RD_RED_Test in Interrupt Method. |
UC-10 | TPTC_A1_RD_SEC_Test in Interrupt Method. |
UC-11 | TPTC_A1_RD_DED_Test in Interrupt Method. |
UC-12 | TPTC_A1_RD_RED_Test in Interrupt Method. |
UC-13 | MSS_CR5A_AXI_WR_RED_Test in Interrupt Method. |
UC-14 | MSS_CR5B_AXI_WR_RED_Test in Interrupt Method. |
UC-15 | MSS_CR5C_AXI_WR_RED_Test in Interrupt Method. |
UC-16 | MSS_CR5D_AXI_WR_RED_Test in Interrupt Method. |
UC-17 | MSS_CR5A_AXI_RD_SEC_Test in Interrupt Method. |
UC-18 | MSS_CR5A_AXI_RD_RED_Test in Interrupt Method. |
UC-19 | MSS_CR5B_AXI_RD_SEC_Test in Interrupt Method. |
UC-20 | MSS_CR5B_AXI_RD_RED_Test in Interrupt Method. |
UC-21 | MSS_CR5C_AXI_RD_SEC_Test in Interrupt Method. |
UC-22 | MSS_CR5C_AXI_RD_RED_Test in Interrupt Method. |
UC-23 | MSS_CR5D_AXI_RD_SEC_Test in Interrupt Method. |
UC-24 | MSS_CR5D_AXI_RD_RED_Test in Interrupt Method. |
UC-25 | MSS_CR5A_AXI_S_SEC_Test in Interrupt Method. |
UC-26 | MSS_CR5A_AXI_S_RED_Test in Interrupt Method. |
UC-27 | MSS_CR5B_AXI_S_SEC_Test in Interrupt Method. |
UC-28 | MSS_CR5B_AXI_S_RED_Test in Interrupt Method. |
UC-29 | MSS_CR5C_AXI_S_SEC_Test in Interrupt Method. |
UC-30 | MSS_CR5C_AXI_S_RED_Test in Interrupt Method. |
UC-31 | MSS_CR5D_AXI_S_SEC_Test in Interrupt Method. |
UC-32 | MSS_CR5D_AXI_S_RED_Test in Interrupt Method. |
Use Cases On AM273X in R5 Core
Use Case | Description |
UC-1 | CR5A_AHB_RED_Test in INTERRUPT Method. |
UC-2 | CR5B_AHB_RED_Test in INTERRUPT Method. |
UC-3 | TPTC_A0_WR_RED_Test in Interrupt Method. |
UC-4 | TPTC_A1_WR_RED_Test in Interrupt Method. |
UC-5 | TPTC_B0_WR_RED_Test in Interrupt Method. |
UC-6 | TPTC_A0_RD_SEC_Test in Interrupt Method. |
UC-7 | TPTC_A0_RD_DED_Test in Interrupt Method. |
UC-8 | TPTC_A0_RD_RED_Test in Interrupt Method. |
UC-9 | TPTC_A1_RD_SEC_Test in Interrupt Method. |
UC-10 | TPTC_A1_RD_DED_Test in Interrupt Method. |
UC-11 | TPTC_A1_RD_RED_Test in Interrupt Method. |
UC-12 | TPTC_B0_RD_SEC_Test in Interrupt Method. |
UC-13 | TPTC_B0_RD_DED_Test in Interrupt Method. |
UC-14 | TPTC_B0_RD_RED_Test in Interrupt Method. |
UC-15 | MSS_CR5A_AXI_WR_RED_Test in Interrupt Method. |
UC-16 | MSS_CR5B_AXI_WR_RED_Test in Interrupt Method. |
UC-17 | MSS_CR5A_AXI_RD_SEC_Test in Interrupt Method. |
UC-18 | MSS_CR5A_AXI_RD_RED_Test in Interrupt Method. |
UC-19 | MSS_CR5B_AXI_RD_SEC_Test in Interrupt Method. |
UC-20 | MSS_CR5B_AXI_RD_RED_Test in Interrupt Method. |
UC-21 | MSS_CR5A_AXI_S_SEC_Test in Interrupt Method. |
UC-22 | MSS_CR5A_AXI_S_RED_Test in Interrupt Method. |
UC-23 | MSS_CR5B_AXI_S_SEC_Test in Interrupt Method. |
UC-24 | MSS_CR5B_AXI_S_RED_Test in Interrupt Method. |
UC-25 | MSS_MBOX_SEC_Test in Interrupt Method. |
UC-26 | MSS_MBOX_DED_Test in Interrupt Method. |
UC-27 | MSS_MBOX_RED_Test in Interrupt Method. |
Use Cases On AWR294X in R5 Core
Use Case | Description |
UC-1 | CR5A_AHB_RED_Test in INTERRUPT Method. |
UC-2 | CR5B_AHB_RED_Test in INTERRUPT Method. |
UC-3 | TPTC_A0_WR_RED_Test in Interrupt Method. |
UC-4 | TPTC_A1_WR_RED_Test in Interrupt Method. |
UC-5 | TPTC_B0_WR_RED_Test in Interrupt Method. |
UC-6 | TPTC_A0_RD_SEC_Test in Interrupt Method. |
UC-7 | TPTC_A0_RD_DED_Test in Interrupt Method. |
UC-8 | TPTC_A0_RD_RED_Test in Interrupt Method. |
UC-9 | TPTC_A1_RD_SEC_Test in Interrupt Method. |
UC-10 | TPTC_A1_RD_DED_Test in Interrupt Method. |
UC-11 | TPTC_A1_RD_RED_Test in Interrupt Method. |
UC-12 | TPTC_B0_RD_SEC_Test in Interrupt Method. |
UC-13 | TPTC_B0_RD_DED_Test in Interrupt Method. |
UC-14 | TPTC_B0_RD_RED_Test in Interrupt Method. |
UC-15 | MSS_CR5A_AXI_WR_RED_Test in Interrupt Method. |
UC-16 | MSS_CR5B_AXI_WR_RED_Test in Interrupt Method. |
UC-17 | MSS_CR5A_AXI_RD_SEC_Test in Interrupt Method. |
UC-18 | MSS_CR5A_AXI_RD_RED_Test in Interrupt Method. |
UC-19 | MSS_CR5B_AXI_RD_SEC_Test in Interrupt Method. |
UC-20 | MSS_CR5B_AXI_RD_RED_Test in Interrupt Method. |
UC-21 | MSS_CR5A_AXI_S_SEC_Test in Interrupt Method. |
UC-22 | MSS_CR5A_AXI_S_RED_Test in Interrupt Method. |
UC-23 | MSS_CR5B_AXI_S_SEC_Test in Interrupt Method. |
UC-24 | MSS_CR5B_AXI_S_RED_Test in Interrupt Method. |
UC-25 | MSS_MBOX_SEC_Test in Interrupt Method. |
UC-26 | MSS_MBOX_DED_Test in Interrupt Method. |
UC-27 | MSS_MBOX_RED_Test in Interrupt Method. |
Use Cases On AWR294X in C66 Core
Use Case | Description |
UC-1 | MCRC_SEC_Test in Interrupt Method |
UC-2 | MCRC_DED_Test in Interrupt Method. |
UC-3 | MCRC_RED_Test in Interrupt Method. |
UC-4 | DSS_L3_BANKA_SEC_Test in Interrupt Method. |
UC-5 | DSS_L3_BANKA_DED_Test in Interrupt Method. |
UC-6 | DSS_L3_BANKA_RED_Test in Interrupt Method. |
UC-7 | DSS_L3_BANKB_SEC_Test in Interrupt Method. |
UC-8 | DSS_L3_BANKB_DED_Test in Interrupt Method. |
UC-9 | DSS_L3_BANKB_RED_Test in Interrupt Method. |
UC-10 | DSS_L3_BANKC_SEC_Test in Interrupt Method. |
UC-11 | DSS_L3_BANKC_DED_Test in Interrupt Method. |
UC-12 | DSS_L3_BANKC_RED_Test in Interrupt Method. |
UC-13 | DSS_L3_BANKD_SEC_Test in Interrupt Method. |
UC-14 | DSS_L3_BANKD_DED_Test in Interrupt Method. |
UC-15 | DSS_L3_BANKD_RED_Test in Interrupt Method. |
UC-16 | DSS_HWA_DMA0_SEC_Test in Interrupt Method. |
UC-17 | DSS_HWA_DMA0_DED_Test in Interrupt Method. |
UC-18 | DSS_HWA_DMA0_RED_Test in Interrupt Method. |
UC-19 | DSS_HWA_DMA1_SEC_Test in Interrupt Method. |
UC-20 | DSS_HWA_DMA1_DED_Test in Interrupt Method. |
UC-21 | DSS_HWA_DMA1_RED_Test in Interrupt Method. |
UC-22 | DSS_MBOX_SEC_Test in Interrupt Method. |
UC-23 | DSS_MBOX_DED_Test in Interrupt Method. |
UC-24 | DSS_MBOX_RED_Test in Interrupt Method. |
UC-25 | CBUFF_FIFO_SEC_Test in Interrupt Method. |
UC-26 | CBUFF_FIFO_DED_Test in Interrupt Method. |
UC-27 | CBUFF_FIFO_RED_Test in Interrupt Method. |
UC-28 | TPTC_A0_WR_RED_Test in Interrupt Method. |
UC-29 | TPTC_A1_WR_RED_Test in Interrupt Method. |
UC-30 | TPTC_B0_WR_RED_Test in Interrupt Method. |
UC-31 | TPTC_B1_WR_RED_Test in Interrupt Method. |
UC-32 | TPTC_C0_WR_RED_Test in Interrupt Method. |
UC-33 | TPTC_C1_WR_RED_Test in Interrupt Method. |
UC-34 | TPTC_C2_WR_RED_Test in Interrupt Method. |
UC-35 | TPTC_C3_WR_RED_Test in Interrupt Method. |
UC-36 | TPTC_C4_WR_RED_Test in Interrupt Method. |
UC-37 | TPTC_C5_WR_RED_Test in Interrupt Method. |
UC-38 | TPTC_A0_RD_SEC_Test in Interrupt Method. |
UC-39 | TPTC_A0_RD_DED_Test in Interrupt Method. |
UC-40 | TPTC_A0_RD_RED_Test in Interrupt Method. |
UC-41 | TPTC_A1_RD_SEC_Test in Interrupt Method. |
UC-42 | TPTC_A1_RD_DED_Test in Interrupt Method. |
UC-43 | TPTC_A1_RD_RED_Test in Interrupt Method. |
UC-44 | TPTC_B0_RD_SEC_Test in Interrupt Method. |
UC-45 | TPTC_B0_RD_DED_Test in Interrupt Method. |
UC-46 | TPTC_B0_RD_RED_Test in Interrupt Method. |
UC-47 | TPTC_B1_RD_SEC_Test in Interrupt Method. |
UC-48 | TPTC_B1_RD_DED_Test in Interrupt Method. |
UC-49 | TPTC_B1_RD_RED_Test in Interrupt Method. |
UC-50 | TPTC_C0_RD_SEC_Test in Interrupt Method. |
UC-51 | TPTC_C0_RD_DED_Test in Interrupt Method. |
UC-52 | TPTC_C0_RD_RED_Test in Interrupt Method. |
UC-53 | TPTC_C1_RD_SEC_Test in Interrupt Method. |
UC-54 | TPTC_C1_RD_DED_Test in Interrupt Method. |
UC-55 | TPTC_C1_RD_RED_Test in Interrupt Method |
UC-56 | TPTC_C2_RD_SEC_Test in Interrupt Method. |
UC-57 | TPTC_C2_RD_DED_Test in Interrupt Method. |
UC-58 | TPTC_C2_RD_RED_Test in Interrupt Method |
UC-59 | TPTC_C3_RD_SEC_Test in Interrupt Method. |
UC-60 | TPTC_C3_RD_DED_Test in Interrupt Method. |
UC-61 | TPTC_C3_RD_RED_Test in Interrupt Method |
UC-62 | TPTC_C4_RD_SEC_Test in Interrupt Method. |
UC-63 | TPTC_C4_RD_DED_Test in Interrupt Method. |
UC-64 | TPTC_C4_RD_RED_Test in Interrupt Method. |
UC-65 | TPTC_C5_RD_SEC_Test in Interrupt Method. |
UC-67 | TPTC_C5_RD_DED_Test in Interrupt Method. |
UC-68 | TPTC_C5_RD_RED_Test in Interrupt Method. |
UC-69 | PCR_SEC_Test in Interrupt Method. |
UC-70 | PCR_RED_Test in Interrupt Method. |
UC-71 | PCR_RED_Test in Interrupt Method. |
UC-72 | DSP_SDMA_SEC_Test in Interrupt Method. |
UC-73 | DSP_SDMA_DED_Test in Interrupt Method. |
UC-74 | DSP_SDMA_RED_Test in Interrupt Method. |
UC-75 | DSP_MDMA_RED_Test in Interrupt Method. |
UC-76 | RSS_MBOX_SEC_Test in Interrupt Method. |
UC-77 | RSS_MBOX_DED_Test in Interrupt Method. |
UC-78 | RSS_MBOX_RED_Test in Interrupt Method. |
UC-79 | RSS_ADCBUF_RD_RED_Test in Interrupt Method. |
UC-80 | RSS_ADCBUF_WR_SEC_Test in Interrupt Method. |
UC-81 | RSS_ADCBUF_WR_DED_Test in Interrupt Method. |
UC-82 | RSS_ADCBUF_WR_RED_Test in Interrupt Method. |
Use Cases On AM273X in C66 Core
Use Case | Description |
UC-1 | MDO_FIFO_DED_Test in Polling Method. |
UC-2 | MDO_FIFO_RED_Test in Polling Method. |
UC-3 | MCRC_SEC_Test in Interrupt Method |
UC-4 | MCRC_DED_Test in Interrupt Method. |
UC-5 | MCRC_RED_Test in Interrupt Method. |
UC-6 | DSS_L3_BANKA_SEC_Test in Interrupt Method. |
UC-7 | DSS_L3_BANKA_DED_Test in Interrupt Method. |
UC-8 | DSS_L3_BANKA_RED_Test in Interrupt Method. |
UC-9 | DSS_L3_BANKB_SEC_Test in Interrupt Method. |
UC-10 | DSS_L3_BANKB_DED_Test in Interrupt Method. |
UC-11 | DSS_L3_BANKB_RED_Test in Interrupt Method. |
UC-12 | DSS_L3_BANKC_SEC_Test in Interrupt Method. |
UC-13 | DSS_L3_BANKC_DED_Test in Interrupt Method. |
UC-14 | DSS_L3_BANKC_RED_Test in Interrupt Method. |
UC-15 | DSS_L3_BANKD_SEC_Test in Interrupt Method. |
UC-16 | DSS_L3_BANKD_DED_Test in Interrupt Method. |
UC-17 | DSS_L3_BANKD_RED_Test in Interrupt Method. |
UC-18 | DSS_HWA_DMA0_SEC_Test in Interrupt Method. |
UC-19 | DSS_HWA_DMA0_DED_Test in Interrupt Method. |
UC-20 | DSS_HWA_DMA0_RED_Test in Interrupt Method. |
UC-21 | DSS_HWA_DMA1_SEC_Test in Interrupt Method. |
UC-22 | DSS_HWA_DMA1_DED_Test in Interrupt Method. |
UC-23 | DSS_HWA_DMA1_RED_Test in Interrupt Method. |
UC-24 | DSS_MBOX_SEC_Test in Interrupt Method. |
UC-25 | DSS_MBOX_DED_Test in Interrupt Method. |
UC-26 | DSS_MBOX_RED_Test in Interrupt Method. |
UC-29 | CBUFF_FIFO_SEC_Test in Interrupt Method. |
UC-30 | CBUFF_FIFO_DED_Test in Interrupt Method. |
UC-31 | CBUFF_FIFO_RED_Test in Interrupt Method. |
UC-32 | TPTC_A0_WR_RED_Test in Interrupt Method. |
UC-33 | TPTC_A1_WR_RED_Test in Interrupt Method. |
UC-32 | TPTC_B0_WR_RED_Test in Interrupt Method. |
UC-33 | TPTC_B1_WR_RED_Test in Interrupt Method. |
UC-34 | TPTC_C0_WR_RED_Test in Interrupt Method. |
UC-35 | TPTC_C1_WR_RED_Test in Interrupt Method. |
UC-36 | TPTC_C2_WR_RED_Test in Interrupt Method. |
UC-37 | TPTC_C3_WR_RED_Test in Interrupt Method. |
UC-38 | TPTC_C4_WR_RED_Test in Interrupt Method. |
UC-39 | TPTC_C5_WR_RED_Test in Interrupt Method. |
UC-40 | TPTC_A0_RD_SEC_Test in Interrupt Method. |
UC-41 | TPTC_A0_RD_DED_Test in Interrupt Method. |
UC-42 | TPTC_A0_RD_RED_Test in Interrupt Method. |
UC-43 | TPTC_A1_RD_SEC_Test in Interrupt Method. |
UC-44 | TPTC_A1_RD_DED_Test in Interrupt Method. |
UC-45 | TPTC_A1_RD_RED_Test in Interrupt Method. |
UC-46 | TPTC_B0_RD_SEC_Test in Interrupt Method. |
UC-47 | TPTC_B0_RD_DED_Test in Interrupt Method. |
UC-48 | TPTC_B0_RD_RED_Test in Interrupt Method. |
UC-49 | TPTC_B1_RD_SEC_Test in Interrupt Method. |
UC-50 | TPTC_B1_RD_DED_Test in Interrupt Method. |
UC-51 | TPTC_B1_RD_RED_Test in Interrupt Method. |
UC-52 | TPTC_C0_RD_SEC_Test in Interrupt Method. |
UC-53 | TPTC_C0_RD_DED_Test in Interrupt Method. |
UC-54 | TPTC_C0_RD_RED_Test in Interrupt Method. |
UC-55 | TPTC_C1_RD_SEC_Test in Interrupt Method. |
UC-56 | TPTC_C1_RD_DED_Test in Interrupt Method. |
UC-57 | TPTC_C1_RD_RED_Test in Interrupt Method |
UC-58 | TPTC_C2_RD_SEC_Test in Interrupt Method. |
UC-59 | TPTC_C2_RD_DED_Test in Interrupt Method. |
UC-60 | TPTC_C2_RD_RED_Test in Interrupt Method |
UC-61 | TPTC_C3_RD_SEC_Test in Interrupt Method. |
UC-62 | TPTC_C3_RD_DED_Test in Interrupt Method. |
UC-63 | TPTC_C3_RD_RED_Test in Interrupt Method |
UC-64 | TPTC_C4_RD_SEC_Test in Interrupt Method. |
UC-65 | TPTC_C4_RD_DED_Test in Interrupt Method. |
UC-66 | TPTC_C4_RD_RED_Test in Interrupt Method |
UC-67 | TPTC_C5_RD_SEC_Test in Interrupt Method. |
UC-68 | TPTC_C5_RD_DED_Test in Interrupt Method. |
UC-69 | TPTC_C5_RD_RED_Test in Interrupt Method |
UC-70 | PCR_SEC_Test in Interrupt Method. |
UC-71 | PCR_RED_Test in Interrupt Method. |
UC-72 | PCR_RED_Test in Interrupt Method. |
UC-73 | DSP_SDMA_SEC_Test in Interrupt Method. |
UC-74 | DSP_SDMA_DED_Test in Interrupt Method. |
UC-75 | DSP_SDMA_RED_Test in Interrupt Method. |
UC-76 | DSP_MDMA_RED_Test in Interrupt Method. |
UC-77 | MDO_FIFO_SEC_Test in Interrupt Method. |
Supported Combinations
Steps to Run the Example
See Also
ECC BUS SAFETY
Sample Output
Shown below is a sample output when the application is run on AM263X in R5 Core,
ECC BUS SAFETY Application
ECC BUS SAFETY TEST START : starting
Applications Name: CR5A_AHB_RED_Test in INTERRUPT Method PASSED and Time taken for the Test is 150 micro secs
Applications Name: CR5B_AHB_RED_Test in INTERRUPT Method PASSED and Time taken for the Test is 140 micro secs
Applications Name: CR5C_AHB_RED_Test in INTERRUPT Method PASSED and Time taken for the Test is 140 micro secs
Applications Name: CR5D_AHB_RED_Test in INTERRUPT Method PASSED and Time taken for the Test is 139 micro secs
Applications Name: TPTC_A0_WR_RED_Test in Interrupt Method PASSED and Time taken for the Test is 105 micro secs
Applications Name: TPTC_A1_WR_RED_Test in Interrupt Method PASSED and Time taken for the Test is 102 micro secs
Applications Name: TPTC_A0_RD_SEC_Test in Interrupt Method PASSED and Time taken for the Test is 127 micro secs
Applications Name: TPTC_A0_RD_DED_Test in Interrupt Method PASSED and Time taken for the Test is 126 micro secs
Applications Name: TPTC_A0_RD_RED_Test in Interrupt Method PASSED and Time taken for the Test is 107 micro secs
Applications Name: TPTC_A1_RD_SEC_Test in Interrupt Method PASSED and Time taken for the Test is 121 micro secs
Applications Name: TPTC_A1_RD_DED_Test in Interrupt Method PASSED and Time taken for the Test is 123 micro secs
Applications Name: TPTC_A1_RD_RED_Test in Interrupt Method PASSED and Time taken for the Test is 106 micro secs
Applications Name: MSS_CR5A_AXI_WR_RED_Test in INTERRUPT Method PASSED and Time taken for the Test is 106 micro secs
Applications Name: MSS_CR5B_AXI_WR_RED_Test in INTERRUPT Method PASSED and Time taken for the Test is 102 micro secs
Applications Name: MSS_CR5C_AXI_WR_RED_Test in INTERRUPT Method PASSED and Time taken for the Test is 102 micro secs
Applications Name: MSS_CR5D_AXI_WR_RED_Test in INTERRUPT Method PASSED and Time taken for the Test is 102 micro secs
Applications Name: MSS_CR5A_AXI_RD_SEC_Test in INTERRUPT Method PASSED and Time taken for the Test is 104 micro secs
Applications Name: MSS_CR5A_AXI_RD_RED_Test in INTERRUPT Method PASSED and Time taken for the Test is 102 micro secs
Applications Name: MSS_CR5B_AXI_RD_SEC_Test in INTERRUPT Method PASSED and Time taken for the Test is 103 micro secs
Applications Name: MSS_CR5B_AXI_RD_RED_Test in INTERRUPT Method PASSED and Time taken for the Test is 101 micro secs
Applications Name: MSS_CR5C_AXI_RD_SEC_Test in INTERRUPT Method PASSED and Time taken for the Test is 102 micro secs
Applications Name: MSS_CR5C_AXI_RD_RED_Test in INTERRUPT Method PASSED and Time taken for the Test is 102 micro secs
Applications Name: MSS_CR5D_AXI_RD_SEC_Test in INTERRUPT Method PASSED and Time taken for the Test is 105 micro secs
Applications Name: MSS_CR5D_AXI_RD_RED_Test in INTERRUPT Method PASSED and Time taken for the Test is 102 micro secs
Applications Name: MSS_CR5A_AXI_S_SEC_Test in INTERRUPT Method PASSED and Time taken for the Test is 102 micro secs
Applications Name: MSS_CR5A_AXI_S_RED_Test in INTERRUPT Method PASSED and Time taken for the Test is 101 micro secs
Applications Name: MSS_CR5B_AXI_S_SEC_Test in INTERRUPT Method PASSED and Time taken for the Test is 103 micro secs
Applications Name: MSS_CR5B_AXI_S_RED_Test in INTERRUPT Method PASSED and Time taken for the Test is 102 micro secs
Applications Name: MSS_CR5C_AXI_S_SEC_Test in INTERRUPT Method PASSED and Time taken for the Test is 103 micro secs
Applications Name: MSS_CR5C_AXI_S_RED_Test in INTERRUPT Method PASSED and Time taken for the Test is 102 micro secs
Applications Name: MSS_CR5D_AXI_S_SEC_Test in INTERRUPT Method PASSED and Time taken for the Test is 103 micro secs
Applications Name: MSS_CR5D_AXI_S_RED_Test in INTERRUPT Method PASSED and Time taken for the Test is 103 micro secs
All tests have passed
Shown below is a sample output when the application is run on AWR294X in R5 Core,
[Cortex_R5_0]
ECC BUS SAFETY Application
ECC BUS SAFETY TEST START : starting
Applications Name: CR5A_AHB_RED_Test in INTERRUPT Method PASSED and Time taken for the Test is 31 micro secs
Applications Name: CR5B_AHB_RED_Test in INTERRUPT Method PASSED and Time taken for the Test is 24 micro secs
Applications Name: TPTC_A0_WR_RED_Test in Interrupt Method PASSED and Time taken for the Test is 23 micro secs
Applications Name: TPTC_A1_WR_RED_Test in Interrupt Method PASSED and Time taken for the Test is 22 micro secs
Applications Name: TPTC_B0_WR_RED_Test in Interrupt Method PASSED and Time taken for the Test is 22 micro secs
Applications Name: TPTC_A0_RD_SEC_Test in Interrupt Method PASSED and Time taken for the Test is 57 micro secs
Applications Name: TPTC_A0_RD_DED_Test in Interrupt Method PASSED and Time taken for the Test is 49 micro secs
Applications Name: TPTC_A0_RD_RED_Test in Interrupt Method PASSED and Time taken for the Test is 26 micro secs
Applications Name: TPTC_A1_RD_SEC_Test in Interrupt Method PASSED and Time taken for the Test is 49 micro secs
Applications Name: TPTC_A1_RD_DED_Test in Interrupt Method PASSED and Time taken for the Test is 48 micro secs
Applications Name: TPTC_A1_RD_RED_Test in Interrupt Method PASSED and Time taken for the Test is 25 micro secs
Applications Name: TPTC_B0_RD_SEC_Test in Interrupt Method PASSED and Time taken for the Test is 49 micro secs
Applications Name: TPTC_B0_RD_DED_Test in Interrupt Method PASSED and Time taken for the Test is 46 micro secs
Applications Name: TPTC_B0_RD_RED_Test in Interrupt Method PASSED and Time taken for the Test is 25 micro secs
Applications Name: MSS_CR5A_AXI_WR_RED_Test in INTERRUPT Method PASSED and Time taken for the Test is 17 micro secs
Applications Name: MSS_CR5B_AXI_WR_RED_Test in INTERRUPT Method PASSED and Time taken for the Test is 17 micro secs
Applications Name: MSS_CR5A_AXI_RD_SEC_Test in INTERRUPT Method PASSED and Time taken for the Test is 22 micro secs
Applications Name: MSS_CR5A_AXI_RD_RED_Test in INTERRUPT Method PASSED and Time taken for the Test is 16 micro secs
Applications Name: MSS_CR5B_AXI_RD_SEC_Test in INTERRUPT Method PASSED and Time taken for the Test is 22 micro secs
Applications Name: MSS_CR5B_AXI_RD_RED_Test in INTERRUPT Method PASSED and Time taken for the Test is 16 micro secs
Applications Name: MSS_CR5A_AXI_S_RED_Test in INTERRUPT Method PASSED and Time taken for the Test is 17 micro secs
Applications Name: MSS_CR5B_AXI_S_RED_Test in INTERRUPT Method PASSED and Time taken for the Test is 17 micro secs
All tests have passed
Shown below is a sample output when the application is run on AM273X in R5 Core,
[Cortex_R5_0]
ECC BUS SAFETY Application
ECC BUS SAFETY TEST START : starting
Applications Name: CR5A_AHB_RED_Test in INTERRUPT Method PASSED and Time taken for the Test is 31 micro secs
Applications Name: CR5B_AHB_RED_Test in INTERRUPT Method PASSED and Time taken for the Test is 24 micro secs
Applications Name: TPTC_A0_WR_RED_Test in Interrupt Method PASSED and Time taken for the Test is 23 micro secs
Applications Name: TPTC_A1_WR_RED_Test in Interrupt Method PASSED and Time taken for the Test is 22 micro secs
Applications Name: TPTC_B0_WR_RED_Test in Interrupt Method PASSED and Time taken for the Test is 22 micro secs
Applications Name: TPTC_A0_RD_SEC_Test in Interrupt Method PASSED and Time taken for the Test is 57 micro secs
Applications Name: TPTC_A0_RD_DED_Test in Interrupt Method PASSED and Time taken for the Test is 49 micro secs
Applications Name: TPTC_A0_RD_RED_Test in Interrupt Method PASSED and Time taken for the Test is 26 micro secs
Applications Name: TPTC_A1_RD_SEC_Test in Interrupt Method PASSED and Time taken for the Test is 49 micro secs
Applications Name: TPTC_A1_RD_DED_Test in Interrupt Method PASSED and Time taken for the Test is 48 micro secs
Applications Name: TPTC_A1_RD_RED_Test in Interrupt Method PASSED and Time taken for the Test is 25 micro secs
Applications Name: TPTC_B0_RD_SEC_Test in Interrupt Method PASSED and Time taken for the Test is 49 micro secs
Applications Name: TPTC_B0_RD_DED_Test in Interrupt Method PASSED and Time taken for the Test is 46 micro secs
Applications Name: TPTC_B0_RD_RED_Test in Interrupt Method PASSED and Time taken for the Test is 25 micro secs
Applications Name: MSS_CR5A_AXI_WR_RED_Test in INTERRUPT Method PASSED and Time taken for the Test is 17 micro secs
Applications Name: MSS_CR5B_AXI_WR_RED_Test in INTERRUPT Method PASSED and Time taken for the Test is 17 micro secs
Applications Name: MSS_CR5A_AXI_RD_SEC_Test in INTERRUPT Method PASSED and Time taken for the Test is 22 micro secs
Applications Name: MSS_CR5A_AXI_RD_RED_Test in INTERRUPT Method PASSED and Time taken for the Test is 16 micro secs
Applications Name: MSS_CR5B_AXI_RD_SEC_Test in INTERRUPT Method PASSED and Time taken for the Test is 22 micro secs
Applications Name: MSS_CR5B_AXI_RD_RED_Test in INTERRUPT Method PASSED and Time taken for the Test is 16 micro secs
Applications Name: MSS_CR5A_AXI_S_RED_Test in INTERRUPT Method PASSED and Time taken for the Test is 17 micro secs
Applications Name: MSS_CR5B_AXI_S_RED_Test in INTERRUPT Method PASSED and Time taken for the Test is 17 micro secs
All tests have passed
Shown below is a sample output when the application is run on AWR294X in C66 Core,
[C66xx_DSP]
ECC BUS SAFETY Application
ECC BUS SAFETY TEST START : starting
Applications Name: MCRC_SEC_Test in Interrupt Method PASSED and Time taken for the Test is 39 micro secs
Applications Name: MCRC_DED_Test in Interrupt Method PASSED and Time taken for the Test is 12 micro secs
Applications Name: MCRC_RED_Test in Interrupt Method PASSED and Time taken for the Test is 12 micro secs
Applications Name: DSS_L3_BANKA_SEC_Test in Interrupt Method PASSED and Time taken for the Test is 39 micro secs
Applications Name: DSS_L3_BANKA_DED_Test in Interrupt Method PASSED and Time taken for the Test is 11 micro secs
Applications Name: DSS_L3_BANKA_RED_Test in Interrupt Method PASSED and Time taken for the Test is 11 micro secs
Applications Name: DSS_L3_BANKB_SEC_Test in Interrupt Method PASSED and Time taken for the Test is 39 micro secs
Applications Name: DSS_L3_BANKB_DED_Test in Interrupt Method PASSED and Time taken for the Test is 12 micro secs
Applications Name: DSS_L3_BANKB_RED_Test in Interrupt Method PASSED and Time taken for the Test is 12 micro secs
Applications Name: DSS_L3_BANKC_SEC_Test in Interrupt Method PASSED and Time taken for the Test is 38 micro secs
Applications Name: DSS_L3_BANKC_DED_Test in Interrupt Method PASSED and Time taken for the Test is 12 micro secs
Applications Name: DSS_L3_BANKC_RED_Test in Interrupt Method PASSED and Time taken for the Test is 10 micro secs
Applications Name: DSS_L3_BANKD_SEC_Test in Interrupt Method PASSED and Time taken for the Test is 39 micro secs
Applications Name: DSS_L3_BANKD_DED_Test in Interrupt Method PASSED and Time taken for the Test is 11 micro secs
Applications Name: DSS_L3_BANKD_RED_Test in Interrupt Method PASSED and Time taken for the Test is 11 micro secs
Applications Name: DSS_HWA_DMA0_SEC_Test in Interrupt Method PASSED and Time taken for the Test is 39 micro secs
Applications Name: DSS_HWA_DMA0_DED_Test in Interrupt Method PASSED and Time taken for the Test is 12 micro secs
Applications Name: DSS_HWA_DMA0_RED_Test in Interrupt Method PASSED and Time taken for the Test is 11 micro secs
Applications Name: DSS_HWA_DMA1_SEC_Test in Interrupt Method PASSED and Time taken for the Test is 38 micro secs
Applications Name: DSS_HWA_DMA1_DED_Test in Interrupt Method PASSED and Time taken for the Test is 11 micro secs
Applications Name: DSS_HWA_DMA1_RED_Test in Interrupt Method PASSED and Time taken for the Test is 12 micro secs
Applications Name: DSS_MBOX_SEC_Test in Interrupt Method PASSED and Time taken for the Test is 38 micro secs
Applications Name: DSS_MBOX_DED_Test in Interrupt Method PASSED and Time taken for the Test is 11 micro secs
Applications Name: DSS_MBOX_RED_Test in Interrupt Method PASSED and Time taken for the Test is 12 micro secs
Applications Name: CBUFF_FIFO_SEC_Test in Interrupt Method PASSED and Time taken for the Test is 39 micro secs
Applications Name: CBUFF_FIFO_DED_Test in Interrupt Method PASSED and Time taken for the Test is 12 micro secs
Applications Name: CBUFF_FIFO_RED_Test in Interrupt Method PASSED and Time taken for the Test is 11 micro secs
Applications Name: TPTC_A0_WR_RED_Test in Interrupt Method PASSED and Time taken for the Test is 11 micro secs
Applications Name: TPTC_A0_WR_RED_Test in Interrupt Method PASSED and Time taken for the Test is 10 micro secs
Applications Name: TPTC_A0_WR_RED_Test in Interrupt Method PASSED and Time taken for the Test is 11 micro secs
Applications Name: TPTC_A0_WR_RED_Test in Interrupt Method PASSED and Time taken for the Test is 11 micro secs
Applications Name: TPTC_A0_WR_RED_Test in Interrupt Method PASSED and Time taken for the Test is 11 micro secs
Applications Name: TPTC_A0_WR_RED_Test in Interrupt Method PASSED and Time taken for the Test is 11 micro secs
Applications Name: TPTC_A0_WR_RED_Test in Interrupt Method PASSED and Time taken for the Test is 11 micro secs
Applications Name: TPTC_A0_WR_RED_Test in Interrupt Method PASSED and Time taken for the Test is 11 micro secs
Applications Name: TPTC_A0_WR_RED_Test in Interrupt Method PASSED and Time taken for the Test is 12 micro secs
Applications Name: TPTC_A0_WR_RED_Test in Interrupt Method PASSED and Time taken for the Test is 11 micro secs
Applications Name: TPTC_A0_RD_SEC_Test in Interrupt Method PASSED and Time taken for the Test is 57 micro secs
Applications Name: TPTC_A0_RD_DED_Test in Interrupt Method PASSED and Time taken for the Test is 31 micro secs
Applications Name: TPTC_A0_RD_RED_Test in Interrupt Method PASSED and Time taken for the Test is 13 micro secs
Applications Name: TPTC_A1_RD_SEC_Test in Interrupt Method PASSED and Time taken for the Test is 57 micro secs
Applications Name: TPTC_A1_RD_DED_Test in Interrupt Method PASSED and Time taken for the Test is 31 micro secs
Applications Name: TPTC_A1_RD_RED_Test in Interrupt Method PASSED and Time taken for the Test is 12 micro secs
Applications Name: TPTC_B0_RD_SEC_Test in Interrupt Method PASSED and Time taken for the Test is 57 micro secs
Applications Name: TPTC_B0_RD_DED_Test in Interrupt Method PASSED and Time taken for the Test is 31 micro secs
Applications Name: TPTC_B0_RD_RED_Test in Interrupt Method PASSED and Time taken for the Test is 13 micro secs
Applications Name: TPTC_B1_RD_SEC_Test in Interrupt Method PASSED and Time taken for the Test is 57 micro secs
Applications Name: TPTC_B1_RD_DED_Test in Interrupt Method PASSED and Time taken for the Test is 31 micro secs
Applications Name: TPTC_B1_RD_RED_Test in Interrupt Method PASSED and Time taken for the Test is 13 micro secs
Applications Name: TPTC_C0_RD_SEC_Test in Interrupt Method PASSED and Time taken for the Test is 59 micro secs
Applications Name: TPTC_C0_RD_DED_Test in Interrupt Method PASSED and Time taken for the Test is 31 micro secs
Applications Name: TPTC_C0_RD_RED_Test in Interrupt Method PASSED and Time taken for the Test is 13 micro secs
Applications Name: TPTC_C1_RD_SEC_Test in Interrupt Method PASSED and Time taken for the Test is 57 micro secs
Applications Name: TPTC_C1_RD_DED_Test in Interrupt Method PASSED and Time taken for the Test is 32 micro secs
Applications Name: TPTC_C1_RD_RED_Test in Interrupt Method PASSED and Time taken for the Test is 14 micro secs
Applications Name: TPTC_C2_RD_SEC_Test in Interrupt Method PASSED and Time taken for the Test is 57 micro secs
Applications Name: TPTC_C2_RD_DED_Test in Interrupt Method PASSED and Time taken for the Test is 32 micro secs
Applications Name: TPTC_C2_RD_RED_Test in Interrupt Method PASSED and Time taken for the Test is 13 micro secs
Applications Name: TPTC_C3_RD_SEC_Test in Interrupt Method PASSED and Time taken for the Test is 57 micro secs
Applications Name: TPTC_C3_RD_DED_Test in Interrupt Method PASSED and Time taken for the Test is 32 micro secs
Applications Name: TPTC_C3_RD_RED_Test in Interrupt Method PASSED and Time taken for the Test is 13 micro secs
Applications Name: TPTC_C4_RD_SEC_Test in Interrupt Method PASSED and Time taken for the Test is 57 micro secs
Applications Name: TPTC_C4_RD_DED_Test in Interrupt Method PASSED and Time taken for the Test is 32 micro secs
Applications Name: TPTC_C4_RD_RED_Test in Interrupt Method PASSED and Time taken for the Test is 13 micro secs
Applications Name: TPTC_C5_RD_SEC_Test in Interrupt Method PASSED and Time taken for the Test is 57 micro secs
Applications Name: TPTC_C5_RD_DED_Test in Interrupt Method PASSED and Time taken for the Test is 33 micro secs
Applications Name: TPTC_C5_RD_RED_Test in Interrupt Method PASSED and Time taken for the Test is 13 micro secs
Applications Name: PCR_SEC_Test in Interrupt Method PASSED and Time taken for the Test is 57 micro secs
Applications Name: PCR_DED_Test in Interrupt Method PASSED and Time taken for the Test is 33 micro secs
Applications Name: PCR_RED_Test in Interrupt Method PASSED and Time taken for the Test is 13 micro secs
Applications Name: DSP_SDMA_SEC_Test in Interrupt Method PASSED and Time taken for the Test is 38 micro secs
Applications Name: DSP_SDMA_DED_Test in Interrupt Method PASSED and Time taken for the Test is 15 micro secs
Applications Name: DSP_SDMA_RED_Test in Interrupt Method PASSED and Time taken for the Test is 14 micro secs
Applications Name: DSP_MDMA_RED_Test in Interrupt Method PASSED and Time taken for the Test is 14 micro secs
Applications Name: RSS_MBOX_SEC_Test in Interrupt Method PASSED and Time taken for the Test is 15 micro secs
Applications Name: RSS_MBOX_DED_Test in Interrupt Method PASSED and Time taken for the Test is 15 micro secs
Applications Name: RSS_MBOX_RED_Test in Interrupt Method PASSED and Time taken for the Test is 15 micro secs
Applications Name: RSS_ADCBUF_RD_RED_Test in Interrupt Method PASSED and Time taken for the Test is 15 micro secs
Applications Name: RSS_ADCBUF_WR_SEC_Test in Interrupt Method PASSED and Time taken for the Test is 15 micro secs
Applications Name: RSS_ADCBUF_WR_DED_Test in Interrupt Method PASSED and Time taken for the Test is 16 micro secs
Applications Name: RSS_ADCBUF_WR_RED_Test in Interrupt Method PASSED and Time taken for the Test is 15 micro secs
All tests have passed
Shown below is a sample output when the application is run on AM273X in C66 Core,
[C66xx_DSP]
ECC BUS SAFETY Application
ECC BUS SAFETY TEST START : starting
Applications Name: MDO_FIFO_DED_Test in Polling Method PASSED and Time taken for the Test is 6 micro secs
Applications Name: MDO_FIFO_RED_Test in Polling Method PASSED and Time taken for the Test is 6 micro secs
Applications Name: MCRC_SEC_Test in Interrupt Method PASSED and Time taken for the Test is 30 micro secs
Applications Name: MCRC_DED_Test in Interrupt Method PASSED and Time taken for the Test is 10 micro secs
Applications Name: MCRC_RED_Test in Interrupt Method PASSED and Time taken for the Test is 9 micro secs
Applications Name: DSS_L3_BANKA_SEC_Test in Interrupt Method PASSED and Time taken for the Test is 29 micro secs
Applications Name: DSS_L3_BANKA_DED_Test in Interrupt Method PASSED and Time taken for the Test is 9 micro secs
Applications Name: DSS_L3_BANKA_RED_Test in Interrupt Method PASSED and Time taken for the Test is 9 micro secs
Applications Name: DSS_L3_BANKB_SEC_Test in Interrupt Method PASSED and Time taken for the Test is 29 micro secs
Applications Name: DSS_L3_BANKB_DED_Test in Interrupt Method PASSED and Time taken for the Test is 9 micro secs
Applications Name: DSS_L3_BANKB_RED_Test in Interrupt Method PASSED and Time taken for the Test is 8 micro secs
Applications Name: DSS_L3_BANKC_SEC_Test in Interrupt Method PASSED and Time taken for the Test is 29 micro secs
Applications Name: DSS_L3_BANKC_DED_Test in Interrupt Method PASSED and Time taken for the Test is 9 micro secs
Applications Name: DSS_L3_BANKC_RED_Test in Interrupt Method PASSED and Time taken for the Test is 9 micro secs
Applications Name: DSS_L3_BANKD_SEC_Test in Interrupt Method PASSED and Time taken for the Test is 30 micro secs
Applications Name: DSS_L3_BANKD_DED_Test in Interrupt Method PASSED and Time taken for the Test is 9 micro secs
Applications Name: DSS_L3_BANKD_RED_Test in Interrupt Method PASSED and Time taken for the Test is 10 micro secs
Applications Name: DSS_HWA_DMA0_SEC_Test in Interrupt Method PASSED and Time taken for the Test is 29 micro secs
Applications Name: DSS_HWA_DMA0_DED_Test in Interrupt Method PASSED and Time taken for the Test is 8 micro secs
Applications Name: DSS_HWA_DMA0_RED_Test in Interrupt Method PASSED and Time taken for the Test is 9 micro secs
Applications Name: DSS_HWA_DMA1_SEC_Test in Interrupt Method PASSED and Time taken for the Test is 29 micro secs
Applications Name: DSS_HWA_DMA1_DED_Test in Interrupt Method PASSED and Time taken for the Test is 9 micro secs
Applications Name: DSS_HWA_DMA1_RED_Test in Interrupt Method PASSED and Time taken for the Test is 9 micro secs
Applications Name: DSS_MBOX_SEC_Test in Interrupt Method PASSED and Time taken for the Test is 30 micro secs
Applications Name: DSS_MBOX_DED_Test in Interrupt Method PASSED and Time taken for the Test is 9 micro secs
Applications Name: DSS_MBOX_RED_Test in Interrupt Method PASSED and Time taken for the Test is 8 micro secs
Applications Name: CBUFF_FIFO_SEC_Test in Interrupt Method PASSED and Time taken for the Test is 29 micro secs
Applications Name: CBUFF_FIFO_DED_Test in Interrupt Method PASSED and Time taken for the Test is 9 micro secs
Applications Name: CBUFF_FIFO_RED_Test in Interrupt Method PASSED and Time taken for the Test is 9 micro secs
Applications Name: TPTC_A0_WR_RED_Test in Interrupt Method PASSED and Time taken for the Test is 8 micro secs
Applications Name: TPTC_A0_WR_RED_Test in Interrupt Method PASSED and Time taken for the Test is 8 micro secs
Applications Name: TPTC_A0_WR_RED_Test in Interrupt Method PASSED and Time taken for the Test is 8 micro secs
Applications Name: TPTC_A0_WR_RED_Test in Interrupt Method PASSED and Time taken for the Test is 8 micro secs
Applications Name: TPTC_A0_WR_RED_Test in Interrupt Method PASSED and Time taken for the Test is 8 micro secs
Applications Name: TPTC_A0_WR_RED_Test in Interrupt Method PASSED and Time taken for the Test is 8 micro secs
Applications Name: TPTC_A0_WR_RED_Test in Interrupt Method PASSED and Time taken for the Test is 8 micro secs
Applications Name: TPTC_A0_WR_RED_Test in Interrupt Method PASSED and Time taken for the Test is 8 micro secs
Applications Name: TPTC_A0_WR_RED_Test in Interrupt Method PASSED and Time taken for the Test is 8 micro secs
Applications Name: TPTC_A0_WR_RED_Test in Interrupt Method PASSED and Time taken for the Test is 8 micro secs
Applications Name: TPTC_A0_RD_SEC_Test in Interrupt Method PASSED and Time taken for the Test is 43 micro secs
Applications Name: TPTC_A0_RD_DED_Test in Interrupt Method PASSED and Time taken for the Test is 24 micro secs
Applications Name: TPTC_A0_RD_RED_Test in Interrupt Method PASSED and Time taken for the Test is 10 micro secs
Applications Name: TPTC_A1_RD_SEC_Test in Interrupt Method PASSED and Time taken for the Test is 43 micro secs
Applications Name: TPTC_A1_RD_DED_Test in Interrupt Method PASSED and Time taken for the Test is 24 micro secs
Applications Name: TPTC_A1_RD_RED_Test in Interrupt Method PASSED and Time taken for the Test is 9 micro secs
Applications Name: TPTC_B0_RD_SEC_Test in Interrupt Method PASSED and Time taken for the Test is 43 micro secs
Applications Name: TPTC_B0_RD_DED_Test in Interrupt Method PASSED and Time taken for the Test is 24 micro secs
Applications Name: TPTC_B0_RD_RED_Test in Interrupt Method PASSED and Time taken for the Test is 10 micro secs
Applications Name: TPTC_B1_RD_SEC_Test in Interrupt Method PASSED and Time taken for the Test is 43 micro secs
Applications Name: TPTC_B1_RD_DED_Test in Interrupt Method PASSED and Time taken for the Test is 25 micro secs
Applications Name: TPTC_B1_RD_RED_Test in Interrupt Method PASSED and Time taken for the Test is 10 micro secs
Applications Name: TPTC_C0_RD_SEC_Test in Interrupt Method PASSED and Time taken for the Test is 43 micro secs
Applications Name: TPTC_C0_RD_DED_Test in Interrupt Method PASSED and Time taken for the Test is 24 micro secs
Applications Name: TPTC_C0_RD_RED_Test in Interrupt Method PASSED and Time taken for the Test is 10 micro secs
Applications Name: TPTC_C1_RD_SEC_Test in Interrupt Method PASSED and Time taken for the Test is 43 micro secs
Applications Name: TPTC_C1_RD_DED_Test in Interrupt Method PASSED and Time taken for the Test is 25 micro secs
Applications Name: TPTC_C1_RD_RED_Test in Interrupt Method PASSED and Time taken for the Test is 11 micro secs
Applications Name: TPTC_C2_RD_SEC_Test in Interrupt Method PASSED and Time taken for the Test is 44 micro secs
Applications Name: TPTC_C2_RD_DED_Test in Interrupt Method PASSED and Time taken for the Test is 25 micro secs
Applications Name: TPTC_C2_RD_RED_Test in Interrupt Method PASSED and Time taken for the Test is 10 micro secs
Applications Name: TPTC_C3_RD_SEC_Test in Interrupt Method PASSED and Time taken for the Test is 43 micro secs
Applications Name: TPTC_C3_RD_DED_Test in Interrupt Method PASSED and Time taken for the Test is 24 micro secs
Applications Name: TPTC_C3_RD_RED_Test in Interrupt Method PASSED and Time taken for the Test is 11 micro secs
Applications Name: TPTC_C4_RD_SEC_Test in Interrupt Method PASSED and Time taken for the Test is 45 micro secs
Applications Name: TPTC_C4_RD_DED_Test in Interrupt Method PASSED and Time taken for the Test is 25 micro secs
Applications Name: TPTC_C4_RD_RED_Test in Interrupt Method PASSED and Time taken for the Test is 11 micro secs
Applications Name: TPTC_C5_RD_SEC_Test in Interrupt Method PASSED and Time taken for the Test is 43 micro secs
Applications Name: TPTC_C5_RD_DED_Test in Interrupt Method PASSED and Time taken for the Test is 25 micro secs
Applications Name: TPTC_C5_RD_RED_Test in Interrupt Method PASSED and Time taken for the Test is 11 micro secs
Applications Name: PCR_SEC_Test in Interrupt Method PASSED and Time taken for the Test is 43 micro secs
Applications Name: PCR_DED_Test in Interrupt Method PASSED and Time taken for the Test is 25 micro secs
Applications Name: PCR_RED_Test in Interrupt Method PASSED and Time taken for the Test is 10 micro secs
Applications Name: DSP_SDMA_SEC_Test in Interrupt Method PASSED and Time taken for the Test is 29 micro secs
Applications Name: DSP_SDMA_DED_Test in Interrupt Method PASSED and Time taken for the Test is 11 micro secs
Applications Name: DSP_SDMA_RED_Test in Interrupt Method PASSED and Time taken for the Test is 11 micro secs
Applications Name: DSP_MDMA_RED_Test in Interrupt Method PASSED and Time taken for the Test is 11 micro secs
Applications Name: MDO_FIFO_SEC_Test in Interrupt Method PASSED and Time taken for the Test is 30 micro secs
All tests have passed