| Feature | Module |
|---|---|
| R5F (No-RTOS, FreeRTOS), C66x (No-RTOS, FreeRTOS), | CPU/OS |
| LwIP with ethernet driver (ENET) for CPSW | LwIP, ENET |
| UART, RTI (Timer), EDMA, EPWM, CBUFF | Drivers |
| IPC, HWA, CSI2-RX, CRC, GPIO, MIBSPI | Drivers |
| QSPI, Flash writer, MCAN, I2C , ESM, Watchdog, GPADC, ECAP | Drivers |
| SBL booting R5F and C66x | Bootloader |
| SOC | Supported CPUs | EVM | Host PC |
|---|---|---|---|
| AM273x | R5F, C66x | AM273x GP EVM (referred to as am273x-evm in code) | Windows 10 64b or Ubuntu 18.04 64b |
| Tools / SW module | Supported CPUs | Version |
|---|---|---|
| Code Composer Studio | R5F, C66x | 12.0.0 |
| SysConfig | R5F, C66x | 1.13.0 build, build 2553 |
| TI ARM CLANG | R5F | 2.1.1.LTS |
| TI C6000 Compiler | C66x | 8.3.12 |
| FreeRTOS Kernel | R5F, C66x | 10.4.3 |
| DSP LIB | C66x | 3.4.0.0 |
DSP LIB package is modified to fix the build in Linux environment from the base version dsplib_c66x_3_4_0_0
| OS | Supported CPUs | SysConfig Support | Key features tested | Key features not tested / NOT supported |
|---|---|---|---|---|
| FreeRTOS Kernel | R5F, C66x | NA | Task, Task notification, interrupts, semaphores, mutexs, timers, event groups. ROV views in CCS IDE, Task load measurement using FreeRTOS run time statistics APIs. | - |
| FreeRTOS POSIX | R5F, C66x | NA | pthread, mqueue, semaphore, clock | - |
| NO RTOS | R5F, C66x | NA | See Driver Porting Layer (DPL) below | - |
| Module | Supported CPUs | SysConfig Support | OS support | Key features tested | Key features not tested / NOT supported |
|---|---|---|---|---|---|
| Cache | R5F, C66x | YES | FreeRTOS, safeRTOS, NORTOS | Cache write back, invalidate, enable/disable | - |
| Clock | R5F, C66x | YES | FreeRTOS, safeRTOS, NORTOS | Tick timer at user specified resolution, timeouts and delays | - |
| CycleCounter | R5F, C66x | NA | FreeRTOS, safeRTOS, NORTOS | Measure CPU cycles using CPU specific internal counters | - |
| Debug | R5F, C66x | YES | FreeRTOS, safeRTOS, NORTOS | Logging and assert to any combo of: UART, CCS, shared memory | - |
| Heap | R5F, C66x | NA | FreeRTOS, safeRTOS, NORTOS | Create arbitrary heaps in user defined memory segments | - |
| Hwi | R5F, C66x | YES | FreeRTOS, safeRTOS, NORTOS | Interrupt register, enable/disable/restore | - |
| MPU | R5F | YES | FreeRTOS, safeRTOS, NORTOS | Setup MPU and control access to address space | - |
| Semaphore | R5F, C66x | NA | FreeRTOS, safeRTOS, NORTOS | Binary, Counting Semaphore, recursive mutexs with timeout | - |
| Task | R5F, C66x | NA | FreeRTOS, safeRTOS | Create, delete tasks | - |
| Timer | R5F, C66x | YES | FreeRTOS, safeRTOS, NORTOS | Configure arbitrary timers | - |
| Event | R5F, C66x | YES | FreeRTOS, safeRTOS | Setting, getting, clearing, and waiting of Event bits | - |
| Peripheral | Supported CPUs | SysConfig Support | Key features tested | Key features not tested / NOT supported |
|---|---|---|---|---|
| ADCBUF | R5F, C66x | YES | Source selection, Set chirp thresholds, continuous mode, configure modes | - |
| CBUFF | R5F, C66x | YES | stream data over LVDS interface | - |
| CRC | R5F, C66x | YES | Two channels, 8, 16, 32 and 64 bit data size, CPU mode | - |
| CSI-RX | R5F, C66x | YES | Setup complexio, dphy, common and context settings, event callbacks | - |
| ECAP | R5F, C66x | YES | Frequency, Duty cycle, interrupt mode | PWM mode not tested |
| EDMA | R5F, C66x | YES | Basic memory copy, DMA/QDMA channels, Interrupt/Polled, Manual/Event trigger, Chaining | - |
| EPWM | R5F | YES | Frequency, Duty cycle, interrupt mode | Tripzone, Deadband and Chopper module not tested |
| ESM | R5F, C66x | YES | Group and Error number selection, Tested ESM notifier with watchdog module | - |
| GPADC | R5F, C66x | YES | 10-bit ADC, Tested single/multiple buffer and on board temperature sensor read | - |
| GPIO | R5F, C66x | YES | Basic input/output, GPIO as interrupt | - |
| HWA | R5F, C66x | YES | FFT, CFAR, compression/decompression and local maxima modules, Interrupt/Polled, Manual/DMA trigger | - |
| I2C | R5F, C66x | YES | Master mode, basic read/write, polling and interrupt mode | Slave mode not supported. Driver not tested from C66x due to EVM limitations |
| IPC Notify | R5F, C66x | YES | Low latency IPC between RTOS/NORTOS CPUs | - |
| IPC Rpmsg | R5F, C66x | YES | RPMessage protocol based IPC for all R5F, C66x running NORTOS/FreeRTOS | - |
| MCAN | R5F | YES | RX, TX, interrupt and polling mode | - |
| MIBSPI | R5F, C66x | YES | Master/Slave mode, basic read/write, Interrupt/Polled, icount enable/disable, CPU/DMA mode | - |
| Pinmux | R5F, C66x | YES | Tested with multiple peripheral pinmuxes | - |
| QSPI | R5F | YES | Read direct, Write indirect, Read/Write commands | Interrupt mode not supported, Dual and Quad writes are not supported |
| SOC | R5F, C66x | YES | Lock/unlock MMRs, get CPU clock, CPU name, clock enable, set frequency | - |
| UART | R5F, C66x | YES | Basic read/write, polling, interrupt mode, CPU/DMA mode | - |
| WATCHDOG | R5F, C66x | YES | Window size and Expiry time selections, Reset mode, Digital windowed | - |
| Module | Supported CPUs | OS support | Key features tested | Key features not tested / NOT supported |
|---|---|---|---|---|
| Bootloader | R5FSS0-0 | NORTOS | Boot modes: QSPI, UART. R5F (Lockstep/Dual Core) and C66x core boot. RPRC, multi-core image format, Pll configuration. | - |
| Peripheral | Supported CPUs | SysConfig Support | Key features tested | Key features not tested |
|---|---|---|---|---|
| EEPROM | R5F | YES | I2C based EEPROM | - |
| Flash | R5F | YES | QSPI based flash | All vendor flash types not tested |
| LED | R5F, C66x | YES | GPIO based LED control | - |
| Module | Supported CPUs | SysConfig Support | OS Support | Key features tested | Key features not tested |
|---|---|---|---|---|---|
| LwIP | R5F | NO | FreeRTOS | TCP/UDP IP networking stack, DHCP, ping, TCP iperf, TCP/UDP IP | Other LwIP features, performance and memory optimizations pending, more robustness tests pending |
| Ethernet driver (ENET) | R5F | NO | FreeRTOS | Ethernet as port using CPSW; MAC loopback and PHY loopback | Ethernet as switch |
| ID | Head Line | Module | Applicable Releases | Resolution/Comments |
|---|---|---|---|---|
| MCUSDK-2457 | Tools installed twice due to makefile based and ccs based builds | Build | 08.01.00 | Fixed |
| MCUSDK-2191 | CPSW example doesn't work with SBL | CPSW | 08.01.00 | Fixed |
| MCUSDK-2346 | docs - Document External JTAG issue workaround | docs | 08.01.00 | Fixed |
| MCUSDK-2396 | Low SVC stack size with Interrupt nesting enabled | DPL | 08.01.00 | Fixed |
| MCUSDK-2301 | Correct main task name from frertos_main to freertos_main | Enet | 08.01.00 | Fixed |
| MCUSDK-2244 | Enet documentation needs to be enabled | Enet | 08.01.00 | Fixed |
| MCUSDK-2151 | I2C Probe does not display slave devices correctly | I2C | 08.01.00, 08.00.02 | Fixed |
| MCUSDK-2541 | IPC developer guide block diagram shows invalid cores | IPC_Notify, IPC_RPMSG | 08.01.00 | Fixed |
| MCUSDK-2507 | [AM273] [QSPI] Missing QSPI driver documentation | QSPI | 08.01.00 | Fixed |
| MCUSDK-3266 | Remove customer name from the code | SBL | 08.01.00 | Fixed |
| MCUSDK-2401 | Application size limitation with SBL_UART | SBL | 08.01.00 | Fixed |
| MCUSDK-2416 | AM64X: Writing images to flash larger than 1024 KByte, uniflash finishes with errors | UART | 08.01.00 | Fixed |
| ID | Head Line | Module | Applicable Releases | Workaround |
|---|---|---|---|---|
| PDK-8405 | MIBSPI non-DMA mode transfer doesn't complete when used in mmWaveSDK | MIBSPI | 8.00.01 | None. Issue is not seen in driver unit test |
| MCUSDK-2037 | MIBSPI: Observing issues with SPI communication on Two-Chip cascade board | MIBSPI | 8.00.01 | None. Issue is not seen when ccs log is enabled in the application. |
| MCUSDK-2453 | R5 - Init code crashes under certain conditions | FreeRTOS, No-RTOS | 8.02.00 | None |
| MCUSDK-2232 | "HWA_paramSetDonePolling" function in HWA driver not working properly | HWA_FFT | 8.02.00 | None |
| MCUSDK-2183 | Streaming of data over Ethernet interface not stable | Enet | 8.02.00 | None |
| ID | Head Line | Module | Reported in Release | Workaround |
|---|---|---|---|---|
| PDK-8404 | QSPI test failing at 80 Mhz | QSPI | 8.00.01 | QSPI driver works at 40 Mhz |
This section lists changes which could affect user applications developed using older SDK versions. Read this carefully to see if you need to do any changes in your existing application when migrating to this SDK version relative to previous SDK version. Also refer to older SDK version release notes to see changes in earlier SDKs.
| Module | Affected API | Change | Additional Remarks |
|---|---|---|---|
| Release Build | - | Updated optimization level in release build to 'Os' as part of bug fix MCUSDK-1980. | The release build with ti-arm-clang compiler has been updated from 'O3' to 'Os' optimization level. It is recommended that user rebuilds the existing libraries and applications with 'Os' option. This can be done by updating CFLAGS_release in library/example makefiles. |