This example is a TCP/UDP IP application using the LwIP networking stack, coupled with ethernet driver (ENET)
On AM273X, we can do ethernet based communication using CPSW as HW mechanism
The examples do below
Parameter | Value |
---|---|
CPU + OS | r5fss0-0_freertos r5fss0-1_freertos |
Toolchain | ti-arm-clang |
Boards | am273x-evm |
Example folder | examples/networking/lwip/enet_lwip_cpsw |
Feature | Section | Description | Remarks/Default Setting |
---|---|---|---|
Mdio Manual Mode Enable | TI Networking / Enet (CPSW) | Flag to enable MDIO manual mode in example. Driver support for Manual mode is enabled, so this parameter configures manual mode in the example. | Default is true. If your silicon is affected with errata i2329— MDIO interface corruption, then TI suggests to use MDIO_MANUAL_MODE as software workaround. |
Enable Packet Pool Allocation | TI Networking / Enet (CPSW) | Flag to enable packet allocation from enet utils library. It should be disabled to avoid utils memory wastage, in case application allots packet via other mechanism. (Ex- Lwip pools) | Default is true. It is disabled for lwip based examples. If enabled size of pkt pool size depends on 'Large Pool Packet Size', 'Large Pool Packet Count', 'Medium Pool Packet Size', 'Medium Pool Packet Count', 'Small Pool Packet Size' and 'Small Pool Packet Count'. |
Number of Tx Packet | TI Networking / Enet (CPSW) / DMA channel config | No of Tx packets required for DMA channel | Default is 16. It contributes to the size of Pkt Mem Pool, DMA ring buffer and accessories. |
Number of Rx Packet | TI Networking / Enet (CPSW) / DMA channel config | No of Rx packets required for DMA channel | Default is 32. It contributes to the size of Pkt Mem Pool, DMA ring buffer and accessories size. |
Argument | Meaning |
---|---|
-s | Run server |
-c | Run Client [Ex: -c 192.168.1.102] |
-u | UDP |
-b | Bandwidth [Used in UDP, Ex: 100M M->Mbits] |
-i | Output interval in Sec [Ex: -i1 1sec interval] |
-t | Time in sec [Ex: -t60 60sec] |
-p | Port number [Ex: -p 5555] |
-w | Windows size [Ex: -w 1M M->Mbits] |
-d | Bi-directional traffic |
-l | Length [Ex: -l 1046 1046bytes] |
-V | Used when IPv6 address is used instead of IPv4 |
> ping 192.168.1.100
iperf
tests as shown below. Below steps have been tried with a Linux Ubuntu 18.04 host PC running bash shelliperf
if not installed by doing below > sudo apt install iperf
0.0.0.0
thenlink_callback==UP
message, if not check the ethernet cable