AM273x MCU+ SDK  08.03.00
GPADC Group Channel Read

Introduction

This example configures a GPADC configuration for multi channel and triggers the multi channel conversion. Upon successful converted adc conversion data is displayed. Conversion happens based on the parameters provided through syscfg

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
Toolchain ti-arm-clang
Boards am273x-evm
Example folder examples/drivers/gpadc/gpadc_group_channel_read/

Steps to Run the Example

See Also

GPADC

Sample Output

Shown below is a sample output when the application is run,

Channel adc conversion successful
Channel HW_CH ADC Value Volt
0 ADC_IN0 0x000002ac 1202mV
1 ADC_IN1 0x00000000 0000mV
2 ADC_IN2 0x00000000 0000mV
3 ADC_IN3 0x00000000 0000mV
4 ADC_IN4 0x00000000 0000mV
5 ADC_IN5 0x00000000 0000mV
6 ADC_IN6 0x00000000 0000mV
7 ADC_IN7 0x00000000 0000mV
8 ADC_IN8 0x00000000 0000mV
All tests have passed!!