AM273x MCU+ SDK  08.03.00
CBUFF Software Trigger

Introduction

This example performs CBUFF software trigger.

  • The user memory is initialized with incremented pattern. Cache write back is done to ensure that initialized data from cache is written to memory.
  • Configures EDMA channel PaRAM set with source address as user buffer and destination as CBUFF FIFO.
  • DCA1000 has to be connected to EVM to capture the data sent over LVDS interface by the test.
  • After the test is completed, a binary file would be captured by DCA1000 EVM which can be verified manually. If the CBUFF module triggers the frame done interrupt test is successful.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
c66ss0 nortos
Toolchain ti-arm-clang
Boards am273x-evm
Example folder examples/drivers/cbuff/cbuff_sw_trigger

Steps to Run the Example

Sample Output

Shown below is a sample output when the application is run,

[CBUFF] SW Trigger Test Started...
waiting for frameDone interrupt : 0
Received frameDone interrupt : 1
Data is transmitted over LVDS successfully.
[CBUFF] SW Trigger Test Completed!!
All tests have passed!!