AM273x MCU+ SDK  08.02.00
Watchdog reset mode

Introduction

This example uses the WDT module in reset mode to trigger SOC warm reset. Servicing the WDT for few iterations before triggering the warm reset. It will reset the device once it reaches the expiry time set by user.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
Toolchain ti-arm-clang
Board am273x-evm
Example folder examples/drivers/watchdog/watchdog_reset/

Supported Combinations

Steps to Run the Example

See Also

WATCHDOG

Sample Output

Shown below is a sample output when the application is run, Please note that application prints in both CCS and UART console.

Note
Console prints will be stopped once WDT triggers warm reset.

CCS Console:

[MAIN_Cortex_R5_0_0] Watchdog reset Mode Test Started ...
Servicing WDT for few iterations
Watchdog triggers warm reset in 3000 (ms)
All tests have passed!!
Prints will be stopped after reset
Prints will be stopped after reset
Prints will be stopped after reset
'' ''
'' ''
'' ''
Prints will be stopped after reset

UART Console:

Watchdog reset Mode Test Started ...
Servicing WDT for few iterations
Watchdog triggers warm reset in 3000 (ms)
All tests have passed!!
Prints will be stopped after reset
Prints will be stopped after reset
Prints will be stopped after reset
'' ''
'' ''
'' ''
Prints will be stopped after reset