This example demonstrates the data transfer from flash connected to QSPI interface in DMA mode
Parameter | Value |
---|---|
CPU + OS | r5fss0-0 freertos |
r5fss0-0 nortos | |
Toolchain | ti-arm-clang |
Boards | am273x-evm |
Example folder | examples/drivers/qspi/qspi_flash_dma_transfer |
Shown below is a sample output when the application is run,