|
AM263x MCU+ SDK
26.00.00
|
|
Go to the documentation of this file.
53 #ifndef INCLUDE_SDL_EXCEPTION_H_
54 #define INCLUDE_SDL_EXCEPTION_H_
66 uint64_t bitErrorOffset,
67 uint32_t bitErrorGroup);
73 typedef struct SDL_EXCEPTION_CallbackFunctions_s
SDL_EXCEPTION_Callback_t swiExptnCallback
Definition: sdl_exception.h:77
void SDL_EXCEPTION_swIntrExptnHandler(void *param)
SW Interrupt Exception Handler.
void SDL_EXCEPTION_undefInstructionExptnHandler(void *param)
Undefined Instruction Exception Handler.
void(* SDL_EXCEPTION_ECCCallback_t)(uint32_t intSource, uint32_t errorAddr, uint32_t ramId, uint64_t bitErrorOffset, uint32_t bitErrorGroup)
Format of Call back function for ECC error events.
Definition: sdl_exception.h:63
void SDL_EXCEPTION_prefetchAbortExptnHandler(void *param)
Prefetch Abort Exception Handler.
SDL_EXCEPTION_Callback_t pabtExptnCallback
Definition: sdl_exception.h:79
Header file contains enumerations, structure definitions and function declarations for SDL COMMON int...
void SDL_EXCEPTION_irqExptnHandler(void *param)
IRQ Exception Handler.
void(* SDL_EXCEPTION_Callback_t)(void)
Format of Call back function for exception.
Definition: sdl_exception.h:70
SDL_EXCEPTION_Callback_t fiqExptnCallback
Definition: sdl_exception.h:87
void SDL_EXCEPTION_init(const SDL_EXCEPTION_CallbackFunctions_t *callbackFunctions)
Initialise Exception module.
Structure of call back functions for various exception events.
Definition: sdl_exception.h:74
SDL_EXCEPTION_Callback_t dabtExptnCallback
Definition: sdl_exception.h:81
void SDL_EXCEPTION_registerECCHandler(SDL_EXCEPTION_ECCCallback_t ECCCallBackFunctionPtr)
Function to register ECC exception handler.
SDL_EXCEPTION_Callback_t irqExptnCallback
Definition: sdl_exception.h:83
void SDL_EXCEPTION_fiqExptnHandler(void *param)
FIQ Exception Handler.
void SDL_EXCEPTION_dataAbortExptnHandler(void *param)
Data Abort Exception Handler.
SDL_EXCEPTION_Callback_t udefExptnCallback
Definition: sdl_exception.h:75