AM263x MCU+ SDK  26.00.00
lldtsync.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2023 Texas Instruments Incorporated
3  * Copyright (c) 2023 Excelfore Corporation (https://excelfore.com)
4  *
5  * All rights reserved not granted herein.
6  * Limited License.
7  *
8  * Texas Instruments Incorporated grants a world-wide, royalty-free,
9  * non-exclusive license under copyrights and patents it now or hereafter
10  * owns or controls to make, have made, use, import, offer to sell and sell ("Utilize")
11  * this software subject to the terms herein. With respect to the foregoing patent
12  * license, such license is granted solely to the extent that any such patent is necessary
13  * to Utilize the software alone. The patent license shall not apply to any combinations which
14  * include this software, other than combinations with devices manufactured by or for TI ("TI Devices").
15  * No hardware patent is licensed hereunder.
16  *
17  * Redistributions must preserve existing copyright notices and reproduce this license (including the
18  * above copyright notice and the disclaimer and (if applicable) source code license limitations below)
19  * in the documentation and/or other materials provided with the distribution
20  *
21  * Redistribution and use in binary form, without modification, are permitted provided that the following
22  * conditions are met:
23  *
24  * * No reverse engineering, decompilation, or disassembly of this software is permitted with respect to any
25  * software provided in binary form.
26  * * any redistribution and use are licensed by TI for use only with TI Devices.
27  * * Nothing shall obligate TI to provide you with source code for the software licensed and provided to you in object code.
28  *
29  * If software source code is provided to you, modification and redistribution of the source code are permitted
30  * provided that the following conditions are met:
31  *
32  * * any redistribution and use of the source code, including any resulting derivative works, are licensed by
33  * TI for use only with TI Devices.
34  * * any redistribution and use of any object code compiled from the source code and any resulting derivative
35  * works, are licensed by TI for use only with TI Devices.
36  *
37  * Neither the name of Texas Instruments Incorporated nor the names of its suppliers may be used to endorse or
38  * promote products derived from this software without specific prior written permission.
39  *
40  * DISCLAIMER.
41  *
42  * THIS SOFTWARE IS PROVIDED BY TI AND TI"S LICENSORS "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING,
43  * BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED.
44  * IN NO EVENT SHALL TI AND TI"S LICENSORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
45  * CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA,
46  * OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY,
47  * OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE
48  * POSSIBILITY OF SUCH DAMAGE.
49 */
56 #ifndef LLDTSYNC_H_
57 #define LLDTSYNC_H_
58 
59 #include "lldtype.h"
60 
64 typedef struct {
68  uint32_t enetType;
72  uint32_t instId;
74 
75 typedef enum
76 {
81 
85 typedef struct LLDTSync LLDTSync_t;
86 
92 
100 
105 void LLDTSyncClose(LLDTSync_t *hTSync);
106 
117 int LLDTSyncGetRxTime(LLDTSync_t *hTSync, uint8_t rxPort, int msgType,
118  uint16_t seqId, uint8_t domain, uint64_t *ts);
119 
130 int LLDTSyncGetTxTime(LLDTSync_t *hTSync, uint8_t txPort, int msgType,
131  uint16_t seqId, uint8_t domain, uint64_t *ts);
132 
139 int LLDTSyncAdjFreq(LLDTSync_t *hTSync, int ppb);
140 
147 int LLDTSyncSetTime(LLDTSync_t *hTSync, uint64_t ts);
148 
155 int LLDTSyncGetTime(LLDTSync_t *hTSync, uint64_t *ts);
156 
164 int LLDTSyncEnableTsEvent(LLDTSync_t *hTSync, uint32_t ports[], uint32_t numPorts);
165 
172 int LLDTSyncShiftTime(LLDTSync_t *hTSync, int64_t offset);
173 
183 int LLDTsyncPhyWaitTxTs(LLDTSync_t *hTSync, uint8_t txPort, int msgType,
184  uint16_t seqId, uint8_t domain);
185 
195 int LLDTSyncProcPhyStatusFrame(void* hEnet, uint8_t coreId , uint8_t txPort,
196  uint8_t* frame, uint32_t size);
197 
198 
199 #endif //LLDTSYNC_H_
200 
LLDTsyncPhyWaitTxTs
int LLDTsyncPhyWaitTxTs(LLDTSync_t *hTSync, uint8_t txPort, int msgType, uint16_t seqId, uint8_t domain)
Put the TX packet in the wait list.
LLDTSyncGetRxTime
int LLDTSyncGetRxTime(LLDTSync_t *hTSync, uint8_t rxPort, int msgType, uint16_t seqId, uint8_t domain, uint64_t *ts)
Retrieves the PTP RX timestamp for a specific message.
LLDTSyncCfgInit
void LLDTSyncCfgInit(LLDTSyncCfg_t *cfg)
Initializes the LLDTSyncCfg_t configuration structure.
LLDTSyncAdjFreq
int LLDTSyncAdjFreq(LLDTSync_t *hTSync, int ppb)
Adjusts the frequency of the PTP clock.
LLDTSyncCfg_t::enetType
uint32_t enetType
Definition: lldtsync.h:68
LLDTSYNC_TS_SOURCE_CPTS
@ LLDTSYNC_TS_SOURCE_CPTS
Definition: lldtsync.h:78
LLDTSyncSetTime
int LLDTSyncSetTime(LLDTSync_t *hTSync, uint64_t ts)
Sets the time for the PTP clock.
LLDTSyncEnableTsEvent
int LLDTSyncEnableTsEvent(LLDTSync_t *hTSync, uint32_t ports[], uint32_t numPorts)
Enables PTP timestamp events for specified ports.
LLDTSyncClose
void LLDTSyncClose(LLDTSync_t *hTSync)
Closes the LLDTSync instance.
lldtype.h
Data types and macros for TI Enet LLD abstract APIs.
LLDTSyncCfg_t::instId
uint32_t instId
Definition: lldtsync.h:72
LLDTSyncGetTime
int LLDTSyncGetTime(LLDTSync_t *hTSync, uint64_t *ts)
Retrieves the current time from the PTP clock.
LLDTSyncShiftTime
int LLDTSyncShiftTime(LLDTSync_t *hTSync, int64_t offset)
Shift the time of the PTP clock by offset nsec.
LLDTSyncCfg_t
Configuration structure for LLDTSync.
Definition: lldtsync.h:64
LLDTSyncOpen
LLDTSync_t * LLDTSyncOpen(LLDTSyncCfg_t *cfg, LLDTsyncTsSource tsSource)
Opens a new LLDTSync instance to access the PTP clock.
LLDTSYNC_TS_SOURCE_INVALID
@ LLDTSYNC_TS_SOURCE_INVALID
Definition: lldtsync.h:77
LLDTsyncTsSource
LLDTsyncTsSource
Definition: lldtsync.h:76
LLDTSync_t
struct LLDTSync LLDTSync_t
Structure representing the LLDTSync instance.
Definition: lldtsync.h:85
LLDTSyncProcPhyStatusFrame
int LLDTSyncProcPhyStatusFrame(void *hEnet, uint8_t coreId, uint8_t txPort, uint8_t *frame, uint32_t size)
Process the status frame.
LLDTSYNC_TS_SOURCE_PHY
@ LLDTSYNC_TS_SOURCE_PHY
Definition: lldtsync.h:79
LLDTSyncGetTxTime
int LLDTSyncGetTxTime(LLDTSync_t *hTSync, uint8_t txPort, int msgType, uint16_t seqId, uint8_t domain, uint64_t *ts)
Retrieves the PTP TX timestamp for a specific message.