![Logo](ti_logo.svg) |
AM263x MCU+ SDK
09.02.00
|
|
Go to the documentation of this file.
47 #ifndef ENET_MOD_MACPORT_H_
48 #define ENET_MOD_MACPORT_H_
67 #define ENET_MACPORT_PUBLIC_IOCTL(x) (ENET_IOCTL_TYPE_PUBLIC | \
68 ENET_IOCTL_MACPORT_BASE | \
72 #define ENET_MACPORT_PRIVATE_IOCTL(x) (ENET_IOCTL_TYPE_PRIVATE | \
73 ENET_IOCTL_MACPORT_BASE | \
82 typedef enum EnetMacPort_Ioctl_e
345 #if ENET_CFG_IS_ON(CPSW_CUTTHRU)
369 typedef enum EnetMac_LayerType_e
384 typedef enum EnetMac_SublayerType_e
405 typedef enum EnetMac_VariantType_e
417 typedef enum EnetMac_SgmiiMode_e
441 typedef struct EnetMacPort_Interface_s
456 typedef struct EnetMacPort_LinkCfg_s
468 typedef enum EnetMacPort_VlanType_e
483 typedef struct EnetMacPort_GenericInArgs_s
492 typedef struct EnetMacPort_SetIngressDscpPriorityMapInArgs_s
504 typedef struct EnetMacPort_SetPriorityRegenMapInArgs_s
516 typedef struct EnetMacPort_SetEgressPriorityMapInArgs_s
528 typedef struct EnetMacPort_EnableEgressTrafficShapingInArgs_s
540 typedef struct EnetMacPort_CreditBasedShaperInArgs_s
552 typedef enum EnetMacPort_PreemptVerifyStatus_e
583 typedef struct EnetMacPort_SetPreemptMinFragSizeInArgs_s
596 typedef enum EnetMacPort_QueuePreemptMode_e
608 typedef struct EnetMacPort_QueuePreemptCfg_s
618 typedef struct EnetMacPort_SetPreemptQueueInArgs_s
627 #if ENET_CFG_IS_ON(CPSW_CUTTHRU)
631 typedef struct EnetMacPort_CutThruParams_s
637 EnetPort_CutThruParams cutThruCfg;
638 } EnetMacPort_CutThruParams;
Enet_MacPort macPort
Definition: enet_mod_macport.h:495
EnetMacPort_PreemptVerifyStatus
MacPort IET Verification status.
Definition: enet_mod_macport.h:553
@ ENET_MACPORT_IOCTL_DISABLE_EGRESS_TRAFFIC_SHAPING
Disable egress traffic shaping configuration.
Definition: enet_mod_macport.h:181
Priority map.
Definition: enet_mod_port.h:128
Enet_MacPort macPort
Definition: enet_mod_macport.h:543
@ ENET_MACPORT_IOCTL_SET_CREDIT_BASED_SHAPING
Set Idleslope for Credit Based Shaper on MAC Port.
Definition: enet_mod_macport.h:217
EnetPort_PriorityMap priorityMap
Definition: enet_mod_macport.h:522
@ ENET_MAC_SGMIIMODE_INVALID
Definition: enet_mod_macport.h:420
@ ENET_MACPORT_VLAN_TYPE_STACKED_TAGS
Definition: enet_mod_macport.h:477
@ ENET_MAC_VERIFYSTATUS_FAILED
Definition: enet_mod_macport.h:567
@ ENET_MACPORT_IOCTL_GET_MAXLEN
Get MRU and MTU.
Definition: enet_mod_macport.h:199
@ ENET_MAC_SGMIIMODE_FIBER_WITH_PHY
Definition: enet_mod_macport.h:423
@ ENET_MAC_LAYER_GMII
Definition: enet_mod_macport.h:375
@ ENET_MAC_SGMIIMODE_SGMII_FORCEDLINK
Definition: enet_mod_macport.h:435
@ ENET_MAC_SGMIIMODE_SGMII_AUTONEG_SLAVE
Definition: enet_mod_macport.h:432
EnetMac_VariantType variantType
Definition: enet_mod_macport.h:450
@ ENET_MAC_VERIFYSTATUS_UNKNOWN
Definition: enet_mod_macport.h:555
static bool EnetMacPort_isMii(const EnetMacPort_Interface *mii)
Check if interface is MII.
Definition: enet_mod_macport.h:724
@ ENET_MACPORT_IOCTL_SET_PRI_REGEN_MAP
Set VLAN priority regeneration map.
Definition: enet_mod_macport.h:136
Enet_MacPort macPort
Definition: enet_mod_macport.h:586
@ ENET_MACPORT_IOCTL_ENABLE_EGRESS_TRAFFIC_SHAPING
Enable egress traffic shaping configuration.
Definition: enet_mod_macport.h:172
@ ENET_MACPORT_IOCTL_GET_EGRESS_QOS_PRI_MAP
Get QoS egress priority map.
Definition: enet_mod_macport.h:163
Enet_Speed
MAC interface speed.
Definition: enet_types.h:343
Link speed and duplexity configuration.
Definition: enet_mod_macport.h:457
Input args for ENET_MACPORT_IOCTL_SET_PREEMPT_QUEUE.
Definition: enet_mod_macport.h:619
@ ENET_MAC_SGMIIMODE_SGMII_AUTONEG_MASTER
Definition: enet_mod_macport.h:429
@ ENET_MAC_SGMIIMODE_SGMII_WITH_PHY
Definition: enet_mod_macport.h:426
@ ENET_MAC_SUBLAYER_SERIAL
Definition: enet_mod_macport.h:393
This file contains the type definitions and helper macros that are common for host and MAC ports.
@ ENET_MACPORT_IOCTL_GET_PREEMPT_VERIFY_STATUS
Get IET verification status.
Definition: enet_mod_macport.h:289
@ ENET_MAC_SUBLAYER_QUAD_SERIAL_SUB
Definition: enet_mod_macport.h:399
@ ENET_MAC_QUEUE_PREEMPT_MODE_EXPRESS
Definition: enet_mod_macport.h:599
EnetPort_CreditBasedShapingCfg cbsCfg
Definition: enet_mod_macport.h:546
Input args for ENET_MACPORT_IOCTL_ENABLE_EGRESS_TRAFFIC_SHAPING command.
Definition: enet_mod_macport.h:529
@ ENET_MACPORT_IOCTL_SET_PREEMPT_MIN_FRAG_SIZE
Set minimum fragment size.
Definition: enet_mod_macport.h:280
static bool EnetMacPort_isGmii(const EnetMacPort_Interface *mii)
Check if interface is GMII.
Definition: enet_mod_macport.h:736
Enet_MacPort
MAC port.
Definition: enet_types.h:409
Enet_Speed speed
Definition: enet_mod_macport.h:459
EnetMacPort_QueuePreemptCfg queuePreemptCfg
Definition: enet_mod_macport.h:624
@ ENET_MACPORT_IOCTL_GET_PREEMPTION_ACTIVE_STATUS
Get preemption active status.
Definition: enet_mod_macport.h:316
@ ENET_MACPORT_IOCTL_GET_INGRESS_DSCP_PRI_MAP
Get ingress DSCP priority (TOS) map.
Definition: enet_mod_macport.h:127
static bool EnetMacPort_isQsgmii(const EnetMacPort_Interface *mii)
Check if interface is QSGMII.
Definition: enet_mod_macport.h:754
EnetMac_LayerType
MAC interface layer type.
Definition: enet_mod_macport.h:370
@ ENET_MACPORT_IOCTL_SET_PREEMPT_QUEUE
Set macport queue preemption mode.
Definition: enet_mod_macport.h:262
@ ENET_MACPORT_IOCTL_GET_QUEUE_PREEMPT_STATUS
Get macport queue preemption status.
Definition: enet_mod_macport.h:253
@ ENET_MAC_LAYER_XGMII
Definition: enet_mod_macport.h:378
@ ENET_MACPORT_IOCTL_SET_EGRESS_QOS_PRI_MAP
Set QoS egress priority map.
Definition: enet_mod_macport.h:154
@ ENET_MAC_SUBLAYER_STANDARD
Definition: enet_mod_macport.h:387
@ ENET_MAC_LAYER_MII
Definition: enet_mod_macport.h:372
Enet_MacPort macPort
Definition: enet_mod_macport.h:486
MacPort Queue Preempt Config.
Definition: enet_mod_macport.h:609
@ ENET_MAC_VARIANT_FORCED
Definition: enet_mod_macport.h:411
DSCP priority map.
Definition: enet_mod_port.h:138
Generic MAC port input args.
Definition: enet_mod_macport.h:484
@ ENET_MAC_VERIFYSTATUS_DISABLED
Definition: enet_mod_macport.h:570
uint8_t preemptMinFragSize
Definition: enet_mod_macport.h:590
@ ENET_MACPORT_IOCTL_GET_PRI_REGEN_MAP
Get VLAN priority regeneration map.
Definition: enet_mod_macport.h:145
@ ENET_MACPORT_VLAN_TYPE_NONE
Definition: enet_mod_macport.h:471
EnetMac_SublayerType sublayerType
Definition: enet_mod_macport.h:447
static bool EnetMacPort_isRmii(const EnetMacPort_Interface *mii)
Check if interface is RMII.
Definition: enet_mod_macport.h:730
EnetMacPort_VlanType
VLAN usage type.
Definition: enet_mod_macport.h:469
EnetPort_TrafficShapingCfg trafficShapingCfg
Definition: enet_mod_macport.h:534
#define ENET_MACPORT_PUBLIC_IOCTL(x)
Helper macro to create IOCTL commands for MAC port module.
Definition: enet_mod_macport.h:67
@ ENET_MACPORT_IOCTL_DISABLE_PREEMPT_VERIFICATION
Disable IET verification.
Definition: enet_mod_macport.h:298
#define ENET_PRI_NUM
Packet priority.
Definition: enet_types.h:165
@ ENET_MACPORT_IOCTL_GET_LINK_CFG
Get MAC port's speed and duplexity.
Definition: enet_mod_macport.h:208
MAC port interface.
Definition: enet_mod_macport.h:442
@ ENET_MAC_SUBLAYER_REDUCED
Definition: enet_mod_macport.h:390
Enet_Duplexity
MAC interface duplexity.
Definition: enet_types.h:361
Enet_MacPort macPort
Definition: enet_mod_macport.h:507
@ ENET_MAC_VERIFYSTATE_INITIAL
Definition: enet_mod_macport.h:558
@ ENET_MACPORT_IOCTL_ENABLE_PREEMPT_VERIFICATION
Enable IET verification.
Definition: enet_mod_macport.h:307
EnetMac_VariantType
MAC interface variant (only for specific interface types).
Definition: enet_mod_macport.h:406
@ ENET_MACPORT_IOCTL_IET_RELEASE_PREEMPT_TRAFFIC
IET release preemptible traffic.
Definition: enet_mod_macport.h:235
@ ENET_MACPORT_IOCTL_GET_CREDIT_BASED_SHAPING
Get Idleslope of Credit Based Shaper on MAC Port.
Definition: enet_mod_macport.h:226
@ ENET_MAC_QUEUE_PREEMPT_MODE_PREEMPT
Definition: enet_mod_macport.h:602
@ ENET_MACPORT_IOCTL_GET_PREEMPTION_ENABLE_STATUS
Get preemption enable status.
Definition: enet_mod_macport.h:325
@ ENET_MAC_VERIFYSTATUS_SUCCEEDED
Definition: enet_mod_macport.h:564
Enet_MacPort macPort
Definition: enet_mod_macport.h:531
Input args for ENET_MACPORT_IOCTL_SET_PREEMPT_MIN_FRAG_SIZE.
Definition: enet_mod_macport.h:584
@ ENET_MAC_SUBLAYER_QUAD_SERIAL_MAIN
Definition: enet_mod_macport.h:396
EnetMac_LayerType layerType
Definition: enet_mod_macport.h:444
EnetMacPort_Ioctl
MAC port IOCTL commands.
Definition: enet_mod_macport.h:83
Enet_MacPort macPort
Definition: enet_mod_macport.h:519
EnetPort_PriorityMap priorityRegenMap
Definition: enet_mod_macport.h:510
Traffic shaping configuration for all priorities.
Definition: enet_mod_port.h:116
@ ENET_MACPORT_IOCTL_DISABLE_PREEMPTION
Disable frame preemption.
Definition: enet_mod_macport.h:334
@ ENET_MACPORT_VLAN_TYPE_SINGLE_TAG
Definition: enet_mod_macport.h:474
@ ENET_MACPORT_IOCTL_PRINT_REGS
Print MAC port registers.
Definition: enet_mod_macport.h:100
Input args for ENET_MACPORT_IOCTL_SET_PRI_REGEN_MAP command.
Definition: enet_mod_macport.h:505
Enet_MacPort macPort
Definition: enet_mod_macport.h:621
@ ENET_MAC_VERIFYSTATUS_RXRESPOND_ERROR
Definition: enet_mod_macport.h:573
Enet_Duplexity duplexity
Definition: enet_mod_macport.h:462
EnetPort_DscpPriorityMap dscpPriorityMap
Definition: enet_mod_macport.h:498
@ ENET_MAC_VERIFYSTATUS_RXVERIFY_ERROR
Definition: enet_mod_macport.h:576
Input args for ENET_MACPORT_IOCTL_SET_INGRESS_DSCP_PRI_MAP command.
Definition: enet_mod_macport.h:493
This file contains the type definitions and helper macros for the Enet Module interface.
@ ENET_MAC_VERIFYSTATE_VERIFYING
Definition: enet_mod_macport.h:561
@ ENET_MACPORT_IOCTL_GET_PREEMPT_MIN_FRAG_SIZE
Get minimum fragment size.
Definition: enet_mod_macport.h:271
EnetMacPort_QueuePreemptMode
Queue preemptive mode: express or preemptive.
Definition: enet_mod_macport.h:597
@ ENET_MACPORT_IOCTL_GET_VERSION
Get the hardware version of the MAC port module.
Definition: enet_mod_macport.h:91
static bool EnetMacPort_isXfi(const EnetMacPort_Interface *mii)
Check if interface is XFI.
Definition: enet_mod_macport.h:761
EnetMac_SublayerType
MAC interface sublayer type.
Definition: enet_mod_macport.h:385
Input args for ENET_MACPORT_IOCTL_SET_EGRESS_QOS_PRI_MAP command.
Definition: enet_mod_macport.h:517
@ ENET_MACPORT_IOCTL_GET_EGRESS_TRAFFIC_SHAPING
Get egress traffic shaping configuration.
Definition: enet_mod_macport.h:190
Input args for ENET_MACPORT_IOCTL_SET_CREDIT_BASED_SHAPING command.
Definition: enet_mod_macport.h:541
static bool EnetMacPort_isRgmii(const EnetMacPort_Interface *mii)
Check if interface is RGMII.
Definition: enet_mod_macport.h:742
@ ENET_MACPORT_IOCTL_IET_HOLD_PREEMPT_TRAFFIC
IET hold preemptible traffic.
Definition: enet_mod_macport.h:244
@ ENET_MACPORT_IOCTL_ENABLE_PREEMPTION
Enable IET frame preemption.
Definition: enet_mod_macport.h:343
@ ENET_MACPORT_IOCTL_SET_INGRESS_DSCP_PRI_MAP
Set ingress DSCP priority (TOS) map.
Definition: enet_mod_macport.h:118
@ ENET_MAC_VARIANT_NONE
Definition: enet_mod_macport.h:408
static bool EnetMacPort_isSgmii(const EnetMacPort_Interface *mii)
Check if interface is SGMII.
Definition: enet_mod_macport.h:748
EnetMac_SgmiiMode
SGMII mode.
Definition: enet_mod_macport.h:418
Credit Based shaping parameters (idleSlope).
Definition: enet_mod_port.h:107