|
AM263x MCU+ SDK
26.00.00
|
|
Go to the documentation of this file.
89 #define CPSW_COMMON_TX_MTU_DEFAULT (2024U)
99 #define CPSW_ESC_PRI_LD_VAL (2U)
102 #define CPSW_PER_PUBLIC_IOCTL(x) (ENET_IOCTL_TYPE_PUBLIC | \
103 ENET_IOCTL_PER_BASE | \
104 ENET_IOCTL_PER_CPSW | \
108 #if defined(SOC_AM273X) || defined(SOC_AWR294X) || defined (SOC_AWR2544)
109 #define CPSW_MAC_PORT_NUM (1U)
111 #define CPSW_MAC_PORT_NUM (8U)
124 #define CPSW_INTERVLAN_INGRESSPKT_MATCH_PORT (CPSW_ALE_POLICER_MATCH_PORT)
127 #define CPSW_INTERVLAN_INGRESSPKT_MATCH_MACSRC (CPSW_ALE_POLICER_MATCH_MACSRC)
130 #define CPSW_INTERVLAN_INGRESSPKT_MATCH_MACDST (CPSW_ALE_POLICER_MATCH_MACDST)
133 #define CPSW_INTERVLAN_INGRESSPKT_MATCH_ETHERTYPE (CPSW_ALE_POLICER_MATCH_ETHERTYPE)
136 #define CPSW_INTERVLAN_INGRESSPKT_MATCH_IPSRC (CPSW_ALE_POLICER_MATCH_IPSRC)
139 #define CPSW_INTERVLAN_INGRESSPKT_MATCH_IPDST (CPSW_ALE_POLICER_MATCH_IPDST)
144 #define CPSW_INTR_STATS_PEND0 (1U)
147 #define CPSW_INTR_MDIO_PEND (2U)
150 #define CPSW_INTR_EVNT_PEND (3U)
159 typedef enum Cpsw_Ioctl_e
220 typedef struct Cpsw_InterVlanRouteIngressPktMatchCfg_s
268 typedef struct Cpsw_InterVlanEgressPortCfg_s
282 typedef struct Cpsw_SetInterVlanRouteUniEgressInArgs_s
296 typedef struct Cpsw_SetInterVlanRouteUniEgressOutArgs_s
308 typedef struct Cpsw_ClearInterVlanRouteUniEgressInArgs_s
327 typedef struct Cpsw_SetInterVlanRouteMultiEgressInArgs_s
346 typedef struct Cpsw_SetInterVlanRouteMultiEgressOutArgs_s
358 typedef struct Cpsw_ClearInterVlanRouteMultiEgressInArgs_s
382 typedef struct Cpsw_SetTxShortIpgCfgInArgs_s
406 typedef struct Cpsw_TxShortIpgCfg_s
423 typedef struct Cpsw_VlanCfg_s
441 typedef struct Cpsw_MdioLinkStateChangeInfo_s
487 typedef struct Cpsw_Cfg_s
CpswAle_IpAddrClassifierInfo dstIpInfo
Definition: cpsw.h:257
Cpsw_InterVlanRouteIngressPktMatchCfg inPktMatchCfg
Definition: cpsw.h:371
ALE IP address classifier info.
Definition: cpsw_ale.h:1421
#define CPSW_MAC_PORT_NUM
Definition: cpsw.h:111
CpswCpts_Cfg cptsCfg
Definition: cpsw.h:510
#define CPSW_ALE_NUM_MAC_PORTS
Number of external ports in the subsystem.
Definition: cpsw_ale.h:96
This file contains the type definitions and helper macros for the Enet Data Path (DMA) interface.
CPSW-level VLAN configuration.
Definition: cpsw.h:424
bool enableQsgmii1RDC
Definition: cpsw.h:541
This file contains the type definitions and helper macros for the CPSW Address Lookup Engine (ALE) mo...
Enet_VlanTagType
Double tagging VLAN type.
Definition: enet_types.h:379
CpswAle_PolicerEntryOutArgs ingressPacketClassifierInfo
Definition: cpsw.h:352
Config structure for Enet CPDMA.
Definition: enet_cpdma.h:433
This file contains the type definitions and helper macros for the CPSW Statistics module interface.
This file contains the type definitions and helper macros for the MDIO module interface.
CpswAle_PolicerEntryOutArgs ingressPacketClassifierInfo
Definition: cpsw.h:302
Cpsw_Ioctl
CPSW peripheral IOCTL commands.
Definition: cpsw.h:160
ALE configuration.
Definition: cpsw_ale.h:2090
uint32_t phyAddr
Definition: cpsw.h:444
bool linkChanged
Definition: cpsw.h:455
Short IPG configuration for CPSW IP.
Definition: cpsw.h:407
void * mdioLinkStateChangeCbArg
Definition: cpsw.h:525
PHY link status change event information.
Definition: cpsw.h:442
void(* Cpsw_MdioLinkStateChangeCb)(Cpsw_MdioLinkStateChangeInfo *info, void *appArg)
CPSW PHY link state change callback function.
Definition: cpsw.h:468
bool aliveChanged
Definition: cpsw.h:448
Enet_MacPort
MAC port.
Definition: enet_types.h:412
Enet_MacPort egressPort
Definition: cpsw.h:271
CpswAle_MacAddrClassifierInfo srcMacAddrInfo
Definition: cpsw.h:239
bool configureGapThresh
Definition: cpsw.h:387
Enet_VlanTagType vlanSwitch
Definition: cpsw.h:429
MAC port's short gap configuration.
Definition: cpsw_macport.h:222
@ CPSW_PER_IOCTL_GET_SHORT_IPG_CFG
Get the current short inter-packet gap (IPG) configuration for all open MAC ports.
Definition: cpsw.h:214
This file contains the type definitions and helper macros for the Ethernet PHY interface.
Cpsw_InterVlanRouteIngressPktMatchCfg inPktMatchCfg
Definition: cpsw.h:287
uint32_t ipgTriggerThreshBlkCnt
Definition: cpsw.h:391
Resource manager configuration parameters.
Definition: enet_rm.h:402
uint32_t packetMatchEnMask
Definition: cpsw.h:224
Mdio_Cfg mdioCfg
Definition: cpsw.h:513
Port interVLAN configuration parameters.
Definition: cpsw_macport.h:258
CpswMacPort_InterVlanRouteId egressPortRouteId
Definition: cpsw.h:299
This file contains private type definitions and helper macros for the CPSW CPTS module.
Input args for CPSW_PER_IOCTL_CLEAR_INTERVLAN_ROUTE_UNI_EGRESS command.
Definition: cpsw.h:309
@ CPSW_PER_IOCTL_CLEAR_INTERVLAN_ROUTE_UNI_EGRESS
Setup interVLAN route for a single egress port.
Definition: cpsw.h:177
@ CPSW_PER_IOCTL_SET_SHORT_IPG_CFG
Configure short inter-packet gap (IPG) for specific MAC ports.
Definition: cpsw.h:204
const EnetDma_Cfg * dmaCfg
Definition: cpsw.h:493
CPSW configuration.
Definition: cpsw.h:488
uint16_t innerVlan
Definition: cpsw.h:435
CPTS configuration.
Definition: cpsw_cpts.h:591
Cpsw_InterVlanRouteIngressPktMatchCfg inPktMatchCfg
Definition: cpsw.h:313
CpswAle_MacAddrClassifierInfo dstMacAddrInfo
Definition: cpsw.h:244
uint32_t intrPriority
Definition: cpsw.h:519
bool vlanAware
Definition: cpsw.h:426
Output args for CPSW_PER_IOCTL_SET_INTERVLAN_ROUTE_UNI_EGRESS command.
Definition: cpsw.h:297
uint32_t vlanId
Definition: cpsw.h:247
MDIO module configuration.
Definition: networking/enet/core/include/mod/mdio.h:108
#define ENET_PRI_NUM
Packet priority.
Definition: enet_types.h:165
uint32_t numEgressPorts
Definition: cpsw.h:330
Cpsw_PortLinkStatusChangeCb portLinkStatusChangeCb
Definition: cpsw.h:529
uint32_t ipgTriggerThreshBlkCnt
Definition: cpsw.h:410
uint32_t escalatePriorityLoadVal
Definition: cpsw.h:490
Input args for CPSW_PER_IOCTL_SET_SHORT_IPG_CFG.
Definition: cpsw.h:383
Input args for CPSW_PER_IOCTL_SET_INTERVLAN_ROUTE_MULTI_EGRESS command.
Definition: cpsw.h:328
Input args for CPSW_PER_IOCTL_SET_INTERVLAN_ROUTE_UNI_EGRESS command.
Definition: cpsw.h:283
Input args for CPSW_PER_IOCTL_CLEAR_INTERVLAN_ROUTE_MULTI_EGRESS command.
Definition: cpsw.h:359
CpswHostPort_Cfg hostPortCfg
Definition: cpsw.h:504
InterVLAN egress port configuration.
Definition: cpsw.h:269
bool enableQsgmii0RDC
Definition: cpsw.h:538
@ CPSW_PER_IOCTL_SET_INTERVLAN_ROUTE_MULTI_EGRESS
Setup interVLAN route for a multiple egress port.
Definition: cpsw.h:186
void * portLinkStatusChangeCbArg
Definition: cpsw.h:532
This file contains the type definitions and helper macros for the CPSW MAC port module interface.
uint32_t delAleEntryMask
Definition: cpsw.h:376
Output args for CPSW_PER_IOCTL_SET_INTERVLAN_ROUTE_MULTI_EGRESS command.
Definition: cpsw.h:347
This file contains the type definitions and helper macros for the Enet Resource Manager module.
Cpsw_InterVlanRouteIngressPktMatchCfg inPktMatchCfg
Definition: cpsw.h:340
InterVLAN route ingress packet match criteria configuration.
Definition: cpsw.h:221
bool disablePhyDriver
Definition: cpsw.h:552
This file contains the type definitions and helper macros for the CPSW host port module.
uint32_t numMacPorts
Definition: cpsw.h:413
Output args for CPSW_ALE_IOCTL_GET_POLICER, CPSW_ALE_IOCTL_SET_POLICER_THREADCFG, CPSW_ALE_IOCTL_BLOC...
Definition: cpsw_ale.h:1596
#define CPSW_PER_PUBLIC_IOCTL(x)
Helper macro to create CPSW IOCTL commands.
Definition: cpsw.h:102
void(* Cpsw_PortLinkStatusChangeCb)(Enet_MacPort macPort, bool isLinkUp, void *appArg)
CPSW port link status change callback function.
Definition: cpsw.h:478
uint16_t etherType
Definition: cpsw.h:262
uint16_t outerVlan
Definition: cpsw.h:432
Enet_MacPort ingressPort
Definition: cpsw.h:234
CpswMacPort_InterVlanRouteId egressPortRouteId
Definition: cpsw.h:349
@ CPSW_PER_IOCTL_SET_INTERVLAN_ROUTE_UNI_EGRESS
Setup interVLAN route for a single egress port.
Definition: cpsw.h:168
ALE classifier/policer match parameters for source or destination MAC address.
Definition: cpsw_ale.h:1221
uint32_t numMacPorts
Definition: cpsw.h:394
Host port module configuration parameters.
Definition: cpsw_hostport.h:138
CpswMacPort_InterVlanRouteId
MAC port interVLAN route identifier.
Definition: cpsw_macport.h:234
Cpsw_VlanCfg vlanCfg
Definition: cpsw.h:496
uint32_t delAleEntryMask
Definition: cpsw.h:321
bool isAlive
Definition: cpsw.h:452
CpswAle_IpAddrClassifierInfo srcIpInfo
Definition: cpsw.h:252
bool ttlCheckEn
Definition: cpsw.h:229
CpswMacPort_InterVlanRoutingCfg outPktModCfg
Definition: cpsw.h:276
Cpsw_MdioLinkStateChangeCb mdioLinkStateChangeCb
Definition: cpsw.h:522
EnetRm_ResCfg resCfg
Definition: cpsw.h:516
Cpsw_InterVlanEgressPortCfg egressCfg
Definition: cpsw.h:290
Cpsw_InterVlanEgressPortCfg egressCfg
Definition: cpsw.h:316
CpswAle_Cfg aleCfg
Definition: cpsw.h:507
@ CPSW_PER_IOCTL_CLEAR_INTERVLAN_ROUTE_MULTI_EGRESS
Clear interVLAN route for a multiple egress port route.
Definition: cpsw.h:195
uint32_t numEgressPorts
Definition: cpsw.h:361
bool isLinked
Definition: cpsw.h:458