AM263x MCU+ SDK  26.00.00
bootloader.h
Go to the documentation of this file.
1 /*
2  * Copyright (C) 2021-2026 Texas Instruments Incorporated
3  *
4  * Redistribution and use in source and binary forms, with or without
5  * modification, are permitted provided that the following conditions
6  * are met:
7  *
8  * Redistributions of source code must retain the above copyright
9  * notice, this list of conditions and the following disclaimer.
10  *
11  * Redistributions in binary form must reproduce the above copyright
12  * notice, this list of conditions and the following disclaimer in the
13  * documentation and/or other materials provided with the
14  * distribution.
15  *
16  * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
21  * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
22  * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
23  * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
24  * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
25  * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
26  * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
27  * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
28  * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
29  * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
30  * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
32 
39 #ifndef BOOTLOADER_H_
40 #define BOOTLOADER_H_
41 
42 #include <stdint.h>
43 #include <kernel/dpl/SystemP.h>
44 #include <drivers/soc.h>
45 #include <drivers/hw_include/csl_types.h>
46 #include <drivers/hw_include/cslr_soc.h>
47 #include <drivers/bootloader/soc/bootloader_soc.h>
48 #include <drivers/bootloader/bootloader_profile.h>
49 #include <drivers/hw_include/soc_config.h>
50 
51 #ifdef __cplusplus
52 extern "C"
53 {
54 #endif
55 
68 #define BOOTLOADER_INVALID_ID (0xDEADBABE)
69 
73 #define BOOTLOADER_OPMODE_LOCKSTEP (0U)
74 #define BOOTLOADER_OPMODE_STANDALONE (1U)
75 
79 #define BOOTLOADER_MEDIA_MEM (0xB0070001)
80 #define BOOTLOADER_MEDIA_FLASH (0xB0070002)
81 #define BOOTLOADER_MEDIA_EMMC (0xB0070003)
82 #define BOOTLOADER_MEDIA_SD (0xB0070004)
83 #define BOOTLOADER_MEDIA_BUFIO (0xB0070005)
84 #define BOOTLOADER_MEDIA_PCIE (0xB0070006)
85 #define BOOTLOADER_MEDIA_USB (0xB0070007)
86 #define BOOTLOADER_MEDIA_UART (0xB0070008)
87 
91 #define BOOTLOADER_SCRATCH_MEM_ENABLE (1U)
92 
96 #define LINUX_LOAD_ONLY_IMAGE_ID (21U)
97 
101 typedef void* Bootloader_Handle;
102 
106 typedef struct Bootloader_Params_s
107 {
109  /* Base address of the appimage in case of a memory bootloader */
110 
111  uint8_t *bufIoTempBuf;
112  /* Temporary buffer to be used if the boot media is a buffered IO */
113 
115  /* Size of the temporary buffer to be used if the boot media is a buffered IO */
116 
118  /* Instance index of the IO device driver (UART) */
119 
120  char* fileName;
121  /*Pointer to the C string that hold name of file to be opened if the boot media is SD*/
122 
124 
142 typedef int32_t (*Bootloader_imgOpenFxn)(void *args, Bootloader_Params *params);
143 
156 typedef int32_t (*Bootloader_imgReadFxn)(void *dstAddr, uint32_t length, void *args);
157 
168 typedef uint32_t (*Bootloader_imgOffsetFxn)(void *args);
169 
181 typedef void (*Bootloader_imgSeekFxn)(uint32_t location, void *args);
182 
194 typedef void (*Bootloader_imgCloseFxn)(void* handle, void *args);
195 
206 typedef int32_t (*Bootloader_imgCustomFxn)(void *args);
207 
214 typedef struct Bootloader_Fxns_s
215 {
222 
224 
228 typedef struct Bootloader_Config_s
229 {
231  void *args;
232  uint32_t bootMedia;
233  uint32_t bootImageSize;
234  uint32_t coresPresentMap;
235  uint8_t *scratchMemPtr;
237  /* These options are for supporting HS-FS development, should be removed
238  after the boot time degradation is fixed for HS devices. */
241  /* Whether to initialize ICSS cores or not */
242  uint32_t initICSSCores;
244 
246 
247 #include <drivers/bootloader/bootloader_flash.h>
248 #include <drivers/bootloader/bootloader_mem.h>
249 #include <drivers/bootloader/bootloader_buf_io.h>
250 #if defined(SOC_AM64X) || defined(SOC_AM243X)
251 #include <drivers/bootloader/bootloader_uart.h>
252 #endif
253 
257 typedef struct Bootloader_CpuInfo_s
258 {
259  uint32_t cpuId;
260  uint32_t clkHz;
261  uint32_t rprcOffset;
262  uintptr_t entryPoint;
263 
265 
269 typedef struct Bootloader_BootImageInfo_s
270 {
272 
274 
281 
288 
295 
311 Bootloader_Handle Bootloader_open(uint32_t instanceNum, Bootloader_Params *openParams);
312 
319 
336 
353 
369 int32_t Bootloader_loadSelfCpu(Bootloader_Handle handle, Bootloader_CpuInfo *cpuInfo, uint32_t skipLoad);
370 
385 
399 
414 
427 
442 
451 int32_t Bootloader_cpuSetAppEntryPoint(Bootloader_BootImageInfo *bootImageInfo, uint32_t bDualSelfR5F);
452 
459 
466 
476 
486 
498 
511 uint32_t Bootloader_isCorePresent(Bootloader_Handle handle, uint32_t cslCoreId);
512 
523 
535 
536 #if defined(SOC_AM64X)
537 
547 int32_t Bootloader_parseAndLoadMultiCoreELFLinux(Bootloader_Handle handle, Bootloader_BootImageInfo *bootImageInfo);
548 #endif
549 
559 uint32_t Bootloader_getX509CertLen(uint8_t *x509_cert_ptr);
560 
571 uint32_t Bootloader_getMsgLen(uint8_t *x509_cert_ptr, uint32_t x509_cert_size);
572 
573 #if defined(SOC_AM64X) || defined(SOC_AM243X)
574 
589 int32_t Bootloader_UartParseAndLoadMultiCoreELF(Bootloader_Handle handle, Bootloader_BootImageInfo *bootImageInfo);
590 #endif
591 
593 #ifdef __cplusplus
594 }
595 #endif
596 
597 #endif
CSL_CORE_ID_MAX
#define CSL_CORE_ID_MAX
Definition: cslr_soc_defines.h:151
Bootloader_Config::coresPresentMap
uint32_t coresPresentMap
Definition: bootloader.h:234
args
void * args
Definition: hsmclient_msg.h:4
Bootloader_Config::fxns
Bootloader_Fxns * fxns
Definition: bootloader.h:230
Bootloader_Config::disableAppImageAuth
uint32_t disableAppImageAuth
Definition: bootloader.h:240
Bootloader_isCorePresent
uint32_t Bootloader_isCorePresent(Bootloader_Handle handle, uint32_t cslCoreId)
API to check if a particular core's image is present in the multicore image.
Bootloader_Params::memArgsAppImageBaseAddr
uint32_t memArgsAppImageBaseAddr
Definition: bootloader.h:108
SystemP.h
Bootloader_bootSelfCpu
int32_t Bootloader_bootSelfCpu(Bootloader_Handle handle, Bootloader_BootImageInfo *bootImageInfo)
API to boot self CPU.
Bootloader_imgCloseFxn
void(* Bootloader_imgCloseFxn)(void *handle, void *args)
Driver implementation to close a specific bootloader driver - Memory, OSPI, UART, MMCSD etc.
Definition: bootloader.h:194
Bootloader_rprcImageParseEntryPoint
int32_t Bootloader_rprcImageParseEntryPoint(Bootloader_Handle handle, Bootloader_CpuInfo *cpuInfo)
Parse entrypoint from RPRC.
Bootloader_getBootMedia
uint32_t Bootloader_getBootMedia(Bootloader_Handle handle)
API to get the selected boot media in the bootloader instance.
Bootloader_Fxns::imgOpenFxn
Bootloader_imgOpenFxn imgOpenFxn
Definition: bootloader.h:216
Bootloader_BootImageInfo_init
void Bootloader_BootImageInfo_init(Bootloader_BootImageInfo *bootImageInfo)
Initialize BootImage info.
Bootloader_Config::isAppimageSigned
uint32_t isAppimageSigned
Definition: bootloader.h:239
Bootloader_Params::bufIoDeviceIndex
uint32_t bufIoDeviceIndex
Definition: bootloader.h:117
Bootloader_Params_init
void Bootloader_Params_init(Bootloader_Params *params)
Initialize Bootloader params.
Bootloader_getMulticoreImageSize
uint32_t Bootloader_getMulticoreImageSize(Bootloader_Handle handle)
API to fetch the size of the multicore image.
Bootloader_CpuInfo::rprcOffset
uint32_t rprcOffset
Definition: bootloader.h:261
Bootloader_Config::args
void * args
Definition: bootloader.h:231
Bootloader_Fxns::imgSeekFxn
Bootloader_imgSeekFxn imgSeekFxn
Definition: bootloader.h:219
Bootloader_runSelfCpuWithLinux
int32_t Bootloader_runSelfCpuWithLinux(void)
API to boot self CPU with Linux.
Bootloader_parseAndLoadMultiCoreELF
int32_t Bootloader_parseAndLoadMultiCoreELF(Bootloader_Handle handle, Bootloader_BootImageInfo *bootImageInfo)
API to parse and load MCELF image.
Bootloader_Params::bufIoTempBuf
uint8_t * bufIoTempBuf
Definition: bootloader.h:111
Bootloader_parseMultiCoreAppImage
int32_t Bootloader_parseMultiCoreAppImage(Bootloader_Handle handle, Bootloader_BootImageInfo *bootImageInfo)
Parse Multicore Appimage.
Bootloader_Config
Bootloader driver configuration, these are filled by SysCfg based on the boot media selected.
Definition: bootloader.h:229
Bootloader_imgCustomFxn
int32_t(* Bootloader_imgCustomFxn)(void *args)
Driver implementation to enable a custom function for a specific bootloader driver - Memory,...
Definition: bootloader.h:206
Bootloader_imgOffsetFxn
uint32_t(* Bootloader_imgOffsetFxn)(void *args)
Driver implementation to get the current offset in the boot media.
Definition: bootloader.h:168
Bootloader_Fxns::imgOffsetFxn
Bootloader_imgOffsetFxn imgOffsetFxn
Definition: bootloader.h:218
Bootloader_close
void Bootloader_close(Bootloader_Handle handle)
Close bootloader driver.
Bootloader_Config::socCoreOpMode
void * socCoreOpMode
Definition: bootloader.h:236
Bootloader_cpuSetAppEntryPoint
int32_t Bootloader_cpuSetAppEntryPoint(Bootloader_BootImageInfo *bootImageInfo, uint32_t bDualSelfR5F)
Set Application entry point for self CPU in the AM65x SOC from reset.
Bootloader_loadSelfCpu
int32_t Bootloader_loadSelfCpu(Bootloader_Handle handle, Bootloader_CpuInfo *cpuInfo, uint32_t skipLoad)
API to load self CPU.
Bootloader_bootCpu
int32_t Bootloader_bootCpu(Bootloader_Handle handle, Bootloader_CpuInfo *cpuInfo)
API to boot a non-self CPU.
Bootloader_runCpu
int32_t Bootloader_runCpu(Bootloader_Handle handle, Bootloader_CpuInfo *cpuInfo)
API to run a non-self CPU.
Bootloader_Config::bootImageSize
uint32_t bootImageSize
Definition: bootloader.h:233
Bootloader_Params::bufIoTempBufSize
uint32_t bufIoTempBufSize
Definition: bootloader.h:114
Bootloader_Params::fileName
char * fileName
Definition: bootloader.h:120
Bootloader_getMsgLen
uint32_t Bootloader_getMsgLen(uint8_t *x509_cert_ptr, uint32_t x509_cert_size)
API to get image length from a x509 certificate.
Bootloader_CpuInfo::clkHz
uint32_t clkHz
Definition: bootloader.h:260
Bootloader_CpuInfo::cpuId
uint32_t cpuId
Definition: bootloader.h:259
Bootloader_CpuInfo
Data structure containing information related to a particular CPU, required for RPRC loading.
Definition: bootloader.h:258
Bootloader_imgOpenFxn
int32_t(* Bootloader_imgOpenFxn)(void *args, Bootloader_Params *params)
Driver implementation to open a specific bootloader driver - Memory, OSPI, UART, MMCSD etc.
Definition: bootloader.h:142
Bootloader_BootImageInfo
Data structure containing information related all CPUs, this will be filled by Bootloader_parseMultiC...
Definition: bootloader.h:270
Bootloader_Config::bootMedia
uint32_t bootMedia
Definition: bootloader.h:232
Bootloader_runSelfCpu
int32_t Bootloader_runSelfCpu(Bootloader_Handle handle, Bootloader_BootImageInfo *bootImageInfo)
API to boot self CPU.
Bootloader_Fxns::imgCustomFxn
Bootloader_imgCustomFxn imgCustomFxn
Definition: bootloader.h:221
Bootloader_initCpu
int32_t Bootloader_initCpu(Bootloader_Handle handle, Bootloader_CpuInfo *cpuInfo)
API to initialize a non-self CPU.
Bootloader_rprcImageLoad
int32_t Bootloader_rprcImageLoad(Bootloader_Handle handle, Bootloader_CpuInfo *cpuInfo)
Load application binaries into SOC memory.
Bootloader_imgSeekFxn
void(* Bootloader_imgSeekFxn)(uint32_t location, void *args)
Driver implementation to read from boot media using a specific bootloader driver - Memory,...
Definition: bootloader.h:181
Bootloader_Fxns::imgCloseFxn
Bootloader_imgCloseFxn imgCloseFxn
Definition: bootloader.h:220
Bootloader_parseAndLoadLinuxAppImage
int32_t Bootloader_parseAndLoadLinuxAppImage(Bootloader_Handle handle, Bootloader_BootImageInfo *bootImageInfo)
Parse and load linux Appimage, containing linux binaries(ATF, OPTEE, SPL)
Bootloader_Fxns
Driver implementation callbacks.
Definition: bootloader.h:215
Bootloader_getX509CertLen
uint32_t Bootloader_getX509CertLen(uint8_t *x509_cert_ptr)
API to get the length of an x509 certificate.
Bootloader_Config::enableScratchMem
uint32_t enableScratchMem
Definition: bootloader.h:243
Bootloader_imgReadFxn
int32_t(* Bootloader_imgReadFxn)(void *dstAddr, uint32_t length, void *args)
Driver implementation to read from boot media using a specific bootloader driver - Memory,...
Definition: bootloader.h:156
Bootloader_Handle
void * Bootloader_Handle
Handle to the Bootloader driver returned by Bootloader_open()
Definition: bootloader.h:101
Bootloader_CpuInfo_init
void Bootloader_CpuInfo_init(Bootloader_CpuInfo *cpuInfo)
Initialize CPU info.
Bootloader_Params
Parameters passed during Bootloader_open()
Definition: bootloader.h:107
Bootloader_open
Bootloader_Handle Bootloader_open(uint32_t instanceNum, Bootloader_Params *openParams)
Open bootloader driver.
Bootloader_loadCpu
int32_t Bootloader_loadCpu(Bootloader_Handle handle, Bootloader_CpuInfo *cpuInfo)
API to load a non-self CPU.
Bootloader_Config::scratchMemPtr
uint8_t * scratchMemPtr
Definition: bootloader.h:235
Bootloader_CpuInfo::entryPoint
uintptr_t entryPoint
Definition: bootloader.h:262
Bootloader_Config::initICSSCores
uint32_t initICSSCores
Definition: bootloader.h:242
Bootloader_Fxns::imgReadFxn
Bootloader_imgReadFxn imgReadFxn
Definition: bootloader.h:217