AM263x MCU+ SDK  09.02.00
V1/sdl_ip_ecc.h
Go to the documentation of this file.
1 
40 #ifndef SDL_ECC_AGGR_H
41 #define SDL_ECC_AGGR_H
42 
43 #ifdef __cplusplus
44 extern "C" {
45 #endif
46 
47 #include <stdint.h>
48 #include <stdbool.h>
49 #include <sdl/ecc/sdlr_ecc.h>
50 
100 #define SDL_ECC_AGGR_INTR_SRC_NONE ((uint32_t) 0U)
101 
102 #define SDL_ECC_AGGR_INTR_SRC_SINGLE_BIT ((uint32_t) 1U)
103 
104 #define SDL_ECC_AGGR_INTR_SRC_DOUBLE_BIT ((uint32_t) 2U)
105 
106 #define SDL_ECC_ADDR_ERROR_TYPE_SUCCESSIVE_SINGLE_BITS ((uint32_t) 3U)
107 
108 #define SDL_ECC_AGGR_INTR_SRC_INVALID ((uint32_t) 4U)
109 
116 #define SDL_ECC_AGGR_SELECT_ERR_CTRL1 (0U)
117 
118 #define SDL_ECC_AGGR_SELECT_ERR_CTRL2 (1U)
119 
120 #define SDL_ECC_AGGR_MAX_NUM_RAM_ERR_CTRL (2U)
121 
128 #define SDL_ECC_AGGR_SELECT_ERR_STAT1 (0U)
129 
130 #define SDL_ECC_AGGR_SELECT_ERR_STAT2 (1U)
131 
132 #define SDL_ECC_AGGR_SELECT_ERR_STAT3 (2U)
133 
134 #define SDL_ECC_AGGR_MAX_NUM_RAM_ERR_STAT (3U)
135 
136 
142 #define SDL_ECC_AGGR_NUM_ENABLE_REGISTERS (8U)
143 
144 #define SDL_ECC_AGGR_VALID_TIMEOUT_ERR (1U)
145 
146 #define SDL_ECC_AGGR_VALID_PARITY_ERR (2U)
147 
149 #define SDL_ECC_AGGR_INJECT_PATTERN_ZERO ((uint32_t) 0U)
150 
151 #define SDL_ECC_AGGR_INJECT_PATTERN_F ((uint32_t) 1U)
152 
153 #define SDL_ECC_AGGR_INJECT_PATTERN_A ((uint32_t) 2U)
154 
155 #define SDL_ECC_AGGR_INJECT_PATTERN_5 ((uint32_t) 3U)
156 /* Max Inject pattern */
157 #define SDL_ECC_EGGR_INJECT_PATTERN_MAX (SDL_ECC_AGGR_INJECT_PATTERN_A)
158 
160 #define SDL_ECC_AGGR_ERROR_SUBTYPE_NORMAL ((uint32_t) 0U)
161 
162 #define SDL_ECC_AGGR_ERROR_SUBTYPE_INJECT ((uint32_t) 1U)
163 
181 typedef uint32_t SDL_Ecc_AggrIntrSrc;
182 
183 
191 
192 
198 typedef uint8_t SDL_ecc_aggrValid;
199 
206 typedef uint32_t SDL_Ecc_injectPattern;
222 typedef struct
223 {
227  uint32_t eccRow;
229  uint32_t eccBit1;
231  uint32_t eccBit2;
235  bool bNextRow;
237 
245 typedef struct
246 {
258  uint32_t eccRow;
260  uint32_t eccBit1;
266 
273 typedef struct {
281 
288 typedef struct {
294  uint32_t timeOutCnt;
296  uint32_t parityCnt;
300 
301 
302 
310 typedef struct {
312  uint32_t REV;
314  uint32_t ECC_CTRL;
316  uint32_t ECC_ERR_CTRL1;
318  uint32_t ECC_ERR_CTRL2;
320  uint32_t ECC_SEC_ENABLE_SET_REG[SDL_ECC_AGGR_NUM_ENABLE_REGISTERS];
322  uint32_t ECC_SEC_ENABLE_CLR_REG[SDL_ECC_AGGR_NUM_ENABLE_REGISTERS];
324  uint32_t ECC_DED_ENABLE_SET_REG[SDL_ECC_AGGR_NUM_ENABLE_REGISTERS];
326  uint32_t ECC_DED_ENABLE_CLR_REG[SDL_ECC_AGGR_NUM_ENABLE_REGISTERS];
328 
363 int32_t SDL_ecc_aggrGetRevision(const SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t *pRev);
364 
388 int32_t SDL_ecc_aggrGetNumRams(const SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t *pNumRams);
389 
417 int32_t SDL_ecc_aggrReadEccRamReg(SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, uint32_t regOffset, uint32_t *pRegVal);
418 
444 int32_t SDL_ecc_aggrReadEccRamWrapRevReg(SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, uint32_t *pRegVal);
445 
472 int32_t SDL_ecc_aggrReadEccRamCtrlReg(SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, uint32_t *pRegVal);
473 
494 int32_t SDL_ecc_aggrReadEccRamErrCtrlReg(SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, uint32_t instSelect, uint32_t *pRegVal);
495 
516 int32_t SDL_ecc_aggrReadEccRamErrStatReg(SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, uint32_t instSelect, uint32_t *pRegVal);
517 
543 int32_t SDL_ecc_aggrWriteEccRamReg(SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, uint32_t regOffset, uint32_t val);
544 
568 int32_t SDL_ecc_aggrWriteEccRamCtrlReg(SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, uint32_t val);
569 
595 int32_t SDL_ecc_aggrWriteEccRamErrCtrlReg(SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, uint32_t instSelect, uint32_t val);
596 
621 int32_t SDL_ecc_aggrWriteEccRamErrStatReg(SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, uint32_t instSelect, uint32_t val);
622 
648 int32_t SDL_ecc_aggrConfigEccRam(SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, bool bEnable, bool bEccCheck, bool bEnableRMW);
649 
676 int32_t SDL_ecc_aggrVerifyConfigEccRam(SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, bool bEnable, bool bEccCheck, bool bEnableRMW);
677 
702 int32_t SDL_ecc_aggrGetEccRamErrorStatus(SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, SDL_Ecc_AggrEccRamErrorStatusInfo *pEccErrorStatus);
703 
728 int32_t SDL_ecc_aggrForceEccRamError(SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, const SDL_Ecc_AggrErrorInfo *pEccForceError);
729 
755 
786 int32_t SDL_ecc_aggrIsEccRamIntrPending(SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, SDL_Ecc_AggrIntrSrc intrSrc, bool *pIsPend);
787 
813 int32_t SDL_ecc_aggrSetEccRamIntrPending(SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, SDL_Ecc_AggrIntrSrc intrSrc);
814 
842 int32_t SDL_ecc_aggrSetEccRamNIntrPending(SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, SDL_Ecc_AggrIntrSrc intrSrc, uint32_t numEvents);
843 
869 int32_t SDL_ecc_aggrClrEccRamIntrPending(SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, SDL_Ecc_AggrIntrSrc intrSrc);
870 
897 int32_t SDL_ecc_aggrClrEccRamNIntrPending(SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, SDL_Ecc_AggrIntrSrc intrSrc, uint32_t numEvents);
898 
930 int32_t SDL_ecc_aggrIsIntrPending(const SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, SDL_Ecc_AggrIntrSrc intrSrc, bool *pIsPend);
931 
955 int32_t SDL_ecc_aggrIsAnyIntrPending(const SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, bool *pIsPend);
956 
982 int32_t SDL_ecc_aggrEnableIntr(const SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, SDL_Ecc_AggrIntrSrc intrSrc);
983 
1009 int32_t SDL_ecc_aggrDisableIntr(const SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, SDL_Ecc_AggrIntrSrc intrSrc);
1010 
1034 int32_t SDL_ecc_aggrEnableAllIntr(const SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId);
1035 
1059 int32_t SDL_ecc_aggrDisableAllIntr(const SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId);
1060 
1085 int32_t SDL_ecc_aggrEnableIntrs(const SDL_ecc_aggrRegs *pEccAggrRegs, SDL_Ecc_AggrIntrSrc intrSrc);
1086 
1111 int32_t SDL_ecc_aggrDisableIntrs(const SDL_ecc_aggrRegs *pEccAggrRegs, SDL_Ecc_AggrIntrSrc intrSrc);
1112 
1135 int32_t SDL_ecc_aggrEnableAllIntrs(const SDL_ecc_aggrRegs *pEccAggrRegs);
1136 
1159 int32_t SDL_ecc_aggrDisableAllIntrs(const SDL_ecc_aggrRegs *pEccAggrRegs);
1160 
1184 int32_t SDL_ecc_aggrReadStaticRegs(SDL_ecc_aggrRegs *pEccAggrRegs, SDL_ECC_staticRegs *pEccAggrStaticRegs);
1185 
1209 int32_t SDL_ecc_aggrIntrEnableCtrl(SDL_ecc_aggrRegs *pEccAggrRegs, const SDL_ecc_aggrEnableCtrl *pEnableCtrl);
1210 
1211 
1236 int32_t SDL_ecc_aggrIntrStatusCtrl(SDL_ecc_aggrRegs *pEccAggrRegs, const SDL_ecc_aggrStatusCtrl *pStatusCtrl);
1237 
1263 int32_t SDL_ecc_aggrIntrGetStatus(const SDL_ecc_aggrRegs *pEccAggrRegs, SDL_ecc_aggrStatusCtrl *pStatusCtrl);
1264 
1265 
1268 #ifdef __cplusplus
1269 }
1270 #endif
1271 
1272 #endif
SDL_ecc_aggrWriteEccRamErrStatReg
int32_t SDL_ecc_aggrWriteEccRamErrStatReg(SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, uint32_t instSelect, uint32_t val)
SDL_ecc_aggrAckIntr
int32_t SDL_ecc_aggrAckIntr(SDL_ecc_aggrRegs *pEccAggrRegs, SDL_Ecc_AggrIntrSrc intrSrc)
SDL_ecc_aggrDisableIntr
int32_t SDL_ecc_aggrDisableIntr(const SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, SDL_Ecc_AggrIntrSrc intrSrc)
SDL_ecc_aggrWriteEccRamReg
int32_t SDL_ecc_aggrWriteEccRamReg(SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, uint32_t regOffset, uint32_t val)
SDL_ecc_aggrStatusCtrl::timeOutCnt
uint32_t timeOutCnt
Definition: V1/sdl_ip_ecc.h:294
SDL_ecc_aggrSetEccRamNIntrPending
int32_t SDL_ecc_aggrSetEccRamNIntrPending(SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, SDL_Ecc_AggrIntrSrc intrSrc, uint32_t numEvents)
SDL_Ecc_AggrEccRamErrorStatusInfo::singleBitErrorCount
uint32_t singleBitErrorCount
Definition: V1/sdl_ip_ecc.h:262
SDL_ECC_staticRegs::REV
uint32_t REV
Definition: V1/sdl_ip_ecc.h:312
SDL_Ecc_AggrEccRamErrorStatusInfo
This structure contains error status information returned by the SDL_ecc_aggrGetEccRamGetErrorStatus ...
Definition: V1/sdl_ip_ecc.h:246
SDL_Ecc_AggrEDCErrorSubType
uint32_t SDL_Ecc_AggrEDCErrorSubType
This enumerator defines the types of possible EDC errors.
Definition: V1/sdl_ip_ecc.h:190
SDL_ecc_aggrIsIntrPending
int32_t SDL_ecc_aggrIsIntrPending(const SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, SDL_Ecc_AggrIntrSrc intrSrc, bool *pIsPend)
SDL_ECC_staticRegs::ECC_CTRL
uint32_t ECC_CTRL
Definition: V1/sdl_ip_ecc.h:314
SDL_ecc_aggrClrEccRamNIntrPending
int32_t SDL_ecc_aggrClrEccRamNIntrPending(SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, SDL_Ecc_AggrIntrSrc intrSrc, uint32_t numEvents)
SDL_ecc_aggrRegs
Definition: V1/sdlr_ecc.h:53
SDL_Ecc_AggrErrorInfo::intrSrc
SDL_Ecc_AggrIntrSrc intrSrc
Definition: V1/sdl_ip_ecc.h:225
SDL_Ecc_AggrErrorInfo::bNextRow
bool bNextRow
Definition: V1/sdl_ip_ecc.h:235
SDL_ecc_aggrEnableCtrl::intrEnableTimeoutErr
bool intrEnableTimeoutErr
Definition: V1/sdl_ip_ecc.h:275
sdlr_ecc.h
SDL_ecc_aggrDisableIntrs
int32_t SDL_ecc_aggrDisableIntrs(const SDL_ecc_aggrRegs *pEccAggrRegs, SDL_Ecc_AggrIntrSrc intrSrc)
SDL_ecc_aggrForceEccRamError
int32_t SDL_ecc_aggrForceEccRamError(SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, const SDL_Ecc_AggrErrorInfo *pEccForceError)
SDL_ecc_aggrReadStaticRegs
int32_t SDL_ecc_aggrReadStaticRegs(SDL_ecc_aggrRegs *pEccAggrRegs, SDL_ECC_staticRegs *pEccAggrStaticRegs)
SDL_ecc_aggrClrEccRamIntrPending
int32_t SDL_ecc_aggrClrEccRamIntrPending(SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, SDL_Ecc_AggrIntrSrc intrSrc)
SDL_Ecc_AggrErrorInfo::eccBit1
uint32_t eccBit1
Definition: V1/sdl_ip_ecc.h:229
SDL_ecc_aggrIntrEnableCtrl
int32_t SDL_ecc_aggrIntrEnableCtrl(SDL_ecc_aggrRegs *pEccAggrRegs, const SDL_ecc_aggrEnableCtrl *pEnableCtrl)
SDL_ecc_aggrStatusCtrl::intrStatusSetTimeoutErr
bool intrStatusSetTimeoutErr
Definition: V1/sdl_ip_ecc.h:290
SDL_ecc_aggrReadEccRamErrStatReg
int32_t SDL_ecc_aggrReadEccRamErrStatReg(SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, uint32_t instSelect, uint32_t *pRegVal)
SDL_ecc_aggrEnableAllIntrs
int32_t SDL_ecc_aggrEnableAllIntrs(const SDL_ecc_aggrRegs *pEccAggrRegs)
SDL_Ecc_AggrErrorInfo
This structure contains error forcing information used by the SDL_ecc_aggrForceEccRamError function.
Definition: V1/sdl_ip_ecc.h:223
SDL_ecc_aggrWriteEccRamErrCtrlReg
int32_t SDL_ecc_aggrWriteEccRamErrCtrlReg(SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, uint32_t instSelect, uint32_t val)
SDL_ecc_aggrStatusCtrl::parityCnt
uint32_t parityCnt
Definition: V1/sdl_ip_ecc.h:296
SDL_ECC_staticRegs::ECC_ERR_CTRL1
uint32_t ECC_ERR_CTRL1
Definition: V1/sdl_ip_ecc.h:316
SDL_ECC_staticRegs::ECC_ERR_CTRL2
uint32_t ECC_ERR_CTRL2
Definition: V1/sdl_ip_ecc.h:318
SDL_ecc_aggrValid
uint8_t SDL_ecc_aggrValid
This defines the valid ecc aggr error configuration.
Definition: V1/sdl_ip_ecc.h:198
SDL_ecc_aggrReadEccRamErrCtrlReg
int32_t SDL_ecc_aggrReadEccRamErrCtrlReg(SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, uint32_t instSelect, uint32_t *pRegVal)
SDL_Ecc_AggrEccRamErrorStatusInfo::controlRegErr
bool controlRegErr
Definition: V1/sdl_ip_ecc.h:248
SDL_ecc_aggrStatusCtrl::intrStatusSetParityErr
bool intrStatusSetParityErr
Definition: V1/sdl_ip_ecc.h:292
SDL_ECC_staticRegs
This structure contains the static register group for Ecc aggregator used by the SDL_ecc_aggrReadStat...
Definition: V1/sdl_ip_ecc.h:310
SDL_ecc_aggrReadEccRamCtrlReg
int32_t SDL_ecc_aggrReadEccRamCtrlReg(SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, uint32_t *pRegVal)
SDL_ecc_aggrIntrStatusCtrl
int32_t SDL_ecc_aggrIntrStatusCtrl(SDL_ecc_aggrRegs *pEccAggrRegs, const SDL_ecc_aggrStatusCtrl *pStatusCtrl)
SDL_ECC_AGGR_NUM_ENABLE_REGISTERS
#define SDL_ECC_AGGR_NUM_ENABLE_REGISTERS
This defines the number of enable registers.
Definition: V1/sdl_ip_ecc.h:142
SDL_Ecc_AggrEccRamErrorStatusInfo::eccBit1
uint32_t eccBit1
Definition: V1/sdl_ip_ecc.h:260
SDL_ecc_aggrReadEccRamReg
int32_t SDL_ecc_aggrReadEccRamReg(SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, uint32_t regOffset, uint32_t *pRegVal)
SDL_Ecc_AggrErrorInfo::eccBit2
uint32_t eccBit2
Definition: V1/sdl_ip_ecc.h:231
SDL_ecc_aggrEnableCtrl::intrEnableParityErr
bool intrEnableParityErr
Definition: V1/sdl_ip_ecc.h:277
SDL_Ecc_AggrEccRamErrorStatusInfo::eccRow
uint32_t eccRow
Definition: V1/sdl_ip_ecc.h:258
SDL_ecc_aggrEnableIntrs
int32_t SDL_ecc_aggrEnableIntrs(const SDL_ecc_aggrRegs *pEccAggrRegs, SDL_Ecc_AggrIntrSrc intrSrc)
SDL_Ecc_AggrErrorInfo::bOneShotMode
bool bOneShotMode
Definition: V1/sdl_ip_ecc.h:233
SDL_Ecc_AggrEccRamErrorStatusInfo::parityErrorCount
uint32_t parityErrorCount
Definition: V1/sdl_ip_ecc.h:256
SDL_Ecc_AggrEccRamErrorStatusInfo::writebackPend
bool writebackPend
Definition: V1/sdl_ip_ecc.h:254
SDL_ecc_aggrDisableAllIntrs
int32_t SDL_ecc_aggrDisableAllIntrs(const SDL_ecc_aggrRegs *pEccAggrRegs)
SDL_ecc_aggrEnableCtrl::validCfg
SDL_ecc_aggrValid validCfg
Definition: V1/sdl_ip_ecc.h:279
SDL_Ecc_AggrIntrSrc
uint32_t SDL_Ecc_AggrIntrSrc
This enumerator defines the types of possible ECC errors.
Definition: V1/sdl_ip_ecc.h:181
SDL_Ecc_injectPattern
uint32_t SDL_Ecc_injectPattern
This enumerator defines the types of ECC patterns.
Definition: V1/sdl_ip_ecc.h:206
SDL_Ecc_AggrEccRamErrorStatusInfo::sVBUSTimeoutErr
bool sVBUSTimeoutErr
Definition: V1/sdl_ip_ecc.h:252
SDL_ecc_aggrVerifyConfigEccRam
int32_t SDL_ecc_aggrVerifyConfigEccRam(SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, bool bEnable, bool bEccCheck, bool bEnableRMW)
SDL_ecc_aggrGetNumRams
int32_t SDL_ecc_aggrGetNumRams(const SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t *pNumRams)
SDL_ecc_aggrWriteEccRamCtrlReg
int32_t SDL_ecc_aggrWriteEccRamCtrlReg(SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, uint32_t val)
SDL_Ecc_AggrEccRamErrorStatusInfo::doubleBitErrorCount
uint32_t doubleBitErrorCount
Definition: V1/sdl_ip_ecc.h:264
SDL_ecc_aggrStatusCtrl
This structure contains the ECC aggr status config.
Definition: V1/sdl_ip_ecc.h:288
SDL_Ecc_AggrEccRamErrorStatusInfo::successiveSingleBitErr
bool successiveSingleBitErr
Definition: V1/sdl_ip_ecc.h:250
SDL_ecc_aggrEnableCtrl
This structure contains the ECC aggr enable error config.
Definition: V1/sdl_ip_ecc.h:273
SDL_ecc_aggrEnableAllIntr
int32_t SDL_ecc_aggrEnableAllIntr(const SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId)
SDL_ecc_aggrGetEccRamErrorStatus
int32_t SDL_ecc_aggrGetEccRamErrorStatus(SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, SDL_Ecc_AggrEccRamErrorStatusInfo *pEccErrorStatus)
SDL_ecc_aggrIsAnyIntrPending
int32_t SDL_ecc_aggrIsAnyIntrPending(const SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, bool *pIsPend)
SDL_ecc_aggrEnableIntr
int32_t SDL_ecc_aggrEnableIntr(const SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, SDL_Ecc_AggrIntrSrc intrSrc)
SDL_ecc_aggrIntrGetStatus
int32_t SDL_ecc_aggrIntrGetStatus(const SDL_ecc_aggrRegs *pEccAggrRegs, SDL_ecc_aggrStatusCtrl *pStatusCtrl)
SDL_ecc_aggrGetRevision
int32_t SDL_ecc_aggrGetRevision(const SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t *pRev)
SDL_ecc_aggrDisableAllIntr
int32_t SDL_ecc_aggrDisableAllIntr(const SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId)
SDL_ecc_aggrIsEccRamIntrPending
int32_t SDL_ecc_aggrIsEccRamIntrPending(SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, SDL_Ecc_AggrIntrSrc intrSrc, bool *pIsPend)
SDL_ecc_aggrSetEccRamIntrPending
int32_t SDL_ecc_aggrSetEccRamIntrPending(SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, SDL_Ecc_AggrIntrSrc intrSrc)
SDL_ecc_aggrStatusCtrl::validCfg
SDL_ecc_aggrValid validCfg
Definition: V1/sdl_ip_ecc.h:298
SDL_Ecc_AggrErrorInfo::eccRow
uint32_t eccRow
Definition: V1/sdl_ip_ecc.h:227
SDL_ecc_aggrConfigEccRam
int32_t SDL_ecc_aggrConfigEccRam(SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, bool bEnable, bool bEccCheck, bool bEnableRMW)
SDL_ecc_aggrReadEccRamWrapRevReg
int32_t SDL_ecc_aggrReadEccRamWrapRevReg(SDL_ecc_aggrRegs *pEccAggrRegs, uint32_t ramId, uint32_t *pRegVal)