AM263x MCU+ SDK  26.00.00
Ethernet AVTP Example

Introduction

This ethernet AVTP example illustrates the usage of IEEE Std 1722™-2016 stack with CPSW peripheral.

In this example, the DUT MAC port is connected to a PC which can act as either AVTP Talker or AVTP Listener. In the talker example, the DUT sends audio stream in AVTP PCM format to PC, where PC logs the received PCM data in a output file. In the listener example, the PC streams the Audio from an input file and DUT receives the Audio data and prints the info to the console. Yang based configuration is also supported in the stack, However file System is not supported yet, hence full yang based support will be added in the future releases.

See also :Ethernet AVB Stack - API and Integration Guide

Supported Combinations

Parameter Value
CPU + OS mcu-r5fss0-0_freertos
Toolchain ti-arm-clang
Board am263x-cc
Example folder source/networking/enet/core/examples/tsn/aafpcmlistener_app, aafpcmtalker_app

Prerequisites

  • EVM Board
  • Cat6 ethernet cable
  • PC with Linux Ubuntu OS with wireshark, xl4 deb build installed.
  • ffplay on PC (Optional, can be used to listen to recorded audio)

Steps to Run the Example

To start AVB app on PC, follow below steps:

  • Create a workspace to run avtp app.
    $ mkdir avbrun_demo && cd avbrun_demo
    $ avbrun -w rnn-cl -d enp3s0 -o setcaps=1
  • This creates a file named avbrun.cfg. open the file and modify [DEFAULT] field, uniconf_conf = uniconf.conf,streaminfo.conf
  • To use Excelfore avbrun as talker, modify avbrun.cfg to read/send AVTP data from wav file
    [Talker] `conl2t_extops: conl2t_extops = --src afile --mfile file_example_WAV_10MG.wav
  • To read/send AVTP data from wav file, modify this line in avbrun.cfg
    conl2t_extops = --src afile --mfile BeepBeep.pcm --conf conl2_talker.conf -C 2 -P 180 -F s16be
    Argument Description
    -C Channel number
    -F Format audio 16be
    -P Number of sample per frame
  • To read/send AVTP data from ec3 file, modify this line in avbrun.cfg
    conl2t_extops = --src afile --format aes32 --mfile in.ec3
  • To use Excelfore avbrun as listener and dump the output in PCM format, modify this line in avbrun.cfg
    [Listener] conl2t_extops: conl2l_extops = --sink afile --mfile output.pcm -C 2 -F s16be
  • To dump the output in EC3 format, modify this line in avbrun.cfg
    `conl2l_extops = --sink afile --mfile out.ec3 --sync-audio-file-type 2`: Dump to ec3 file
  • To play output.pcm ffplay -f s16be -ar 48k -ac 2 output.pcm.
  • Create a file with name streaminfo.conf and paste the contents mentioned below. In xl4 deb pakages from 7.0.7 version, there is new configuration file added to conl2 test app to check for stream information. Prepare streaminfo.conf with below content, replace eno1 with the name of your network device and replace all instances of stream-id:00-01-02-03-04-05:00-02 with your stream ID, This stream-id can be kept unchanged for the existing examples.
    /ieee802-dot1q-cnc-config/cnc-config/domain|domain-id:domain00|/cuc|cuc-id:br0|/stream|stream-id:00-01-02-03-04-05:00-02|/talker/end-station-interfaces|mac-address:00-01-02-03-04-05|interface-name:eno1|/accept 1
    /ieee802-dot1q-cnc-config/cnc-config/domain|domain-id:domain01|/cuc|cuc-id:br0|/stream|stream-id:00-01-02-03-04-05:00-02|/listener|index:0|/end-station-interfaces|mac-address:00-01-02-03-04-05|interface-name:eno1|/accept 1
    /ieee802-dot1q-cnc-config/cnc-config/domain|domain-id:domain00|/cuc|cuc-id:br0|/stream|stream-id:00-01-02-03-04-05:00-02|/talker/stream-rank/rank 1
    ../data-frame-specification|index:0|/ieee802-mac-addresses/destination-mac-address 91-E0-F0-00-FE-00
    source-mac-address 00-01-02-03-04-05
    ../ieee802-vlan-tag/priority-code-point 3
    vlan-id 110
    /ieee802-dot1q-cnc-config/cnc-config/domain|domain-id:domain00|/cuc|cuc-id:br0|/stream|stream-id:00-01-02-03-04-05:00-02|/talker/traffic-specification/
    max-frames-per-interval 1
    max-frame-size 1400
    interval/numerator 1
    denominator 8000
    /ieee802-dot1q-cnc-config/cnc-config/domain|domain-id:domain01|/cuc|cuc-id:br0|/stream|stream-id:00-01-02-03-04-05:00-02|/listener|index:0|/interface-configuration/interface-list|mac-address:00-01-02-03-04-05|interface-name:eno1|/config-list|index:0|/ieee802-mac-addresses/destination-mac-address 91-E0-F0-00-FE-00
    source-mac-address 00-01-02-03-04-05
    ../ieee802-vlan-tag/priority-code-point 3
    vlan-id 110
  • Create uniconf.conf file in the same folder and paste the following contents. Replace eno1 with the name of your network device.
    /ietf-interfaces/interfaces/interface|name:eno1|/enabled true
  • For Talker, Create conl2_talker.conf and paste the following contents.
    /xl4-extmod/xl4conl2/CONL2_INSTANCE|INSTANCE_INDEX:0|/
    CONF_NOSYNC false
    CONF_AVTPD_BUFFTIME_MSEC 1000
    CONF_SEND_AHEADTS_USEC 20000
    CONF_AUDIO_PAYLOAD_TYPE "aaf"
    CONF_ECHOBACK false
    CONF_DROPLATE false
    CONF_SINK_DEVICE_NAME ""
    CONF_SOURCE_AUDIO_CHANNELS 2
    CONF_SOURCE_AUDIO_RATE 48000
    CONF_SINK_FILE_NAME ""
    CONF_SOURCE_FILE_NAME ""
    CONF_SOURCE_WAVE_FREQ 500
    CONF_SOURCE_AUDIO_SAMPLES 180
    CONF_TSOFFSET_USEC 200000
    CONF_AUDIO_LITTLE false
    CONF_GPTP_SHMEM "/gptp_mc_shmeno1"
    CONF_SHMEM_SUFFIX "avmt"
    CONF_MEDIA_SOURCE "sinwave"
    CONF_SOURCE_AUDIO_FORMAT "s24be"
  • For Listener, Create conl2_listener.conf and paste the following contents.
    /xl4-extmod/xl4conl2/CONL2_INSTANCE|INSTANCE_INDEX:1|/
    CONF_NOSYNC false
    CONF_AVTPD_BUFFTIME_MSEC 1000
    CONF_SEND_AHEADTS_USEC 20000
    CONF_AUDIO_PAYLOAD_TYPE "aaf"
    CONF_ECHOBACK false
    CONF_DROPLATE false
    CONF_SINK_DEVICE_NAME ""
    CONF_SOURCE_AUDIO_CHANNELS 2
    CONF_SOURCE_AUDIO_RATE 48000
    CONF_SINK_FILE_NAME ""
    CONF_SOURCE_FILE_NAME ""
    CONF_SOURCE_WAVE_FREQ 500
    CONF_SOURCE_AUDIO_SAMPLES 180
    CONF_TSOFFSET_USEC 200000
    CONF_AUDIO_LITTLE false
    CONF_GPTP_SHMEM "/gptp_mc_shmeno1"
    CONF_SHMEM_SUFFIX "avml"
    CONF_SINK_AUDIO_FILE_TYPE "1"
    CONF_MEDIA_SINK "aplay"
    CONF_SOURCE_AUDIO_FORMAT "s24be"
  • To start the AVB Talker
    avbrun -r talker
  • To start the AVB Listener
    avbrun -r listener

Build the example

Refer Ethernet TSN gPTP Examples to build the avtp examples.

HW Setup

Refer Ethernet TSN gPTP Examples for HW Setup.

Create a network between EVM and host PC

EVM and PC has to be connected directly as shown below using CAT6 or CAT5 cable

Local network between PC and EVM

PORT1 instead of PORT0 on EVM can be used as well.

Run the example

Attention
If you need to reload and run again, a CPU power-cycle is MUST

Refer :Ethernet AVB Stack - API and Integration Guide for how to configure AVTP parameters.

AVTP verification

DUT as pcmaaf_talker

Flash binary in am263x-cc and start it.

On the PC side, configure avbrun as conl2 listener(pcm) and start avbrun -r listener.

The log on DUT side should be printed:

INF:avtp:audio talker sent: 200.000000(packets/sec), 1.536000(mbps)
INF:avtp:audio talker sent: 200.000595(packets/sec), 1.536005(mbps)
INF:avtp:audio talker sent: 199.999786(packets/sec), 1.535998(mbps)
INF:avtp:audio talker sent: 200.000000(packets/sec), 1.536000(mbps)

On PC side, after running for a while, stop avbrun and confirm output.pcm is created. Play the file with ffplay -f s16be -ar 48k -ac 2 output.pcm, the audio should be heard from speaker.

Verification DUT as pcmaaf_listener

Flash binary in aafpcm_listener and start it.

On the PC side, configure avbrun as conl2 talker(pcm) and start avbrun -r talker.

On the DUT side, correct pcm info including bitdepth, channels, format and data rate should be printed.

[RX 00:01:02:03:04:05:00:02] Rp#8 Mbps(1.536034, 1.536804) Delay(-23487, -11303894, -17810) Pkt(2413, 0, 0)
IFV:gptp:000369-441329:domainIndex=0, clock_master_sync_receive:the master clock rate to 97579ppb, GMdiff=-6nsec
IFV:gptp:000369-565787:domainIndex=0, clock_master_sync_receive:the master clock rate to 97429ppb, GMdiff=-72nsec
IFV:gptp:000369-690810:domainIndex=0, clock_master_sync_receive:the master clock rate to 97675ppb, GMdiff=46nsec
IFV:gptp:000369-817439:domainIndex=0, clock_master_sync_receive:the master clock rate to 97486ppb, GMdiff=-44nsec
IFV:gptp:000369-940807:domainIndex=0, clock_master_sync_receive:the master clock rate to 97839ppb, GMdiff=117nsec
IFV:gptp:000370-065716:domainIndex=0, clock_master_sync_receive:the master clock rate to 97623ppb, GMdiff=8nsec
IFV:gptp:000370-191183:domainIndex=0, clock_master_sync_receive:the master clock rate to 97642ppb, GMdiff=16nsec
IFV:gptp:000370-315754:domainIndex=0, clock_master_sync_receive:the master clock rate to 97846ppb, GMdiff=105nsec
[RX 00:01:02:03:04:05:00:02] Rp#9 Mbps(1.536211, 1.536745) Delay(-23490, -11303892, -17810) Pkt(2681, 0, 0)
IFV:gptp:000370-440775:domainIndex=0, clock_master_sync_receive:the master clock rate to 97900ppb, GMdiff=118nsec
370.471s : CPU load = 8.20 %
IFV:gptp:000370-566110:domainIndex=0, clock_master_sync_receive:the master clock rate to 97677ppb, GMdiff=6nsec
IFV:gptp:000370-690721:domainIndex=0, clock_master_sync_receive:the master clock rate to 97796ppb, GMdiff=59nsec
domain=0, offset=0nsec, hw-adjrate=97796ppb
gmsync=true, last_setts64=0nsec
IFV:gptp:000370-816837:domainIndex=0, clock_master_sync_receive:the master clock rate to 97877ppb, GMdiff=89nsec
IFV:gptp:000370-941093:domainIndex=0, clock_master_sync_receive:the master clock rate to 97951ppb, GMdiff=112nsec
IFV:gptp:000371-065656:domainIndex=0, clock_master_sync_receive:the master clock rate to 97736ppb, GMdiff=4nsec
IFV:gptp:000371-190631:domainIndex=0, clock_master_sync_receive:the master clock rate to 97719ppb, GMdiff=-4nsec
IFV:gptp:000371-316052:domainIndex=0, clock_master_sync_receive:the master clock rate to 97921ppb, GMdiff=87nsec
[RX 00:01:02:03:04:05:00:02] Rp#10 Mbps(1.536044, 1.536681) Delay(-23490, -11303894, -17810) Pkt(2949, 0, 0)
IFV:gptp:000371-440734:domainIndex=0, clock_master_sync_receive:the master clock rate to 97887ppb, GMdiff=62nsec
IFV:gptp:000371-566091:domainIndex=0, clock_master_sync_receive:the master clock rate to 97812ppb, GMdiff=22nsec
IFV:gptp:000371-691026:domainIndex=0, clock_master_sync_receive:the master clock rate to 97839ppb, GMdiff=32nsec
IFV:gptp:000371-816876:domainIndex=0, clock_master_sync_receive:the master clock rate to 97812ppb, GMdiff=16nsec
IFV:gptp:000371-940623:domainIndex=0, clock_master_sync_receive:the master clock rate to 97836ppb, GMdiff=25nsec
IFV:gptp:000372-066382:domainIndex=0, clock_master_sync_receive:the master clock rate to 97957ppb, GMdiff=76nsec
IFV:gptp:000372-190569:domainIndex=0, clock_master_sync_receive:the master clock rate to 98008ppb, GMdiff=91nsec
IFV:gptp:000372-315571:domainIndex=0, clock_master_sync_receive:the master clock rate to 98019ppb, GMdiff=86nsec
[RX 00:01:02:03:04:05:00:02] Rp#11 Mbps(1.536200, 1.536641) Delay(-23490, -11303881, -17810) Pkt(3217, 0, 0)

See Also

Ethernet And Networking | Ethernet AVB Stack - API and Integration Guide