Introduction
This example demonstrates the usage of the SDL R5 CCM module. The example shows how to setup and use the R5 CCM Safety Diagnostic operation.
Use Cases
| Use Case | Description |
| UC-1 | self test on R5 CCM. |
| UC-2 | self test with error force on R5 CCM. |
Supported Combinations
| Parameter | Value |
| CPU + OS | r5fss0-0 nortos |
| Toolchain | ti-arm-clang |
| Board | am263x-cc |
| Example folder | examples/sdl/ccm/sdl_ccm_example/ |
Steps to Run the Example
Steps to Test the Example
- CCM example should only be tested in QSPI boot mode and should not be tested in no boot mode with debugger connected.
- Follow the below procedure to test the CCM and CCM_VIM example.
- A quick recap of steps done so far that are needed for the flashing to work
- Make sure the UART port used for terminal is identified as mentioned in Setup UART Terminal
- Make sure python3 is installed as mentioned in Python3
- Make sure you have the EVM power cable and UART cable connected as shown in Cable Connections
- Build the hello world application as mentioned in Build a Hello World example, Build a Hello World example
- As part of the build process in the final step a file with extension .appimage is generated. This is the file we need to flash.
- When building with makefiles and single-core projects, this file can be found here
${SDK_INSTALL_PATH}/examples/sdl/ccm/sdl_ccm_example/{board}/r5fss0-0_nortos/ti-arm-clang/sdl_ccm_example.release.appimage
- A default configuration file can be found at below path. You can edit this file directly or take a copy and edit this file.
${SDK_INSTALL_PATH}/tools/boot/sbl_prebuilt/{board}/default_sbl_qspi.cfg
- Edit below line in the config file to point to your application .appimage file. Give the absolute path to the .appimage file or path relative to ${SDK_INSTALL_PATH}/tools/boot. Make sure to use forward slash / in the filename path.
--file=../../examples/sdl/ccm/sdl_ccm_example/{board}/r5fss0-0_nortos/ti-arm-clang/sdl_ccm_example.release.appimage --operation=flash --flash-offset=0x80000
- NOTE : edit sdl_ccm_example to sdl_ccm_vim for ccm vim example testing.
- Save and close the config file.
- Flash the application by follow the steps mentioned in the page, Flash a Hello World example
See Also
CCM
Sample Output
Shown below is a sample output when the CCM application is run.
R5 CPU Application
CCM Example Test Started: R5F0
MCU ESM Initialization completed
CCM Test Init completed
CCM Verify Init completed
CCM Functional Test
CCM self test: starting
CCM Self Test completed
CCM self test with error forcing: starting
CCM Self Test with error forcing completed
CCM inject error: test starting
CCM inject Test completed
CPU Functionality
Passed.
All tests have passed.
R5 CPU Application
CCM Example Test Started: R5F0
MCU ESM Initialization completed
CCM Test Init completed
CCM Verify Init completed
CCM Functional Test
CCM self test: starting
CCM Self Test completed
CCM self test with error forcing: starting
CCM Self Test with error forcing completed
CCM inject error: test starting
CCM inject Test completed
CCM Example Test Started: R5F1
MCU ESM Initialization completed
CCM Test Init completed
CCM Verify Init completed
CCM Functional Test
CCM self test: starting
CCM Self Test completed
CCM self test with error forcing: starting
CCM Self Test with error forcing completed
CCM inject error: test starting
CCM inject Test completed
CPU Functionality
Passed.
All tests have passed.
Shown below is a sample output when the TMU application is run.