AM263x MCU+ SDK  09.01.00
I2C Read

Introduction

This example demonstrates reading data from I2C based EEPROM devices present in the board. Application reads 20 samples from the EEPROM and exits.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
Toolchain ti-arm-clang
Boards am263x-cc, am263x-lp
Example folder examples/drivers/i2c/i2c_read

Steps to Run the Example

See Also

I2C

Sample Output

Shown below is a sample output when the application is run,

[I2C] Read data ... !!!
[I2C] Sample 0: 255
[I2C] Sample 1: 255
[I2C] Sample 2: 255
[I2C] Sample 3: 255
[I2C] Sample 4: 255
[I2C] Sample 5: 255
[I2C] Sample 6: 255
[I2C] Sample 7: 255
[I2C] Sample 8: 255
[I2C] Sample 9: 255
[I2C] Sample 10: 255
[I2C] Sample 11: 255
[I2C] Sample 12: 255
[I2C] Sample 13: 255
[I2C] Sample 14: 255
[I2C] Sample 15: 255
[I2C] Sample 16: 255
[I2C] Sample 17: 255
[I2C] Sample 18: 255
[I2C] Sample 19: 255
[I2C] Read data ... DONE !!!All tests have passed!!