Introduction
This example demonstrates the data transfer using EDMA in interrupt mode
Supported Combinations
Parameter | Value |
CPU + OS | r5fss0-0 freertos |
r5fss0-1 nortos |
r5fss1-0 nortos |
r5fss1-1 nortos |
Toolchain | ti-arm-clang |
Boards | am263x-cc, am263x-lp |
Example folder | examples/drivers/edma/edma_interrupt_transfer/ |
Steps to Run the Example
- When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
- When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles) || SOC_AM263PX
- Launch a CCS debug session, follow the steps for running multi core applications in Prerequisites and run the executables, see CCS Launch, Load and Run
- This is a multi-core example. Hence the executables should be loaded and run for all the above mentioned cores
Sample Output
Shown below is a sample output when the application is run,
[EDMA] Interrupt Transfer Test Started...
[EDMA] Interrupt Transfer Test Completed!!
All tests have passed!!