AM263x MCU+ SDK  09.00.00
SDL PBIST

Introduction

This example demonstrates the usage of the PBIST module. The example shows how to setup and use the PBIST controller. The example configures the algorithm and memory group. Example also prints the time taken for test execution.

Use Cases

Use Case Description
UC-1 Configure wrong combination of algorithm and memory group.
UC-2 Configure correct combination of algorithm and memory group.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
Toolchain ti-arm-clang
Board am263x-cc
Example folder examples/sdl/pbist/pbist_mcu/

Steps to Run the Example

See Also

PBIST

Sample Output

Shown below is a sample output when the application is run,

[Cortex_R5_0]
PBIST Application
Starting PBIST failure insertion test on TOP PBIST
PBIST failure Insertion test complete for TOP BIST
PBIST Failure Insertion Test completed in 47 micro secs
Starting PBIST test on TOP PBIST
PBIST complete for R5 STC
PBIST complete for R51 STC
PBIST complete for PBISTROM
PBIST complete for CPSW
PBIST complete for ICSSM
PBIST complete for MBOX
PBIST complete for MCAN
PBIST complete for TPCC
PBIST complete for MSS_L2_1
PBIST complete for MSS_L2_2
PBIST complete for MSS_L2_3
PBIST complete for VIM1 R5SS0
PBIST complete for VIM0 R5SS1
PBIST complete for VIM1 R5SS1
PBIST complete for R5SS1 RAM
PBIST complete for MSS CR5B ATCM0
PBIST complete for MSS CR5B ATCM1
PBIST complete for MSS CR5B BTCM0
PBIST complete for MSS CR5B BTCM1
All tests have passed.
[Cortex_R5_2]
PBIST Application
Starting PBIST failure insertion test on TOP PBIST
PBIST failure Insertion test complete for TOP BIST
PBIST Failure Insertion Test completed in 0 micro secs
Starting PBIST test on TOP PBIST
PBIST complete for VIM0 R5SS0
PBIST complete for MSS_L2_0
PBIST complete for R5SS0 RAM
PBIST complete for CR5A ROM0
PBIST complete for TRACE
PBIST complete for MMCH0
PBIST complete for MSS CR5A ATCM0
PBIST complete for MSS CR5A ATCM1
PBIST complete for MSS CR5A BTCM0
PBIST complete for MSS CR5A BTCM1
All tests have passed.