Introduction
This examples demonstrates the prioritization of interrupts in VIM through nesting of 3 Timer interrupts of different priority.
The example does the below
- Sets up Timer's 0,1,2 with same tick period.
- Sets up Timer interrupt with Timer 0 being highest priority, TImer 2 lowest.
- Nesting of interrupts is visualised with the help of trace buffer which captures the start and end of each Timer ISR.
- Timer2 is started first followed by Timer1 and then Timer0.
- Timer2 Interrupts gets nested by Timer1 interrupt which in turn gets nested by Timer0 interrupt.
- The trace macros used are -
- 0xA0 - Timer0 ISR start
- 0xB0 - Timer0 ISR end
- 0xA1 - Timer1 ISR start
- 0xB1 - Timer1 ISR end
- 0xA2 - Timer2 ISR start
- 0xB2 - Timer2 ISR end
- Note
- This example uses SysCfg to configure priority of Timer interrupts. For configuring the priority of interrupts which are not supported by SysCfg, use the element "HwiP_Params.priority" in HwiP. Priority can be specified from a level of 0 to 15, where 0 denotes highest priority.
Supported Combinations
Parameter | Value |
CPU + OS | r5fss0-0 freertos |
r5fss0-0 nortos |
Toolchain | ti-arm-clang |
Board | am263x-cc, am263x-lp |
Example folder | examples/kernel/dpl/interrupt_prioritization/ |
Steps to Run the Example
- When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
- When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
- Launch a CCS debug session and run the executable, see CCS Launch, Load and Run
- The trace gets printed and can be used to verify interrupt nesting and prioritization.
See Also
Driver Porting Layer (DPL)
Sample Output
Shown below is a sample output when the application is run,
[DPL] Interrupt prioritization Test Started...
[DPL] All timers stopped
[DPL] Printing Trace -
A2 - A1 - A0 - B0 - B1 - B2 - A2 - A1 - A0 - B0 - B1 - B2 - A2 - A1 - A0 - B0 - B1 - B2 - A2 - A1 - A0 - B0 - B1 - B2 -
[DPL] Interrupt prioritization Test Passed!
All tests have passed!!