Introduction
This example configures a GPIO pin connected to an LED on the EVM in output mode. The application toggles the LED ON/OFF for 10 seconds using RTI Timer and exits.
Supported Combinations
Parameter | Value |
CPU + OS | r5fss0-0 freertos |
r5fss0-0 nortos |
Toolchain | ti-arm-clang |
Boards | am263x-cc, am263x-lp |
Example folder | examples/drivers/rti/rti_led_blink |
Steps to Run the Example
AM263X-CC
- Watch out for LED LD13 on the CC to blink which is controlled by GPIO0_1.
AM263X-LP
- Watch out for LED DS2 on the LP to blink which is controlled by GPIO0_26.
Sample Output
Shown below is a sample output when the application is run,
[RTI LED Blink Test] Starting ...
[RTI LED Blink Test] Timer Started...
[RTI LED Blink Test] Timer Stopped...
[RTI LED Blink Test] Blinking the LED...
All tests have passed!!