Introduction
This example demonstrates setting of multiple LED at the same time connected to the same I2C controller. The application will blink all the I2C controlled LED in the EVM.
Application exits after 10 iterations..
Supported Combinations
Parameter | Value |
CPU + OS | r5fss0-0 freertos |
r5fss0-0 nortos |
Toolchain | ti-arm-clang |
Boards | am263x-cc, am263x-lp |
Example folder | examples/drivers/i2c/i2c_led_blink |
AM263X-CC
- Watch out for LEDs LD2, LD3, LD4, LD5, LD6, LD7, LD8, LD9, LD10, LD11 on the CC to blink which is controlled by I2C2.
AM263X-LP
- Watch out for LED D7, D8, D9, D10, D11, D12, D13, D14 on the LP to blink which is controlled by I2C1.
Steps to Run the Example
See Also
I2C
Sample Output
Shown below is a sample output when the application is run,
I2C LED Blink Test Started ...
LED will Blink for 10 loop ...
I2C LED Blink Test Passed!!
All tests have passed!!