![Logo](ti_logo.svg) |
AM263x MCU+ SDK
08.05.00
|
|
Go to the documentation of this file.
43 #include <drivers/hw_include/soc_config.h>
44 #include <board/flash/flash_config.h>
46 #define FLASH_INVALID_VALUE (0xFFFFFFFFU)
79 typedef struct Flash_DevConfig_s {
152 uint8_t *buf, uint32_t len) ;
168 uint8_t *buf, uint32_t len) ;
236 typedef struct Flash_Params_s {
246 typedef struct Flash_Fxns_s
261 typedef struct Flash_Attrs_s {
281 typedef struct Flash_Config_s
291 #if defined (DRV_VERSION_FLASH_V0)
292 #include <board/flash/ospi/flash_nor_ospi.h>
295 #if defined (DRV_VERSION_FLASH_V1)
296 #include <board/flash/qspi/flash_nor_qspi.h>
uint32_t flashType
Definition: flash.h:263
void Flash_close(Flash_Handle handle)
Close flash driver.
Flash_Attrs * attrs
Definition: flash.h:283
uint32_t flashSize
Definition: flash.h:268
Flash_OpenFxn openFxn
Definition: flash.h:248
FlashCfg_EraseConfig eraseCfg
Definition: flash.h:101
uint32_t blockCount
Definition: flash.h:269
FlashCfg_ProtoEnConfig protocolCfg
Definition: flash.h:103
uint8_t cmdExtType
Definition: flash.h:81
void(* Flash_CloseFxn)(Flash_Config *config)
Driver implementation to close a specific flash driver.
Definition: flash.h:136
uint8_t cmdWren
Definition: flash.h:87
Flash_DevConfig * devConfig
Definition: flash.h:285
uint32_t driverInstance
Definition: flash.h:267
Flash driver configuration, these are filled by SysCfg based on the flash device that is selected.
Definition: flash.h:282
int32_t Flash_offsetToBlkPage(Flash_Handle handle, uint32_t offset, uint32_t *block, uint32_t *page)
Utility API to convert offset in bytes to (Block Num, Page Num)
int32_t Flash_SectorPageToOffset(Flash_Handle handle, uint32_t *offset, uint32_t sector, uint32_t page)
Utility API to convert (Sector Num, Page Num) to offset in bytes.
uint8_t deviceBusyType
Definition: flash.h:93
uint8_t cmdRdsr
Definition: flash.h:88
uint32_t xspiWipReg
Definition: flash.h:96
Flash_EraseSectorFxn eraseSectorFxn
Definition: flash.h:253
uint32_t flashBusyTimeout
Definition: flash.h:99
uint32_t sectorSize
Definition: flash.h:274
Flash_Fxns * fxns
Definition: flash.h:284
uint32_t pageSize
Definition: flash.h:272
uint8_t addrByteSupport
Definition: flash.h:84
int32_t(* Flash_ReadFxn)(Flash_Config *config, uint32_t offset, uint8_t *buf, uint32_t len)
Driver implementation to read from flash using a specific flash driver.
Definition: flash.h:151
int32_t Flash_blkPageToOffset(Flash_Handle handle, uint32_t *offset, uint32_t block, uint32_t page)
Utility API to convert (Block Num, Page Num) to offset in bytes.
Flash device attributes, these are filled by SysCfg based on the flash device that is selected.
Definition: flash.h:261
char * flashName
Definition: flash.h:264
uint32_t xspiWipBit
Definition: flash.h:97
Flash_EraseFxn eraseFxn
Definition: flash.h:252
Flash_Handle Flash_getHandle(uint32_t instanceId)
Get handle to flash driver.
Driver implementation callbacks.
Definition: flash.h:247
int32_t(* Flash_EraseFxn)(Flash_Config *config, uint32_t blockNum)
Driver implementation to erase a block using a specific flash driver.
Definition: flash.h:181
uint32_t Flash_getPhyTuningOffset(Flash_Handle handle)
Return flash offset to write PHY tuning data.
uint8_t fourByteAddrEnSeq
Definition: flash.h:86
uint8_t srWip
Definition: flash.h:89
uint8_t srWel
Definition: flash.h:91
struct Flash_Config_s Flash_Config
Forward declaration of Flash_Config.
Definition: flash.h:67
uint8_t resetType
Definition: flash.h:92
int32_t(* Flash_WriteFxn)(Flash_Config *config, uint32_t offset, uint8_t *buf, uint32_t len)
Driver implementation to write to flash using specific flash driver.
Definition: flash.h:167
Flash_CloseFxn closeFxn
Definition: flash.h:249
uint32_t flashWriteTimeout
Definition: flash.h:98
void Flash_Params_init(Flash_Params *params)
Set default parameters in the Flash_Params structure.
int32_t(* Flash_ResetFxn)(Flash_Config *config)
Driver implementation to soft reset the flash.
Definition: flash.h:207
uint32_t pageCount
Definition: flash.h:271
struct Flash_Params_s Flash_Params
Forward declaration of Flash_Params.
Definition: flash.h:72
int32_t(* Flash_custProtocolFxn)(Flash_Config *config)
User implementation of a custom function to configure flash to operate in a specific protocol.
Definition: flash.h:228
Flash_Attrs * Flash_getAttrs(uint32_t instanceId)
Return flash attributes.
uint8_t xspiWipRdCmd
Definition: flash.h:94
uint32_t blockSize
Definition: flash.h:270
FlashCfg_ReadIDConfig idCfg
Definition: flash.h:102
int32_t Flash_offsetToSectorPage(Flash_Handle handle, uint32_t offset, uint32_t *sector, uint32_t *page)
Utility API to convert offset in bytes to (Sector Num, Page Num)
int32_t Flash_eraseSector(Flash_Handle handle, uint32_t sectorNum)
Erase a sector from flash.
uint32_t deviceId
Definition: flash.h:265
Flash_ReadFxn readFxn
Definition: flash.h:250
uint8_t enable4BAddr
Definition: flash.h:83
int32_t Flash_reset(Flash_Handle handle)
Do a soft reset of the flash.
int32_t(* Flash_EraseSectorFxn)(Flash_Config *config, uint32_t sectorNum)
Driver implementation to erase a sector using a specific flash driver.
Definition: flash.h:194
Flash_WriteFxn writeFxn
Definition: flash.h:251
int32_t(* Flash_OpenFxn)(Flash_Config *config, Flash_Params *params)
Driver implementation to open a specific flash driver.
Definition: flash.h:124
Flash_Handle Flash_open(uint32_t instanceId, Flash_Params *params)
Open flash driver.
uint8_t byteOrder
Definition: flash.h:82
uint32_t manufacturerId
Definition: flash.h:266
Flash_ResetFxn resetFxn
Definition: flash.h:254
int32_t Flash_eraseBlk(Flash_Handle handle, uint32_t blockNum)
Erase a block from flash.
int32_t Flash_write(Flash_Handle handle, uint32_t offset, uint8_t *buf, uint32_t len)
Write to flash.
int32_t(* Flash_quirksFxn)(Flash_Config *config)
User implementation of a custom function to handle vendor specific quirks.
Definition: flash.h:219
uint32_t sectorCount
Definition: flash.h:273
Parameters passed during Flash_open()
Definition: flash.h:236
void * Flash_Handle
Handle to the FLash driver returned by Flash_opem()
Definition: flash.h:62
Flash_quirksFxn quirksFxn
Definition: flash.h:238
Flash_custProtocolFxn custProtoFxn
Definition: flash.h:239
Flash device config. This will be part of the flash config, so has to be filled by sysconfig or other...
Definition: flash.h:79
int32_t Flash_read(Flash_Handle handle, uint32_t offset, uint8_t *buf, uint32_t len)
Read data from flash.
void * object
Definition: flash.h:286