Introduction
This example demonstrates the usage of the SDL R5 CCM module. The example shows how to setup and use the R5 CCM Safety Diagnostic operation.
Use Cases
Use Case | Description |
UC-1 | self test on R5 CCM. |
UC-2 | self test with error force on R5 CCM. |
Supported Combinations
Parameter | Value |
CPU + OS | r5fss0-0 nortos |
Toolchain | ti-arm-clang |
Board | am263x-cc |
Example folder | examples/sdl/ccm/sdl_ccm_example/ |
Steps to Run the Example
See Also
CCM
Sample Output
Shown below is a sample output when the application is run,
R5F0 CORE:
R5 CPU Application
R5F-CPU example application CCM_Test_init: Init MCU ESM complete
CCM_Test_init: CCM Init complete
R5F-CPU example application CCM_Test_init: CCM Init complete
CCM Functional Test
R5F-CPU example application CCM self test: starting
R5F-CPU example application CCM Self Test complete
R5F-CPU example application CCM self test with error forcing: starting
R5F-CPU example application CCM Self Test with error forcing complete
R5F-CPU example application CCM inject error: test starting
R5F-CPU example application CCM inject Test complete
CPU Functionality Passed.
All tests have passed.
R5F1 CORE:
R5 CPU Application
R5F-CPU example application CCM_Test_init: Init MCU ESM complete
CCM_Test_init: CCM Init complete
R5F-CPU example application CCM_Test_init: CCM Init complete
CCM Functional Test
R5F-CPU example application CCM self test: starting
R5F-CPU example application CCM Self Test complete
R5F-CPU example application CCM self test with error forcing: starting
R5F-CPU example application CCM Self Test with error forcing complete
R5F-CPU example application CCM inject error: test starting
R5F-CPU example application CCM inject Test complete
CPU Functionality Passed.
All tests have passed.