AM263x MCU+ SDK  08.05.00
EPWM Hr Updown

Introduction

EPWM HR UpDown

This example modifies the MEP control registers to show edge displacement for high-resolution period with ePWM in Up-Down count mode due to the HRPWM control extension of the respective ePWM module.

Block Diagram for EPWM HR UpDown example

External Connections

  • Pin can be connected to high resolution oscilloscope (1 GHz) to observe the edge displacement.

AM263X-CC

When using AM263x-CC with TMDSHSECDOCK (HSEC180 controlCARD Baseboard Docking Station)

  • Capture waveform on HSEC Pin 49, 51 for epwm0
  • Capture waveform on HSEC Pin 53, 55 for epwm1
  • Capture waveform on HSEC Pin 50, 52 for epwm2
  • Capture waveform on HSEC Pin 54, 56 for epwm3
  • Capture waveform on HSEC Pin 57, 59 for epwm4

AM263X-LP

This example is not supported on AM263X-LP

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
Toolchain ti-arm-clang
Board am263x-cc
Example folder examples/drivers/epwm/epwm_hr_updown

Steps to Run the Example

  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
  • Establish connections as mentioned in External Connections section
  • Launch a CCS debug session and run the executable, see CCS Launch, Load and Run

See Also

EPWM

Sample Output

Shown below is a sample output when the application is run,

EPWM High Resolution Up Down Test Started ...
EPWM High Resolution Up Down Test Passed!!
All tests have passed!!

EPWM HR UpDown waveform