AM263x MCU+ SDK  08.05.00
EDMA Polled Transfer

Introduction

This example demonstrates the data transfer using EDMA in polled mode

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
r5fss0-0 freertos
Toolchain ti-arm-clang
Boards am263x-cc, am263x-lp
Example folder examples/drivers/edma/edma_polled_transfer/

Steps to Run the Example

Sample Output

Shown below is a sample output when the application is run,

[EDMA] Polled Transfer Test Started...
[EDMA] Polled Transfer Test Completed!!
All tests have passed!!