Introduction
- Post Processing Blocks of the ADC are featured with limit checking on the PPBResult registers. the following are limits that each PPB can check,
- High Limit
- Low Limit
- Zero Crossing.
- PPB can generate Event flags, for selected events. Also, each PPB can generate an EVTINT based on which event has occured. ADCxEVTINT is a logical OR of all such PPBxEVTINT in given ADC.
Example Block diagram
Example Description
This example is a demonstration of such feature and uses the loopback from DAC to generate the required analog wave form (ramp wave is choosen for this example). Once the High and Low values are touched, the PPBs generate the EVTINT and ISR will check the events of PPB0, PPB1 (both configured for SOC0) and determine which limit has occured.
SOC configuration
- SOC0 is configured to sample on AIN0
- Sample window of 20 is selected (arbitrary)
- Software only trigger is selected.
PPB Configurations
- SOC0 is selected for PPB0 and PPB1
- PPB1 is set for Higher Limit Checking i.e., PPB Event is set for TripHigh
- PPB1EVTINT is set for TripHigh
- PPB2 is set for Lower Limit Checking i.e., PPB Event is set for TripLow
- PPB2EVTINT is set for TripLow Note : PPBEVTINT is a logical OR for all the PPBxEVTINT, and is source for ISR
ISR Configuration
- App_adc_PPB_ISR is set for INTXbar0, selected for ADC1EVTINT
- ISR checks which event has occured and load the corresponding PPB result to respective arrays.
- ISR Clears the events for further generated event identification
External Connections
Am263x-CC
Loop DAC output back to ADC1 Channel 0
- Connect HSEC Pin 9 to HSEC Pin 18
Am263x-LP
Loop DAC output back to ADC1 Channel 0
- Connect J1/J3 Pin 30 to J1/J3 Pin 24
Watch Variables
- gAdcHighLimitOutputs[] - holds the High limit trip values
- gAdcLowLimitOutputs[] - holds the Low limit trip values
Supported Combinations
Parameter | Value |
CPU + OS | r5fss0-0 nortos |
Toolchain | ti-arm-clang |
Board | am263x-cc, am263x-lp |
Example folder | examples/drivers/adc/adc_ppb_limits/ |
Steps to Run the Example
- When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
- When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
- Establish connections as mentioned in External Connections section
- Launch a CCS debug session and run the executable, see CCS Launch, Load and Run
- Using the watch variables, view the ADC conversion results.
- Observe 6 EPWM waveforms. After ADC input voltage exceeds the PPB limit, PWMs get tripped.
See Also
ADC
Sample Output
Shown below is a sample output when the application is run,
ADC PPB Limits Test Started
ADC trip high events occurred for Conversion Values :
3046
3207
3208
3204
3207
ADC trip low events occurred for Conversion Values :
90
195
301
402
503
608
713
816
920
90
195
299
402
503
607
714
817
919
90
194
297
ADC PPB Limits Test Passed
All tests have passed!!