This section is aimed at explaining what a bootloader is, why is it needed and details regarding the bootloader and bootflow used in the MCU+SDK.
Generally speaking, bootloader is a piece of software / firmware that runs as soon as you power on an SoC. A bootloader's main duty is to start the subsequent pieces of software, such an OS, a baremetal application or in some cases another bootloader. When it comes to embedded, the bootloader is usually closely tied with the underlying SoC architecture. The bootloader is usually stored in a protected, non-volatile on-chip memory. Typically the bootloader performs various hardware checks, initializes the processor and configures the SoC registers etc. Since the primary aim of the bootloader is to load the next piece of software, it needs to communicate to the external world to receive this firmware/application image. This can be over a number of protocols - USB, UART, SPI, I2C, External Flash, Internal Flash, SD Card, Ethernet, CAN etc. Bootloader is also a key component in embedded security. Hardware Root-of-Trust is usually passed onto the bootloader and is passed on down the line.
As mentioned earlier, sometimes the bootloader would be loading another bootloader which can load another one and so on. This is usually the case in advanced SoCs, and there are various reasons for this. The first bootloader is usually kept on secure, read-only memory for security reasons and to have a known state always before application software starts. It makes sense then to keep this bootloader simple and let it do only the bare minimum configuration required. This secondary bootloader can be complex and configurable to suit the needs of the application. This can also be updated easily compared to the first stage bootloader. In fact for the devices in MCU+SDK, we have a two-stage bootloading - the first stage bootloader is called ROM Bootloader (RBL) and the second stage bootloader is called Secondary Bootloader (SBL).
Multi-core bootloading is almost always a follow up when there is a multi-stage bootloading. In this case the first bootloader technically might not be even aware of the other cores, it will just boot the next stage bootloader and this second stage bootloader will take care of the complex bootloading on the different cores.
Loading a multi-core application is slightly more complicated than loading a single core application. There would be concerns regarding image preparation, shared memory access, and so on. Mostly there would be a particular format in which the individual core images are created, and then they may/may not be concatenated into a single image for SBL to load. Whatever format the application image is in, the SBL should be aware of it so that it can parse and load the image correctly.
In the MCU+SDK, the bootflow takes place mainly in two steps after you power ON the device
The RBL or ROM Bootloader is stored in read-only memory and is almost considered as part of the SoC. The details regarding the RBL and ROM Boot is out of scope for this user guide. Please refer to the Technical Reference Manual of the device for more details. But basically the ROM expects an x509 signed binary image of the secondary bootloader to be provided for boot.
The x509 template for ROM looks something like this:
The SBL is like any other application, created using the same compiler and linker toolchain. However the steps to convert the application .out
into a bootable image are different for SBL as listed below
wfi
loop. This is done by specifying a different entry point -e_vectors_sbl
in the linker command file for the SBL application. In _vectors_sbl
the very first thing it does is detect the core and continue execution for Core0, while if the core is Core1 then it enters wfi
loop.0x70002000
and this is the entry point for the SBL.0x70002000
to 0x70040000
should be used by SBL code, data, stack etc.out
file is first converted to a binary format .bin
using the TI ARM CLANG objcopy
tool.objcopy
fills the gaps with 0x00
..bin
file is then signed using the Signing Scripts to create the final .tiimage
bootable image..tiimage
file can then be flashed or copied to a boot image using the Flashing Tools
SBL BOOT
makefile_ccs_bootimage_gen
that is included in every example and secondary bootloader (SBL) CCS project.makefile
in the example folder.Shown below are the different steps that are done to convert the compiler+linker generated application .out
into a format suitable for flashing and booting
out2rpc
is used to convert the ELF .out to a binary file containing only the loadable sections. This is called a RPRC file.multiCoreGen
is then used to combine all the RPRC files per CPU into a single .appimage
file which is a concatenation of the individual CPU specific RPRC files..appimage
is then flash to the EVM
.appimage
) is created one needs to copy or flash these to a supported boot media so that the application can start executing once the SOC is powered ONAfter a SBL and application image is flashed, shown below is the high level boot flow, after the SOC is powered on.
The SBL is like any other example of the SDK. They use the bootloader library APIs to carry out the bootloading process. Depending on the boot media from which we load the application binary, we have multiple SBLs like sbl_ospi
,sbl_uart
etc. A bare minimum SBL called the sbl_null
is also included which aids the users to load their applications via CCS. Here are some details regarding those.
sbl_null
is a secondary bootloader which doesn't load any application binary, but just does the SOC initialization and puts all the cores in WFI (Wait For Interrupt) mode.sbl_qspi
is a secondary bootloader which reads and parses the application image from a location in the QSPI flash and then moves on to core initialization and other stepssbl_qspi
, the application image needs to be flashed at a particular location in the QSPI flash memory.sbl_qspi
application. Currently this is 0x80000. In most cases you wouldn't need to change this.sbl_uart
is a secondary bootloader which receives the multicore appimage via UART, stores it in memory and then does the parsing, core initialization etc.sbl_uart
, you can refer to UART Bootloader Python Script subsection. Detailed steps on the usage is mentioned in the same subsection.See also these additional pages for more details and examples about the boot flow,