- Note
- MPU FIREWALL driver cannot be used without encrypted HSMRt binary on HS-FS devices (will be available in 8.4) and TIFS-MCU on HS-SE devices (available on mySecureSW).
MPU FIREWALL driver provides API to configure different regions in all supported firewalls.
Features Supported
- APIs to setup MPU Firewall regions, including region start address, size, attributes like access permissions and AID configurations
SysConfig Features
- Note
- It is strongly recommend to use SysConfig where it is available instead of using direct SW API calls. This will help simplify the SW application and also catch common mistakes early in the development cycle.
- MPU Firewall selection
- Region configuration for each firewall
- Start address and Size configuration
- Privilege ID and access permission configuration
Features NOT Supported
Important Usage Guidelines
Example Usage
Include the below file to access the APIs
Example to setup MPU Firewall regions is shown below,
API
APIs for MPU Firewall