Booting user defined applications on a SOC involves multiples steps as listed below,
Firstly, there are multiple steps involved to convert a user application, created using a compiler+linker toolchain, into a binary format that is suitable to be booted by the SOC
Next, we need to flash this binary to the EVM flash
Finally, when the SOC is powered on, the previously flashed binary is executed.
After powering on the EVM, the bootflow takes place mainly in two steps
ROM boot, in which the ROM bootloader boots a secondary bootloader or an SBL
SBL boot in which the secondary bootloader boots the application
Note, that a system application itself can consist of multiple CPU specific application binaries that all collaborate together to realize the overall system goal.
This section details these steps and gives an overview of the bootloaders to understand the process better.
Additional References
See also these additional pages for more details and examples about the boot flow,
To understand different secondary bootloader (SBL) examples see,
To understand the boot image creation tools, see Booting Tools
Preparing the application for boot
Note
To see the exact sequence of steps in which applications and secondary bootloader (SBL) are converted from compiler generated .out files to boot images, see the makefile makefile_ccs_bootimage_gen that is included in every example and secondary bootloader (SBL) CCS project.
If you are using makefile based build, then see the file named makefile in the example folder.
Shown below are the different steps that are done to convert the compiler+linker generated application .out into a format suitable for flashing and booting
For each CPU, the compiler+linker toolchain is used to create the application .out "ELF" file which can be loaded and run via CCS
The below "post build" steps are then used to convert the application .out into a "flash" friendly format
For each CPU, out2rpc is used to convert the ELF .out to a binary file containing only the loadable sections. This is called a RPRC file.
For each CPU, xipGen is used to split this RPRC file into two RPRC files.
One RPRC, containing the section that during boot need to be loaded to RAM
Second RPRC, containing the section that during boot are not loaded to RAM but are instead "eXecuted In Place", i.e XIP
multiCoreGen is then used to combine all the non-XIP RPRC files per CPU into a single .appimage file which is a concatenation of the individual CPU specific RPRC files.
multiCoreGen is used again to combine all the XIP RPRC files per CPU into a single .appimage_xip file which is a concatenation of the individual CPU specific RPRC XIP files.
This .appimage and .appimage_xip is then flash to the EVM
Post build steps
Flashing the application for boot
Once the application images (.appimage and .appimage_xip) are created one needs to copy or flash these to a supported boot media so that the application can start executing once the SOC is powered ON
When flashing the application we also need to flash a bootloader or SBL image.
See Flashing Tools for detailed steps that are done to flash a user application
Booting the application
After a SBL and application image is flashed, shown below is the high level boot flow, after the SOC is powered on.
HIGH LEVEL BOOTFLOW
ROM Boot
As soon as the EVM is powered ON, the ROM bootloader or RBL starts running. The RBL is the primary bootloader.
Depending on which boot mode is selected on the EVM, the RBL will load the secondary bootloader or SBL from a boot media (OSPI flash, SD card or via UART).
Rest of the booting is done by the SBL.
The RBL expects the image it boots (SBL in our case) to always be signed. Refer Booting Tools for more information on signing scripts.
SBL Boot
The SBL is essentially an example application of the bootloader library.
We call it a secondary bootloader because it is booted by the RBL, which is the primary bootloader.
An SBL typically does a bunch of SOC specific initializations and proceeds to the application loading.
Depending on the type of SBL loaded, SBL looks for the multicore appimage (refer Booting Tools for more on multicore appimage) of the application binary at a specified location in a boot media.
If the appimage is found, the multicore appimage is parsed into multiple RPRCs. These are optimized binaries which are then loaded into individual CPUs.
Each RPRC image will have information regarding the core on which it is to be loaded, entry points and multiple sections of that application binary
The SBL uses this information to initialize each core which has a valid RPRC. It then loads the RPRC according to the sections specified, sets the entry points and releases the core from reset. Now the core will start running
SBL BOOT
Secondary Bootloaders
Depending on the boot media from which we load the application binary, we have multiple SBLs like sbl_ospi,sbl_uart etc. A bare minimum SBL called the sbl_null is also included which aids the users to load their applications via CCS.
SBL NULL
The sbl_null is a secondary bootloader which doesn't load any application binary, but just does the SOC initialization and puts all the cores in WFI (Wait For Interrupt) mode.
The sbl_qspi is a secondary bootloader which reads and parses the application image from a location in the QSPI flash and then moves on to core initialization and other steps
To boot an application using the sbl_qspi, the application image needs to be flashed at a particular location in the QSPI flash memory.
This location or offset is specified in the SysConfig of the sbl_qspi application. Currently this is 0x80000. In most cases you wouldn't need to change this.
To flash an application (or any file in fact) to a location in the QSPI flash memory, follow the steps mentioned in Basic steps to flash files
SBL UART
The sbl_uart is a secondary bootloader which receives the multicore appimage via UART, stores it in memory and then does the parsing, core initialization etc.
To boot an application using the sbl_uart, you can refer to UART Bootloader Python Script subsection. Detailed steps on the usage is mentioned in the same subsection.
Preparing the SBL for boot
The SBL is like any other application, created using the same compiler and linker toolchain. However the steps to convert the application .out into a bootable image are different for SBL as listed below
The SBL entry point needs to be different vs other applications. On AM263X after power-ON ROM boots the SBL and sets the entry point of SBL to both R5FSS0-0 as well as R5FSS0-1. However for SBL we need to detect the core and run SBL only on Core0 and keep Core1 in wfi loop. This is done by specifying a different entry point -e_vectors_sbl in the linker command file for the SBL application. In _vectors_sbl the very first thing it does is detect the core and continue execution for Core0, while if the core is Core1 then it enters wfi loop.
Other special factors for SBL application are listed below
The linker command file for SBL has to place vectors at address 0x70002000 and this is the entry point for the SBL.
Nothing should be placed in ATCM or BTCM
Only the region 0x70002000 to 0x70040000 should be used by SBL code, data, stack etc
After building, the SBL application .out file is first converted to a binary format .bin using the GCC objcopy tool.
This copies the loadable sections from the .out into a binary image stripping all symbol and section information.
If there are two loadable sections in the image which are not contiguous then objcopy fills the gaps with 0xFF.
It is highly recommended to keep all loadable sections together within a SBL application.
This .bin file is then signed using the Signing Scripts to create the final .tiimage bootable image.
A default key is used for this.
This is a ROM bootloader requirement and is needed even on a non-secure device.
This .tiimage file can then be flashed or copied to a boot image using the Flashing Tools